<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TypeA Layer3 Card Detection on PN7642 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/TypeA-Layer3-Card-Detection-on-PN7642/m-p/2379672#M14296</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262640"&gt;@wangea&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Layer 3 covers anti-collision, UID selection and card activation, while ISO 14443 layer 4 presents a set of standardized commands for data exchange. Basic Tags/Cards stop after Layer 3 and use proprietary memory-read/write commands instead of Layer 4.&lt;/P&gt;
&lt;P&gt;As you mentioned, you could try to implement the proprietary command set for your device. Please refer to NxpNfcRdlib -&amp;gt; types -&amp;gt; ph_Status.h for the Status Code definitions.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Wed, 10 Jun 2026 18:59:03 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2026-06-10T18:59:03Z</dc:date>
    <item>
      <title>TypeA Layer3 Card Detection on PN7642</title>
      <link>https://community.nxp.com/t5/NFC/TypeA-Layer3-Card-Detection-on-PN7642/m-p/2379433#M14295</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I'm using the demo&amp;nbsp;pnev7642fama_Nfcrdlib_SimplifiedAPI_ISO_Freertos_Pub for card detection, there are&amp;nbsp;&lt;SPAN&gt;E_PH_NFCLIB_MIFARE_CLASSIC_1K and&amp;nbsp;E_PH_NFCLIB_TYPEA_LAYER4&amp;nbsp; application cases, and it works well. But there is no application for&amp;nbsp;E_PH_NFCLIB_TYPEA_LAYER3, I tried to implement the application based on the card datasheet, but&amp;nbsp; there was no response, the status of&amp;nbsp;phNfcLib_Transmit() was always 0x20000. The card used are FM1208-10 and FM1216. I couldn't find the reason.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wangea_0-1781083669584.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/388505i523E8E7C60D3638B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wangea_0-1781083669584.png" alt="wangea_0-1781083669584.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have no idea why there is no application case for&amp;nbsp;E_PH_NFCLIB_TYPEA_LAYER3, Is there any references for this card type?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 09:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/TypeA-Layer3-Card-Detection-on-PN7642/m-p/2379433#M14295</guid>
      <dc:creator>wangea</dc:creator>
      <dc:date>2026-06-10T09:28:22Z</dc:date>
    </item>
    <item>
      <title>Re: TypeA Layer3 Card Detection on PN7642</title>
      <link>https://community.nxp.com/t5/NFC/TypeA-Layer3-Card-Detection-on-PN7642/m-p/2379672#M14296</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262640"&gt;@wangea&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Layer 3 covers anti-collision, UID selection and card activation, while ISO 14443 layer 4 presents a set of standardized commands for data exchange. Basic Tags/Cards stop after Layer 3 and use proprietary memory-read/write commands instead of Layer 4.&lt;/P&gt;
&lt;P&gt;As you mentioned, you could try to implement the proprietary command set for your device. Please refer to NxpNfcRdlib -&amp;gt; types -&amp;gt; ph_Status.h for the Status Code definitions.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 18:59:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/TypeA-Layer3-Card-Detection-on-PN7642/m-p/2379672#M14296</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-06-10T18:59:03Z</dc:date>
    </item>
  </channel>
</rss>