<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN7642 LPUART_polling demo issue</title>
    <link>https://community.nxp.com/t5/NFC/PN7642-LPUART-polling-demo-issue/m-p/2370371#M14242</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262640"&gt;@wangea&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;I can see that your custom board uses C101 variant. C101 uses FW v2.00 by default, and something important to remark is that an SDK is bound to a certain FW version. If your SDK version does not correspond to the FW version, some unexpected behavior may occur.&lt;/P&gt;
&lt;P&gt;Please try updating your firmware version through ay of the available methods described in &lt;A href="https://www.nxp.com/docs/en/application-note/AN14540.pdf" target="_blank"&gt;Firmware update on PN7642&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Fri, 22 May 2026 21:29:55 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2026-05-22T21:29:55Z</dc:date>
    <item>
      <title>PN7642 LPUART_polling demo issue</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-LPUART-polling-demo-issue/m-p/2370155#M14238</link>
      <description>&lt;P&gt;Hello&amp;nbsp;@&lt;SPAN&gt;EduardoZamora,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I got a similar issue when using&amp;nbsp;LPUART_polling SDK demo on our prototype, which had been reported on the forums linked&amp;nbsp;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NFC/PN7642-resets-when-calling-LPUART-Init/m-p/1785561" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/NFC/PN7642-resets-when-calling-LPUART-Init/m-p/1785561&lt;/A&gt;&amp;nbsp;&amp;amp; &lt;A href="https://community.nxp.com/t5/Other-NXP-Products/PN7642-LPUART-examples-not-working/m-p/1867980" target="_blank" rel="noopener"&gt;PN7642, LPUART examples not working - NXP Community&lt;/A&gt;&amp;nbsp; I couldn't see the further solution.&amp;nbsp;&amp;nbsp;no&amp;nbsp;I2C, I3C, SPI and USB interfaces used on our application. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There was no such issue with the demo examples&amp;nbsp;hello_world or Blinky.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SO what is the reason for this issue and how can we reslove it ?&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;with the reset chip, it couldn't be connected with Jlink. Is this recoverable？if yes, how?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ethan.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 09:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-LPUART-polling-demo-issue/m-p/2370155#M14238</guid>
      <dc:creator>wangea</dc:creator>
      <dc:date>2026-05-22T09:38:45Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 LPUART_polling demo issue</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-LPUART-polling-demo-issue/m-p/2370371#M14242</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/262640"&gt;@wangea&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;I can see that your custom board uses C101 variant. C101 uses FW v2.00 by default, and something important to remark is that an SDK is bound to a certain FW version. If your SDK version does not correspond to the FW version, some unexpected behavior may occur.&lt;/P&gt;
&lt;P&gt;Please try updating your firmware version through ay of the available methods described in &lt;A href="https://www.nxp.com/docs/en/application-note/AN14540.pdf" target="_blank"&gt;Firmware update on PN7642&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 21:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-LPUART-polling-demo-issue/m-p/2370371#M14242</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-05-22T21:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 LPUART_polling demo issue</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-LPUART-polling-demo-issue/m-p/2370745#M14248</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Appreciate for your quick response.&lt;/P&gt;&lt;P&gt;I had updated the fw to v3.00 using SDK version 2.15.006, since there is only one prototype left, i will take the verification for the lpuart after other function testing done.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently, I got another issue about RF distance when using the nfc example(pnev7642fama_NfcrdlibEx4_MIFAREClassic_Freertos_Pub).&amp;nbsp; &lt;SPAN&gt;The RF distance is only 2 cm, which is much smaller than the maximum distance supported by the PN7642.&amp;nbsp; since there is no usb inferface used on our prototype,&amp;nbsp; i added some configurations in the sw instead of NFC Cockpit, Shown as below,&amp;nbsp; attached is the detailed implements for each fuction. Besides, i had read&amp;nbsp;&lt;/SPAN&gt;RX_CONTROL_STATUS register (0x28)&amp;nbsp;&lt;SPAN&gt;and found&amp;nbsp;&lt;/SPAN&gt;HF_ATT_VALUE was always 63, even Increase or decrease RRx&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wangea_0-1779699417200.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386692i3BD635D57F568E42/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wangea_0-1779699417200.png" alt="wangea_0-1779699417200.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;pn7642 works in boost mode, and the antenna range is approximately 40*60 mm&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wangea_1-1779699632572.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/386695i15C65A06AECED59B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wangea_1-1779699632572.png" alt="wangea_1-1779699632572.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My question is:&lt;/P&gt;&lt;P&gt;Are the configurations correct or enough? If not, what should i do to improve the RF distance.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;Ethan.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 May 2026 09:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-LPUART-polling-demo-issue/m-p/2370745#M14248</guid>
      <dc:creator>wangea</dc:creator>
      <dc:date>2026-05-25T09:09:39Z</dc:date>
    </item>
  </channel>
</rss>