<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: PN7462AU Manual RF TX Power Control Using Runtime Commands</title>
    <link>https://community.nxp.com/t5/NFC/PN7462AU-Manual-RF-TX-Power-Control-Using-Runtime-Commands/m-p/2367121#M14223</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261175"&gt;@uday_gowda&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please consider that a device using DPC requires a dedicated antenna tuning. Disabling DPC or setting a wrong calibration/configuration may lead to damage.&lt;BR /&gt;&lt;BR /&gt;Although it is recommended to enable DPC, it is possible to disable it. You can refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN11742.pdf" target="_blank"&gt;AN11742 Dynamic Power Control&lt;/A&gt;, Section 1.2.1 for more information on register configuration.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Mon, 18 May 2026 20:44:33 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2026-05-18T20:44:33Z</dc:date>
    <item>
      <title>PN7462AU Manual RF TX Power Control Using Runtime Commands</title>
      <link>https://community.nxp.com/t5/NFC/PN7462AU-Manual-RF-TX-Power-Control-Using-Runtime-Commands/m-p/2365507#M14214</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;I am working on PN7462AU and need to implement manual RF transmitter power control with 3 configurable power levels (LOW / MEDIUM / HIGH) that can be changed dynamically based on received UART/CLI commands.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Currently, DPC handles TX power automatically, but my requirement is to bypass/fix the DPC behavior and manually switch TX power levels during runtime.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I would like to know:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Which RF registers are recommended to control TX power manually on PN7462AU?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any API already available for runtime TX power switching?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 11:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462AU-Manual-RF-TX-Power-Control-Using-Runtime-Commands/m-p/2365507#M14214</guid>
      <dc:creator>uday_gowda</dc:creator>
      <dc:date>2026-05-14T11:16:10Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462AU Manual RF TX Power Control Using Runtime Commands</title>
      <link>https://community.nxp.com/t5/NFC/PN7462AU-Manual-RF-TX-Power-Control-Using-Runtime-Commands/m-p/2367121#M14223</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261175"&gt;@uday_gowda&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please consider that a device using DPC requires a dedicated antenna tuning. Disabling DPC or setting a wrong calibration/configuration may lead to damage.&lt;BR /&gt;&lt;BR /&gt;Although it is recommended to enable DPC, it is possible to disable it. You can refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN11742.pdf" target="_blank"&gt;AN11742 Dynamic Power Control&lt;/A&gt;, Section 1.2.1 for more information on register configuration.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 18 May 2026 20:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462AU-Manual-RF-TX-Power-Control-Using-Runtime-Commands/m-p/2367121#M14223</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-05-18T20:44:33Z</dc:date>
    </item>
  </channel>
</rss>