<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RF Amplifier for NXP Contactless NFC Reader IC's in NFC</title>
    <link>https://community.nxp.com/t5/NFC/RF-Amplifier-for-NXP-Contactless-NFC-Reader-IC-s/m-p/2347206#M14156</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38496"&gt;@andydong1583&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Transmitting a power of 6 W from PN7160 or PN5180 through an external PA is an impractical and unfeasible design solution in NFC/HF RFID applications.&lt;/P&gt;</description>
    <pubDate>Wed, 08 Apr 2026 12:22:18 GMT</pubDate>
    <dc:creator>KaiLi</dc:creator>
    <dc:date>2026-04-08T12:22:18Z</dc:date>
    <item>
      <title>RF Amplifier for NXP Contactless NFC Reader IC's</title>
      <link>https://community.nxp.com/t5/NFC/RF-Amplifier-for-NXP-Contactless-NFC-Reader-IC-s/m-p/2346996#M14155</link>
      <description>&lt;P&gt;Hi，&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;How about&amp;nbsp;&lt;A href="https://www.nxp.com.cn/products/PN7160" rel="noopener nofollow noreferrer" target="_blank"&gt;&lt;SPAN class=""&gt;PN7160&lt;/SPAN&gt;&lt;/A&gt;/&lt;A href="https://www.nxp.com.cn/products/PN5180" rel="noopener nofollow noreferrer" target="_blank"&gt;&lt;SPAN class=""&gt;PN5180&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;SPAN&gt;Can the solution for adding an external PA refer to AN11003? If so, are there any specific recommendations for ISO15693?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Additionally, if the TX power is increased to 6W (1A, 6V), what precautions should be taken when using it with the NTAG 5 Link?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;andy&lt;/P&gt;</description>
      <pubDate>Wed, 08 Apr 2026 09:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RF-Amplifier-for-NXP-Contactless-NFC-Reader-IC-s/m-p/2346996#M14155</guid>
      <dc:creator>andydong1583</dc:creator>
      <dc:date>2026-04-08T09:58:04Z</dc:date>
    </item>
    <item>
      <title>Re: RF Amplifier for NXP Contactless NFC Reader IC's</title>
      <link>https://community.nxp.com/t5/NFC/RF-Amplifier-for-NXP-Contactless-NFC-Reader-IC-s/m-p/2347206#M14156</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/38496"&gt;@andydong1583&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Transmitting a power of 6 W from PN7160 or PN5180 through an external PA is an impractical and unfeasible design solution in NFC/HF RFID applications.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Apr 2026 12:22:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RF-Amplifier-for-NXP-Contactless-NFC-Reader-IC-s/m-p/2347206#M14156</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2026-04-08T12:22:18Z</dc:date>
    </item>
    <item>
      <title>Re: RF Amplifier for NXP Contactless NFC Reader IC's</title>
      <link>https://community.nxp.com/t5/NFC/RF-Amplifier-for-NXP-Contactless-NFC-Reader-IC-s/m-p/2347849#M14158</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205266"&gt;@KaiLi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the reason? (NFC standard requires less than 7.5 A/m)&lt;BR /&gt;1. NTAG 5's La/Lb: 12 A/m; peak value up to 61.87; and maximum La/Lb peak current is +/-168 mA.&lt;BR /&gt;2. Usage scenario: the reader is more than 5 cm away from the NTAG 5. Antenna ratio is 10:1.&lt;BR /&gt;3. The reader only works with NTAG 5 series tags and does not read other cards.&lt;/P&gt;&lt;P&gt;What about using an external PA to increase the power to 3W (5V, 600 mA)? Is it feasible?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;andy&lt;/P&gt;</description>
      <pubDate>Thu, 09 Apr 2026 03:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RF-Amplifier-for-NXP-Contactless-NFC-Reader-IC-s/m-p/2347849#M14158</guid>
      <dc:creator>andydong1583</dc:creator>
      <dc:date>2026-04-09T03:13:47Z</dc:date>
    </item>
  </channel>
</rss>