<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックJ-Link Commander Cannot Download Image to PN7642 (Some Units Previously Working Now Failing)</title>
    <link>https://community.nxp.com/t5/NFC/J-Link-Commander-Cannot-Download-Image-to-PN7642-Some-Units/m-p/2344508#M14147</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm encountering an issue when using &lt;EM&gt;&lt;STRONG&gt;J-Link Commander&lt;/STRONG&gt;&lt;/EM&gt; to download firmware to the &lt;LI-PRODUCT title="PN7642" id="PN7642"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Summary:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;* Total units: 36&lt;/P&gt;&lt;P&gt;* 22 units: working normally&lt;/P&gt;&lt;P&gt;* 14 units: consistently failing&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Important note:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;All units were previously programmed successfully with our earlier firmware. The issue appeared when attempting to reprogram them with a newer image.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Issue description:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;For the failing units, J-Link Commander cannot connect to the target device. The log output is shown below:&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;Connecting to target via SWD&lt;BR /&gt;Found SW-DP with ID 0x6BA02477&lt;BR /&gt;DPIDR: 0x6BA02477&lt;BR /&gt;CoreSight SoC-400 or earlier&lt;BR /&gt;Scanning AP map to find all available APs&lt;BR /&gt;AP[1]: Stopped AP scan as end of AP map seems to be reached&lt;BR /&gt;AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)&lt;BR /&gt;Iterating through AP map to find AHB-AP to use&lt;BR /&gt;AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;Attach to CPU failed. Executing connect under reset.&lt;BR /&gt;Failed to power up DAP&lt;BR /&gt;Found SW-DP with ID 0x6BA02477&lt;BR /&gt;DPIDR: 0x6BA02477&lt;BR /&gt;CoreSight SoC-400 or earlier&lt;BR /&gt;Scanning AP map to find all available APs&lt;BR /&gt;AP[1]: Stopped AP scan as end of AP map seems to be reached&lt;BR /&gt;AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)&lt;BR /&gt;Iterating through AP map to find AHB-AP to use&lt;BR /&gt;AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;Attach to CPU failed. Executing connect under reset.&lt;BR /&gt;Failed to power up DAP&lt;BR /&gt;Error occurred: Could not connect to the target device.&lt;BR /&gt;For troubleshooting steps visit: &lt;A href="https://wiki.segger.com/J-Link_Troubleshooting" target="_blank"&gt;https://wiki.segger.com/J-Link_Troubleshooting&lt;/A&gt;&lt;BR /&gt;```&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Additional information:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I have tried issuing the r (reset) command in J-Link Commander, but it does not resolve the issue&lt;/LI&gt;&lt;LI&gt;Same hardware setup is used for both working and failing units (same J-Link, same board, same procedure)&lt;/LI&gt;&lt;LI&gt;All failing units show identical behavior&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Observations:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Failure occurs during SWD connection:&lt;UL&gt;&lt;LI&gt;Cannot read CPUID&lt;/LI&gt;&lt;LI&gt;DAP power-up fails&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;Working units remain fully programmable&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Questions:&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Are there known mechanisms in PN7642 that can disable or lock SWD after programming?&lt;/LI&gt;&lt;LI&gt;Is there a recommended way recover access (e.g., connect under reset, mass erase, boot pin configuration)?&lt;/LI&gt;&lt;LI&gt;Could this indicate the device entering a protected or low-power state that blocks debug access?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance on how to recover these devices or further debug the root cause would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Apr 2026 10:41:02 GMT</pubDate>
    <dc:creator>axis-zhao</dc:creator>
    <dc:date>2026-04-02T10:41:02Z</dc:date>
    <item>
      <title>J-Link Commander Cannot Download Image to PN7642 (Some Units Previously Working Now Failing)</title>
      <link>https://community.nxp.com/t5/NFC/J-Link-Commander-Cannot-Download-Image-to-PN7642-Some-Units/m-p/2344508#M14147</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm encountering an issue when using &lt;EM&gt;&lt;STRONG&gt;J-Link Commander&lt;/STRONG&gt;&lt;/EM&gt; to download firmware to the &lt;LI-PRODUCT title="PN7642" id="PN7642"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Summary:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;* Total units: 36&lt;/P&gt;&lt;P&gt;* 22 units: working normally&lt;/P&gt;&lt;P&gt;* 14 units: consistently failing&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Important note:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;All units were previously programmed successfully with our earlier firmware. The issue appeared when attempting to reprogram them with a newer image.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Issue description:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;For the failing units, J-Link Commander cannot connect to the target device. The log output is shown below:&lt;/P&gt;&lt;P&gt;```&lt;/P&gt;&lt;P&gt;Connecting to target via SWD&lt;BR /&gt;Found SW-DP with ID 0x6BA02477&lt;BR /&gt;DPIDR: 0x6BA02477&lt;BR /&gt;CoreSight SoC-400 or earlier&lt;BR /&gt;Scanning AP map to find all available APs&lt;BR /&gt;AP[1]: Stopped AP scan as end of AP map seems to be reached&lt;BR /&gt;AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)&lt;BR /&gt;Iterating through AP map to find AHB-AP to use&lt;BR /&gt;AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;Attach to CPU failed. Executing connect under reset.&lt;BR /&gt;Failed to power up DAP&lt;BR /&gt;Found SW-DP with ID 0x6BA02477&lt;BR /&gt;DPIDR: 0x6BA02477&lt;BR /&gt;CoreSight SoC-400 or earlier&lt;BR /&gt;Scanning AP map to find all available APs&lt;BR /&gt;AP[1]: Stopped AP scan as end of AP map seems to be reached&lt;BR /&gt;AP[0]: AHB-AP (IDR: 0x84770001, ADDR: 0x00000000)&lt;BR /&gt;Iterating through AP map to find AHB-AP to use&lt;BR /&gt;AP[0]: Skipped. Could not read CPUID register&lt;BR /&gt;Attach to CPU failed. Executing connect under reset.&lt;BR /&gt;Failed to power up DAP&lt;BR /&gt;Error occurred: Could not connect to the target device.&lt;BR /&gt;For troubleshooting steps visit: &lt;A href="https://wiki.segger.com/J-Link_Troubleshooting" target="_blank"&gt;https://wiki.segger.com/J-Link_Troubleshooting&lt;/A&gt;&lt;BR /&gt;```&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Additional information:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I have tried issuing the r (reset) command in J-Link Commander, but it does not resolve the issue&lt;/LI&gt;&lt;LI&gt;Same hardware setup is used for both working and failing units (same J-Link, same board, same procedure)&lt;/LI&gt;&lt;LI&gt;All failing units show identical behavior&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Observations:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Failure occurs during SWD connection:&lt;UL&gt;&lt;LI&gt;Cannot read CPUID&lt;/LI&gt;&lt;LI&gt;DAP power-up fails&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;Working units remain fully programmable&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Questions:&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Are there known mechanisms in PN7642 that can disable or lock SWD after programming?&lt;/LI&gt;&lt;LI&gt;Is there a recommended way recover access (e.g., connect under reset, mass erase, boot pin configuration)?&lt;/LI&gt;&lt;LI&gt;Could this indicate the device entering a protected or low-power state that blocks debug access?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance on how to recover these devices or further debug the root cause would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Apr 2026 10:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/J-Link-Commander-Cannot-Download-Image-to-PN7642-Some-Units/m-p/2344508#M14147</guid>
      <dc:creator>axis-zhao</dc:creator>
      <dc:date>2026-04-02T10:41:02Z</dc:date>
    </item>
    <item>
      <title>Re: J-Link Commander Cannot Download Image to PN7642 (Some Units Previously Working Now Failing)</title>
      <link>https://community.nxp.com/t5/NFC/J-Link-Commander-Cannot-Download-Image-to-PN7642-Some-Units/m-p/2344608#M14148</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261323"&gt;@axis-zhao&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please try J-Flash, it works fine on my side, like attach picture.&lt;/P&gt;
&lt;DIV id="tinyMceEditorKaiLi_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Apr 2026 12:23:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/J-Link-Commander-Cannot-Download-Image-to-PN7642-Some-Units/m-p/2344608#M14148</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2026-04-02T12:23:30Z</dc:date>
    </item>
    <item>
      <title>Re: J-Link Commander Cannot Download Image to PN7642 (Some Units Previously Working Now Failing)</title>
      <link>https://community.nxp.com/t5/NFC/J-Link-Commander-Cannot-Download-Image-to-PN7642-Some-Units/m-p/2344661#M14149</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205266"&gt;@KaiLi&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thanks for the suggestion to try J-Flash.&lt;/P&gt;&lt;P&gt;I've attempted to use J-Flash with my PN7642, but I'm consistently running into connection failures. The behavior is similar to what I observed with J-Link Commander - J-Flash is unable to establish a connection to the target. (See the attached file, 'j_flash_connection_error.png').&lt;/P&gt;&lt;P&gt;Are there any additional steps or recovery methods you would recommend to regain access?&lt;/P&gt;&lt;P&gt;Any guidance would be greatly appreciated!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&lt;/P&gt;</description>
      <pubDate>Thu, 02 Apr 2026 12:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/J-Link-Commander-Cannot-Download-Image-to-PN7642-Some-Units/m-p/2344661#M14149</guid>
      <dc:creator>axis-zhao</dc:creator>
      <dc:date>2026-04-02T12:54:02Z</dc:date>
    </item>
  </channel>
</rss>