<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN5190B1 pin layout setup in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2320384#M14077</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Taking a look at your schematics, I could not find VDDIO power supply; this voltage is required for the Host Interface and GPIOs. Also, pull-up resistor on VEN pin should be connected to VDDIO. Aside from that, all other power connections and capacitors should be OK.&lt;BR /&gt;&lt;BR /&gt;For the layout, please refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12549.pdf" target="_blank"&gt;PN5190 antenna design guide&lt;/A&gt;, Section 3.4. These are the recommendations for VBATPWR, VDDBOOST, BOOST_LX:&lt;/P&gt;
&lt;P&gt;1. Place components as close as possible to each other.&lt;/P&gt;
&lt;P&gt;2. Route VBATPWR, BOOSTLX, VDDBOOST as short as possible.&lt;/P&gt;
&lt;P&gt;3. Provide Cu shape. If shape is not possible, route with a wide trace (150mils).&lt;/P&gt;
&lt;P&gt;4. No vias are allowed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Feb 2026 18:16:44 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2026-02-19T18:16:44Z</dc:date>
    <item>
      <title>PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2317087#M14048</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Im creating the schematic and layout for the&amp;nbsp;PN5190B1 and due my ultra low power consuption request i will nor TXLDO not DC-DC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, i assume that i need to go for configuration example 3 on chapter 9.5.3.6 of the datasheet.&lt;/P&gt;&lt;P&gt;My doubt is what to do with following pins: BOOST_LX, VDDBOOTS, VUP ,VSS PWR and VDDPA.&amp;nbsp; I would say that i need to left some open and not connected to anything but i can not find a clear advise on that and on the datasheet figure it looks that they are connected....&lt;/P&gt;&lt;P&gt;Could you help me?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks in advanced,&lt;/P&gt;&lt;P&gt;ignacio&lt;/P&gt;</description>
      <pubDate>Thu, 12 Feb 2026 11:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2317087#M14048</guid>
      <dc:creator>ignacioS</dc:creator>
      <dc:date>2026-02-12T11:14:18Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2317406#M14053</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259860"&gt;@ignacioS&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;As I understand, you are considering a design that uses neither TXLDO nor DC-DC, is this correct? Configuration example 3 shown in &lt;A href="https://www.nxp.com/docs/en/data-sheet/PN5190B2.pdf" target="_blank"&gt;PN5190 Data Sheet&lt;/A&gt; does use TXLDO, while not using DC-DC converter. The VBAT = VUP drives the TXLDO, which provides the VDDPA.&lt;/P&gt;
&lt;P&gt;According to your requirements, please consider using configuration example 5 as reference for the required connections:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_0-1770933125896.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/376693iF771F5700893F0A9/image-size/large?v=v2&amp;amp;px=999" role="button" title="EduardoZamora_0-1770933125896.png" alt="EduardoZamora_0-1770933125896.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_0-1770933125896.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Feb 2026 21:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2317406#M14053</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-02-12T21:53:42Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2317842#M14058</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hi Eduardo,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Thank you for your quick reply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Before moving forward, I think I first need to better understand the available options. My device will operate in ultra-low-power mode using polling. That’s why I have already read that I should not use the DC/DC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;However, regarding the LDO: in principle, to avoid additional consumption I am not planning to use it, and I intend to power everything directly from the 3.3 V rail of the supply. This leads to my first question: is “not using the LDO” the same as “not connecting it”? If both options are possible, do they consume the same? I assume that leaving it unconnected would be more efficient.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;My second question is about the DCDC and LDO pins. In the figures in the datasheet I see BOOST_LX, VDDBOOST,VUP,... connected to VBATPWR. This is what I don’t understand. If I am not using the boost converter, do I simply skip the inductor and direct connect that line to VBATPWR? I’m not sure what I should do with these pins if I am not using them.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Thank you very much for your help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Feb 2026 12:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2317842#M14058</guid>
      <dc:creator>ignacioS</dc:creator>
      <dc:date>2026-02-13T12:25:07Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2318070#M14062</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For ULPCD usage, either "TX_LDO transmitter supply" or "Direct transmitter supply" connections are recommended. According to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12551.pdf" target="_blank"&gt;PN5190 design-in recommendations&lt;/A&gt;, Section 2.1.4, not using the TXLDO (DPC becomes obsolete) should save a few mV at the TX driver supply.&lt;/P&gt;
&lt;P&gt;If you are not using the TXLDO, you should consider a Direct transmitter supply configuration, where TXLDO is configured OFF and VUP_TX and VDDPA are connected to VBAT/VBATPWR.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_0-1771016740938.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/376862iDD2C774755E20087/image-size/large?v=v2&amp;amp;px=999" role="button" title="EduardoZamora_0-1771016740938.png" alt="EduardoZamora_0-1771016740938.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_0-1771016740938.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Boost inductor is only required for DC-DC operation. According to your requirements, please refer to configuration example 5, which requires the following connections:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_1-1771016779662.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/376863i0143224DE39D366D/image-size/large?v=v2&amp;amp;px=999" role="button" title="EduardoZamora_1-1771016779662.png" alt="EduardoZamora_1-1771016779662.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_1-1771016779662.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Feb 2026 21:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2318070#M14062</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-02-13T21:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2318478#M14067</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hi Eduardo,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;Thank you! Now that I’ve re-read everything again, I’m no longer sure I’m thinking about this correctly.&lt;/P&gt;&lt;P class=""&gt;My device has to stay in ULPCD mode all the time, and when it detects a card or a mobile phone it will wake up. I initially understood that, to achieve the lowest possible consumption, I should operate without the DC/DC boost and without the LDO. However, I’m now thinking my interpretation may be incorrect, and that what I actually need to do is simply disable them when entering ULPCD, but when the device is active and communicating it may be useful to have them enabled.&lt;/P&gt;&lt;P class=""&gt;Is that correct?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks again!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Feb 2026 09:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2318478#M14067</guid>
      <dc:creator>ignacioS</dc:creator>
      <dc:date>2026-02-16T09:20:45Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2318745#M14068</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For low-power reader devices, the use of DC-DC does not make sense; ULPCD cannot be used together with the DC-DC function. Also, specific hardware configurations ("TX_LDO transmitter supply" or "Direct transmitter supply") that would make DC-DC not available are required.&lt;/P&gt;
&lt;P&gt;When DC-DC converter is not used, there some settings that must be considered for TXLDO. Please, refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN13669.pdf" target="_blank"&gt;PN5190 questions and answers&lt;/A&gt;, Chapter 9.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 16 Feb 2026 20:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2318745#M14068</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-02-16T20:28:19Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2319014#M14072</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Hi Eduardo,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Thanks for your message. In your opinion, given your experience with NXP, is it worth enabling the TXLDO or not?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;My understanding (please correct me if I’m wrong) is that while the device is in ULPCD/ULP mode I should keep TXLDO disabled, but when it wakes up and needs to communicate I can enable TXLDO to supply the TX path.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;In my design, the NXP module/IC is powered only from a single 3.3 V rail coming from another board (battery + regulator). The environment will be challenging, with metal around and partially in front of the device, so any improvement in RF performance would be very helpful.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I assum&lt;/SPAN&gt;&lt;SPAN&gt;e that keeping TXLDO disabled in ULPCD does not add any extra current consumption, correct? During communication I could accept some losses/overhead, since it will only transmit a few times per day.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What do you think?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;On the other hand, going back to the DC/DC: it surprises me that if I don’t want to use it, I still have to connect it directly to VBATPWR, but in any case that’s what I will do. I will follow configuration 3 from the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ignacioS_0-1771329852897.png" style="width: 463px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377036iFC21DC94E8B6B676/image-dimensions/463x242?v=v2" width="463" height="242" role="button" title="ignacioS_0-1771329852897.png" alt="ignacioS_0-1771329852897.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ignacioS_0-1771329852897.png&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Once I have the schematic ready, I’d like to paste it here so you can take a look and tell me if you see anything unusual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for your support&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Feb 2026 12:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2319014#M14072</guid>
      <dc:creator>ignacioS</dc:creator>
      <dc:date>2026-02-17T12:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2319222#M14074</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Operation without DC-DC converter, but with TXLDO, is a typical use case. TXLDO does not exclude the use of ULPCD. Configuration example 3 should be OK for this purpose.&lt;/P&gt;
&lt;P&gt;Although ULPCD (together with a proper &lt;A href="https://www.nxp.com/docs/en/application-note/AN12549.pdf" target="_blank"&gt;antenna design for PN5190&lt;/A&gt;) could achieve up to ~4cm, a metal environment will be a challenge since sensitivity is reduced in this mode.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Feb 2026 20:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2319222#M14074</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-02-17T20:53:06Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2319997#M14076</link>
      <description>&lt;P&gt;Thanks Eduardo, lets just help me to check some details and i think we are done here.&lt;/P&gt;&lt;P&gt;My question is about the pins BOOST_LX, VDDBOOST and VSS_PWR. In the configuration example 3 , the first two are connected to the input supply, and VSS_PWR is connected to GND. This is my biggest doubt: &lt;STRONG&gt;1.&lt;/STRONG&gt;- is this correct?, or should these three pins be left unconnected (floating) if the DCDC boost is not used? I see what the datasheet shows but , not sure, i really have doubts that this is like that and i would apreciate a clear confirmation.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ignacioS_0-1771459995978.png" style="width: 637px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377200i729918D4A658DF6D/image-dimensions/637x352?v=v2" width="637" height="352" role="button" title="ignacioS_0-1771459995978.png" alt="ignacioS_0-1771459995978.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ignacioS_0-1771459995978.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is my current schematic, in which I have added the three connections that are generating doubts for me. Apart from these, &lt;STRONG&gt;2.-&lt;/STRONG&gt; is the schematic correct for my product?&lt;/P&gt;&lt;P&gt;I would appreciate it if you could double-check it, as I am going to migrate the entire product range to this chip and I urgently need the prototypes to work correctly on the first run.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Assuming they must be connected, I also see in the diagram that they are connected before the input capacitor. &lt;STRONG&gt;3&lt;/STRONG&gt;.-&amp;nbsp; Would a layout where I connect pins 1 and 2 to pin 39 under the chip (with a 0.2 mm trace) be acceptable?, or would it be better to route the connection outside the package? &amp;nbsp;&amp;nbsp;&lt;STRONG&gt;4.- &lt;/STRONG&gt;Is it important that it is before the capacitor, or does it not matter?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ignacioS_1-1771460081481.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377201i11BAA9E6EE92907E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ignacioS_1-1771460081481.png" alt="ignacioS_1-1771460081481.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ignacioS_1-1771460081481.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your help.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Feb 2026 00:19:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2319997#M14076</guid>
      <dc:creator>ignacioS</dc:creator>
      <dc:date>2026-02-19T00:19:12Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2320384#M14077</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Taking a look at your schematics, I could not find VDDIO power supply; this voltage is required for the Host Interface and GPIOs. Also, pull-up resistor on VEN pin should be connected to VDDIO. Aside from that, all other power connections and capacitors should be OK.&lt;BR /&gt;&lt;BR /&gt;For the layout, please refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN12549.pdf" target="_blank"&gt;PN5190 antenna design guide&lt;/A&gt;, Section 3.4. These are the recommendations for VBATPWR, VDDBOOST, BOOST_LX:&lt;/P&gt;
&lt;P&gt;1. Place components as close as possible to each other.&lt;/P&gt;
&lt;P&gt;2. Route VBATPWR, BOOSTLX, VDDBOOST as short as possible.&lt;/P&gt;
&lt;P&gt;3. Provide Cu shape. If shape is not possible, route with a wide trace (150mils).&lt;/P&gt;
&lt;P&gt;4. No vias are allowed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Feb 2026 18:16:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2320384#M14077</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-02-19T18:16:44Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190B1 pin layout setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2320460#M14079</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;Wow Eduardo, that was a very good catch on a major mistake on my side — thank you very much for that.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I’ve just adjusted everything and have now tied &lt;/SPAN&gt;VDDIO to 3V3, and also fixed the VEN pull-up&lt;SPAN&gt; accordingly. With this, I think we can consider this topic closed , isnt' it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ignacioS_0-1771542044154.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377309i6E89FB2481941D60/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ignacioS_0-1771542044154.png" alt="ignacioS_0-1771542044154.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ignacioS_0-1771542044154.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;To avoid mixing topics, I’ve opened another thread regarding the different models and their firmware versions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Many thanks again for your help.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Feb 2026 23:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190B1-pin-layout-setup/m-p/2320460#M14079</guid>
      <dc:creator>ignacioS</dc:creator>
      <dc:date>2026-02-19T23:04:47Z</dc:date>
    </item>
  </channel>
</rss>