<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN7642 Module FCC ID</title>
    <link>https://community.nxp.com/t5/NFC/PN7642-Module-FCC-ID/m-p/2294525#M13989</link>
    <description>Thanks Eduardo, I have followed the guidelines and the unit has passed testing. FCC has particular requirements, such as a mandatory screen can, which is used on the pagoda reference design, which I had used as a starting point. Beyond that it is mainly paperwork!</description>
    <pubDate>Thu, 15 Jan 2026 18:59:14 GMT</pubDate>
    <dc:creator>scroggyg</dc:creator>
    <dc:date>2026-01-15T18:59:14Z</dc:date>
    <item>
      <title>PN7642 Module FCC ID</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Module-FCC-ID/m-p/2294232#M13986</link>
      <description>&lt;P&gt;We have designed a NFC module based around PN7642, is there an application note on meeting the FCC requirements to get it listed as a module?&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jan 2026 11:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Module-FCC-ID/m-p/2294232#M13986</guid>
      <dc:creator>gredpath</dc:creator>
      <dc:date>2026-01-15T11:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 Module FCC ID</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Module-FCC-ID/m-p/2294523#M13988</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/115877"&gt;@gredpath&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;My apologies, there is no specific documentation about FCC-compliance. I would recommend you confirm that you have followed the guidelines included in &lt;A href="https://www.nxp.com/docs/en/application-note/AN13467.pdf" target="_blank"&gt;PN76 family antenna design guide&lt;/A&gt;, which describes the NFC antenna design and tuning, DPC functionality and layout recommendations; also, please take a look at the &lt;A href="https://www.nxp.com/docs/en/application-note/AN14138.pdf" target="_blank"&gt;PN7642 design-in recommendations&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Additionally, I could also recommend following the &lt;A href="https://www.nxp.com/design/design-center/training/TIP-NFC-ANTENNA-DESIGN" target="_blank"&gt;NFC Antenna Design training series&lt;/A&gt; as it describes key aspects for the antenna, debugging, test and qualification, and EMC related design.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jan 2026 18:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Module-FCC-ID/m-p/2294523#M13988</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-01-15T18:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 Module FCC ID</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Module-FCC-ID/m-p/2294525#M13989</link>
      <description>Thanks Eduardo, I have followed the guidelines and the unit has passed testing. FCC has particular requirements, such as a mandatory screen can, which is used on the pagoda reference design, which I had used as a starting point. Beyond that it is mainly paperwork!</description>
      <pubDate>Thu, 15 Jan 2026 18:59:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Module-FCC-ID/m-p/2294525#M13989</guid>
      <dc:creator>scroggyg</dc:creator>
      <dc:date>2026-01-15T18:59:14Z</dc:date>
    </item>
  </channel>
</rss>