<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NT3H2111 VOUT Max Capacitance in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2291919#M13977</link>
    <description>&lt;P&gt;The NT3H2111 datasheet lists a "total connected capacitor" range of "150 nF up to 220 nF maximum". Is the 0.22uF max a hard limit? I'd like to run the energy harvest output through a LDO to provide a normalized voltage with multiple possible voltage sources (VOUT from the HT3H2111, power from a debug/programming probe). The LDO requires a 1uF input cap, which exceeds the 0.22uF limit.&lt;/P&gt;&lt;P&gt;Even if I didn't use an LDO, the combined decoupling caps on the microcontroller will exceed the 0.22uF limit.&lt;/P&gt;&lt;P&gt;How do people deal with this limit? Or can it be safely ignored?&lt;/P&gt;&lt;P&gt;Thanks, mike&lt;/P&gt;</description>
    <pubDate>Mon, 12 Jan 2026 18:18:30 GMT</pubDate>
    <dc:creator>mike_durian</dc:creator>
    <dc:date>2026-01-12T18:18:30Z</dc:date>
    <item>
      <title>NT3H2111 VOUT Max Capacitance</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2291919#M13977</link>
      <description>&lt;P&gt;The NT3H2111 datasheet lists a "total connected capacitor" range of "150 nF up to 220 nF maximum". Is the 0.22uF max a hard limit? I'd like to run the energy harvest output through a LDO to provide a normalized voltage with multiple possible voltage sources (VOUT from the HT3H2111, power from a debug/programming probe). The LDO requires a 1uF input cap, which exceeds the 0.22uF limit.&lt;/P&gt;&lt;P&gt;Even if I didn't use an LDO, the combined decoupling caps on the microcontroller will exceed the 0.22uF limit.&lt;/P&gt;&lt;P&gt;How do people deal with this limit? Or can it be safely ignored?&lt;/P&gt;&lt;P&gt;Thanks, mike&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jan 2026 18:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2291919#M13977</guid>
      <dc:creator>mike_durian</dc:creator>
      <dc:date>2026-01-12T18:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 VOUT Max Capacitance</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2292728#M13981</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/114664"&gt;@mike_durian&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;As stated in the documentation, and as you mention, NXP recommends a storage capacitor in the range of 150nF to 220nF between VOUT and GND to ensure the voltage does not drop during modulation or application.&lt;/P&gt;
&lt;P&gt;You should consider that the capacity connected to the energy harvesting pin should only be as large as needed by the external system – the larger the capacity is, the harder it is for the reader to wake up and supply the NTAG I²C.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jan 2026 17:02:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2292728#M13981</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-01-13T17:02:18Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 VOUT Max Capacitance</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2292744#M13982</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for the reply. So the 0.22uF limit is not a hard cap? You say a larger load will make it harder for the reader to wake up.&amp;nbsp;Is there any documentation, charts, graphs, etc. that show the effect of load capacitance on system behavior (at different field strengths)?&lt;/P&gt;&lt;P&gt;How do people power MCUs and associated circuitry that require larger load capacitance?&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jan 2026 17:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2292744#M13982</guid>
      <dc:creator>mike_durian</dc:creator>
      <dc:date>2026-01-13T17:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 VOUT Max Capacitance</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2294481#M13987</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;My apologies, the only information available regarding Energy Harvesting behavior is included in &lt;A href="https://www.nxp.com/docs/en/application-note/AN11578.pdf" target="_blank"&gt;AN11578 Energy Harvesting with the NTAG I²C and NTAG I²C plus&lt;/A&gt; (considering a 220nF capacitor) and &lt;A href="https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf" target="_blank"&gt;NTAG I2C plus Data Sheet&lt;/A&gt;, Chapter 8.6.&lt;/P&gt;
&lt;P&gt;Perhaps you could consider a Diode to try to isolate a "local" capacitance; however, this out of my scope and it depends on your design. Please keep in mind that our recommendation is to use a total capacitance in the range of 150nF - 220nF for reliable operation, otherwise the proper functioning cannot be guaranteed. I apologize for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jan 2026 17:34:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-VOUT-Max-Capacitance/m-p/2294481#M13987</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2026-01-15T17:34:45Z</dc:date>
    </item>
  </channel>
</rss>