<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with NTAG protected in NFC side in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2264729#M13926</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;BR /&gt;In the screenshots I sent in the ticket, you can see that in the SET PASSWORD command I used 0x01 for reading and 0x02 for writing. From the tests I ran, only the read command in a read-protected memory region worked. For writing in a write-protected memory region, I used the following commands:&lt;BR /&gt;- SET PASSWORD with password identifier 0x02; this command worked;&lt;BR /&gt;- WRITE in register 0x14, for example; this command returns 0x01 0x0F.&lt;/P&gt;&lt;P&gt;Based on these tests I performed and the register values I sent in my previous reply, can you replicate the same scenario on your end?&lt;BR /&gt;Is there any configuration error in either the register values or the commands?&lt;BR /&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;NSF&lt;/P&gt;</description>
    <pubDate>Wed, 17 Dec 2025 09:47:15 GMT</pubDate>
    <dc:creator>NSF</dc:creator>
    <dc:date>2025-12-17T09:47:15Z</dc:date>
    <item>
      <title>Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2259945#M13905</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the NXP tag NTP5332 and actually I has problems with commands that are sent via NFC using customized mobile app. On the NFC side, I am having problems writing to a password-protected memory region. To read a memory region protected against reading, I follow the sequence of commands described above, changing only the Password Identifier to 0x01 and the operation to read; in this case, the read operation is successful. If the password protection against reading and writing is removed, the read and write commands work without any problems.&lt;/P&gt;&lt;P&gt;Can anyone help me with these issues? Am I sending the wrong command?&lt;BR /&gt;Thanks for your help!&lt;/P&gt;</description>
      <pubDate>Thu, 11 Dec 2025 09:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2259945#M13905</guid>
      <dc:creator>NSF</dc:creator>
      <dc:date>2025-12-11T09:37:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2263097#M13920</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257913"&gt;@NSF&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please confirm that is the memory region you are trying to write to (User memory or Configuration memory)?&lt;/P&gt;
&lt;P&gt;What is the configuration of your Protection Pointer and related conditions?&lt;/P&gt;
&lt;P&gt;Is there any chance you have perform a Lock operation to the region you are trying to write? What is the value of your NFC Lock Block Configuration blocks?&lt;/P&gt;
&lt;P&gt;Please consider that we recommend using &lt;A href="https://www.nxp.com/design/design-center/software/rfid-developer-resources/taplinx-software-development-kit-sdk:TAPLINX" target="_blank"&gt;TapLinx SDK&lt;/A&gt;. This SDK provides some tools for contactless applications development in smartphones. The open API allows developers open access to all hardware features of NXP‘s NFC product portfolio. It provides a subset of features for quick and easy development of lightweight applications.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Dec 2025 22:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2263097#M13920</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-12-15T22:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2263747#M13923</link>
      <description>&lt;DIV&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for your reply!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;These are the configurations that the NFC tag has:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Reg. 0x1037 (Configuration Bytes): [0]: 0x09; [1]: 0x00; [2]: 0x5f; [3]: 0x00&lt;/DIV&gt;&lt;DIV&gt;Reg. 0x103F (Device Security Configuration): [0]: 0x45; [1]: 0x00; [2]: 0xff; [3]: 0xff&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- NFC security: plain password&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- Configuration area is not read and write protected from NFC perspective&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- PP_AREA_1: 0xFFFF (is pointing outside the user memory)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;Reg. 0x1020 (Read Password): [0]: 0x00; [1]: 0x00; [2]: 0x00; [3]: 0x00&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- Read Password is 0x00000000&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;Reg. 0x1021 (Write Password): [0]: 0x00; [1]: 0x00; [2]: 0x00; [3]: 0x00&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- Write Password is 0x00000000&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;Reg. 0x1058 (NFC Protection Pointer): [0]: 0x08; [1]: 0x30; [2]: 0x00; [3]: 0x00&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- NFC_PP_AREA_0H: 0x08&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- NFC_PPC: 0x30 (AREA_0-H is write and read protected; AREA_0-L is not read and write protected)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;Reg. 0x100C: [0]: 0x00; [1]: 0x81; [2]: 0x00; [3]: 0x00&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;- NFC_GCH: 0x81 (The NFC passwords can be read and written with the READ CONFIG&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; and WRITE CONFIG commands)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Memory organization:&lt;/DIV&gt;&lt;DIV&gt;0x00 - 0x08 --&amp;gt; NFC_AREA_0_L (is not read and write protected)&lt;/DIV&gt;&lt;DIV&gt;0x08 - end of memory --&amp;gt; NFC_AREA_0_H (read and write protected)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;NSF&lt;/DIV&gt;</description>
      <pubDate>Tue, 16 Dec 2025 10:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2263747#M13923</guid>
      <dc:creator>NSF</dc:creator>
      <dc:date>2025-12-16T10:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2264196#M13924</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Please, try performing SET PASSWORD for both Read and Write, and then try writing to the block.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Dec 2025 20:17:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2264196#M13924</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-12-16T20:17:19Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2264729#M13926</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;BR /&gt;In the screenshots I sent in the ticket, you can see that in the SET PASSWORD command I used 0x01 for reading and 0x02 for writing. From the tests I ran, only the read command in a read-protected memory region worked. For writing in a write-protected memory region, I used the following commands:&lt;BR /&gt;- SET PASSWORD with password identifier 0x02; this command worked;&lt;BR /&gt;- WRITE in register 0x14, for example; this command returns 0x01 0x0F.&lt;/P&gt;&lt;P&gt;Based on these tests I performed and the register values I sent in my previous reply, can you replicate the same scenario on your end?&lt;BR /&gt;Is there any configuration error in either the register values or the commands?&lt;BR /&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;NSF&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 09:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2264729#M13926</guid>
      <dc:creator>NSF</dc:creator>
      <dc:date>2025-12-17T09:47:15Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2264738#M13927</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Any progress,&amp;nbsp;&lt;SPAN&gt;am having the same problem writing to a password-protected memory region.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 09:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2264738#M13927</guid>
      <dc:creator>BPrada</dc:creator>
      <dc:date>2025-12-17T09:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2265252#M13928</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Try the following sequence:&lt;/P&gt;
&lt;P&gt;- SELECT NTAG&lt;BR /&gt;- Get Random Number&lt;BR /&gt;- SET PASSWORD for PID 01&lt;BR /&gt;- SET PASSWORD for PID 02&lt;BR /&gt;- Write to register 0x14&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 18:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2265252#M13928</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-12-17T18:00:52Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with NTAG protected in NFC side</title>
      <link>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2266887#M13933</link>
      <description>&lt;PRE&gt;&lt;SPAN class=""&gt;Good morning,&lt;BR /&gt;
Yes, we already tested it and it was resolved. 

Thank you very much,&lt;BR /&gt;NSF&lt;/SPAN&gt;&lt;/PRE&gt;</description>
      <pubDate>Fri, 19 Dec 2025 10:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Problem-with-NTAG-protected-in-NFC-side/m-p/2266887#M13933</guid>
      <dc:creator>NSF</dc:creator>
      <dc:date>2025-12-19T10:57:11Z</dc:date>
    </item>
  </channel>
</rss>