<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NTP5332 - Problem with write data to a write-protected block using NFC in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NTP5332-Problem-with-write-data-to-a-write-protected-block-using/m-p/2253216#M13864</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257383"&gt;@GoncaloS&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer the following log to format read and write command:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KaiLi_0-1764682352687.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/368226i91CB79C875F221B8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KaiLi_0-1764682352687.png" alt="KaiLi_0-1764682352687.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Dec 2025 13:32:46 GMT</pubDate>
    <dc:creator>KaiLi</dc:creator>
    <dc:date>2025-12-02T13:32:46Z</dc:date>
    <item>
      <title>NTP5332 - Problem with write data to a write-protected block using NFC</title>
      <link>https://community.nxp.com/t5/NFC/NTP5332-Problem-with-write-data-to-a-write-protected-block-using/m-p/2253152#M13863</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the NXP tag NTP5332 and actually I has problems with commands that are sent via NFC using customized mobile app. Using a microcontroller, I configured the tag with plain password for NFC side. Bellow is possible to see the values of the configuration registers:&lt;/P&gt;&lt;P&gt;0x1037: [0]: 0x09; [1]: 0x00; [2]: 0x5f; [3]: 0x00&lt;BR /&gt;0x103F: [0]: 0x45; [1]: 0x00; [2]: 0xff; [3]: 0xff&lt;BR /&gt;0x1020: [0]: 0x00; [1]: 0x00; [2]: 0x00; [3]: 0x00&lt;BR /&gt;0x1021: [0]: 0x11; [1]: 0x22; [2]: 0x33; [3]: 0x44&lt;BR /&gt;0x1058: [0]: 0x08; [1]: 0x30; [2]: 0x00; [3]: 0x00&lt;BR /&gt;0x100C: [0]: 0x00; [1]: 0x81; [2]: 0x00; [3]: 0x00&lt;/P&gt;&lt;P&gt;I followed the example described in chapter 7.1 Write/Store (derived) PWD using the following sequence:&lt;/P&gt;&lt;P&gt;1. Select Cmd (0x25)&lt;BR /&gt;0x22 | 0x25 | UID&lt;BR /&gt;Result: 0x00&lt;/P&gt;&lt;P&gt;2. Get Random Number (0xB2)&lt;BR /&gt;0x12 0xB2 0x04&lt;BR /&gt;Result: 0x00 0x89 0x45&lt;/P&gt;&lt;P&gt;3. Set Password (0xB3)&lt;BR /&gt;0x12 0xB3 0x04 0x02 0x89 0x45 0x89 0x45 (Write Password: 0x00 0x00 0x00 0x00)&lt;BR /&gt;Result: 0x00&lt;/P&gt;&lt;P&gt;4. Write new PWD&lt;BR /&gt;0x12 0x21 0x14 0x11 0x22 0x33 0x44&lt;BR /&gt;Result: 0x00&lt;/P&gt;&lt;P&gt;5: Write in write protected block&lt;BR /&gt;0x12 0x21 0x14 0x01 0x02 0x03 0x04&lt;BR /&gt;Result: 0x01 0x0F&lt;/P&gt;&lt;P&gt;In the example above that I tested, I was able to write a new password, but the operation of writing data to a write and read-protected block continues to fail. Before this test, I followed steps 1, 2, 3, and 5, but I got the same error. If I replace steps 4 and 5 with a read in a read and write-protected block, I am successful.&lt;BR /&gt;Is the Password identifier 0x02 of the set password command only for writing passwords? If so, shouldn't it also be for writing information in the blocks?&lt;/P&gt;&lt;P&gt;Can anyone help me with these issues? Am I sending the wrong command?&lt;BR /&gt;Thanks for the help!&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;GoncaloS&lt;/P&gt;</description>
      <pubDate>Tue, 02 Dec 2025 12:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTP5332-Problem-with-write-data-to-a-write-protected-block-using/m-p/2253152#M13863</guid>
      <dc:creator>GoncaloS</dc:creator>
      <dc:date>2025-12-02T12:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: NTP5332 - Problem with write data to a write-protected block using NFC</title>
      <link>https://community.nxp.com/t5/NFC/NTP5332-Problem-with-write-data-to-a-write-protected-block-using/m-p/2253216#M13864</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257383"&gt;@GoncaloS&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer the following log to format read and write command:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KaiLi_0-1764682352687.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/368226i91CB79C875F221B8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KaiLi_0-1764682352687.png" alt="KaiLi_0-1764682352687.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Dec 2025 13:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTP5332-Problem-with-write-data-to-a-write-protected-block-using/m-p/2253216#M13864</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-12-02T13:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: NTP5332 - Problem with write data to a write-protected block using NFC</title>
      <link>https://community.nxp.com/t5/NFC/NTP5332-Problem-with-write-data-to-a-write-protected-block-using/m-p/2253309#M13867</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205266" target="_blank"&gt;@KaiLi&lt;/A&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In my side, I tested the commands that you sent and worked.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What do I need to do now?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;GoncaloS&lt;BR /&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Media.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/368250iFF0501554DAFFED4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Media.jpg" alt="Media.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Dec 2025 15:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTP5332-Problem-with-write-data-to-a-write-protected-block-using/m-p/2253309#M13867</guid>
      <dc:creator>GoncaloS</dc:creator>
      <dc:date>2025-12-02T15:15:46Z</dc:date>
    </item>
  </channel>
</rss>