<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CLRC663 - Active Antenna Concept in NFC</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-Active-Antenna-Concept/m-p/2250497#M13849</link>
    <description>&lt;P&gt;For validation of my digital block Analog Front End of CLRC663 is to be bypassed for that I want to use Active Antenna Concept as mentioned in "&lt;EM&gt;CLRC663&lt;BR /&gt;High performance multi-protocol NFC frontend CLRC663 and CLRC663 plus&lt;BR /&gt;Rev. 5.3 — 3 January 2024".&amp;nbsp;&lt;BR /&gt;&lt;/EM&gt;&lt;BR /&gt;I am using CLEV663B and configured it as reader for ISO/IEC 14443B using NFC Cockpit. After sending REQB it expects a response from PICC. Bypassing the Analog RF, "Rcv.SigInSe = 11" indicates I can drive SIGIN pin over s3c generic.&lt;BR /&gt;&lt;BR /&gt;Now, I want to know what is meant by s3c generic, and what is expected as an input to this pin. Baseband signal (@106KHz) or BPSK modulates sub-carrier signal. Also, do I just need to transmit characters/data bytes or add SOF and EOF. Does my input signal needs to be synchronized with RF of antenna.&lt;/P&gt;</description>
    <pubDate>Thu, 27 Nov 2025 17:09:05 GMT</pubDate>
    <dc:creator>lokeshjassal2004</dc:creator>
    <dc:date>2025-11-27T17:09:05Z</dc:date>
    <item>
      <title>CLRC663 - Active Antenna Concept</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Active-Antenna-Concept/m-p/2250497#M13849</link>
      <description>&lt;P&gt;For validation of my digital block Analog Front End of CLRC663 is to be bypassed for that I want to use Active Antenna Concept as mentioned in "&lt;EM&gt;CLRC663&lt;BR /&gt;High performance multi-protocol NFC frontend CLRC663 and CLRC663 plus&lt;BR /&gt;Rev. 5.3 — 3 January 2024".&amp;nbsp;&lt;BR /&gt;&lt;/EM&gt;&lt;BR /&gt;I am using CLEV663B and configured it as reader for ISO/IEC 14443B using NFC Cockpit. After sending REQB it expects a response from PICC. Bypassing the Analog RF, "Rcv.SigInSe = 11" indicates I can drive SIGIN pin over s3c generic.&lt;BR /&gt;&lt;BR /&gt;Now, I want to know what is meant by s3c generic, and what is expected as an input to this pin. Baseband signal (@106KHz) or BPSK modulates sub-carrier signal. Also, do I just need to transmit characters/data bytes or add SOF and EOF. Does my input signal needs to be synchronized with RF of antenna.&lt;/P&gt;</description>
      <pubDate>Thu, 27 Nov 2025 17:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Active-Antenna-Concept/m-p/2250497#M13849</guid>
      <dc:creator>lokeshjassal2004</dc:creator>
      <dc:date>2025-11-27T17:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 - Active Antenna Concept</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Active-Antenna-Concept/m-p/2251441#M13855</link>
      <description>&lt;P&gt;We don't use the&amp;nbsp;&lt;SPAN&gt;s3c generic. It is an internal signal of process unit.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 29 Nov 2025 07:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Active-Antenna-Concept/m-p/2251441#M13855</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-11-29T07:14:07Z</dc:date>
    </item>
  </channel>
</rss>