<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NHS3100 WLCSP25 PACKAGE ISSUE in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NHS3100-WLCSP25-PACKAGE-ISSUE/m-p/2248189#M13837</link>
    <description>&lt;P&gt;We're developing using the NHS3100.&lt;BR /&gt;We're using the WLCSP25 package IC, and while downloading is possible, we can't find the START POINT in debug mode.&lt;/P&gt;&lt;P&gt;Are there any additional settings we need to make in the SDK file when applying the WLCSP25 package?&lt;/P&gt;</description>
    <pubDate>Tue, 25 Nov 2025 08:51:45 GMT</pubDate>
    <dc:creator>SANGHWAN</dc:creator>
    <dc:date>2025-11-25T08:51:45Z</dc:date>
    <item>
      <title>NHS3100 WLCSP25 PACKAGE ISSUE</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-WLCSP25-PACKAGE-ISSUE/m-p/2248189#M13837</link>
      <description>&lt;P&gt;We're developing using the NHS3100.&lt;BR /&gt;We're using the WLCSP25 package IC, and while downloading is possible, we can't find the START POINT in debug mode.&lt;/P&gt;&lt;P&gt;Are there any additional settings we need to make in the SDK file when applying the WLCSP25 package?&lt;/P&gt;</description>
      <pubDate>Tue, 25 Nov 2025 08:51:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-WLCSP25-PACKAGE-ISSUE/m-p/2248189#M13837</guid>
      <dc:creator>SANGHWAN</dc:creator>
      <dc:date>2025-11-25T08:51:45Z</dc:date>
    </item>
  </channel>
</rss>