<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NTAG5 Link: Single SRAM Block Write Not Triggering I2C Master Read - Full SRAM Write Works in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NTAG5-Link-Single-SRAM-Block-Write-Not-Triggering-I2C-Master/m-p/2247791#M13836</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257240"&gt;@kavya_ap&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;There may not be a direct implementation to trigger ED pin on single SRAM block write. As you mention, pass-through mode expects SRAM write from 00h to 3Fh in order to trigger ED pin, as depicted in &lt;A href="https://www.nxp.com/docs/en/application-note/AN12364.pdf" target="_blank"&gt;NTAG 5 - Bidirectional data exchange&lt;/A&gt;, Figure 1.&lt;/P&gt;
&lt;P&gt;For proper pass-through implementation, please stick to the procedures and recommendations described in &lt;A href="https://www.nxp.com/docs/en/application-note/AN12364.pdf" target="_blank"&gt;NTAG 5 - Bidirectional data exchange&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Mon, 24 Nov 2025 22:57:25 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2025-11-24T22:57:25Z</dc:date>
    <item>
      <title>NTAG5 Link: Single SRAM Block Write Not Triggering I2C Master Read - Full SRAM Write Works</title>
      <link>https://community.nxp.com/t5/NFC/NTAG5-Link-Single-SRAM-Block-Write-Not-Triggering-I2C-Master/m-p/2247386#M13834</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;I'm implementing&amp;nbsp; pass-through application using NTAG5 Link (NTP53x2). The system writes small configuration data blocks to SRAM via NFC and reads them via I2C on an embedded MCU.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;Current Findings:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P class=""&gt;Single SRAM block write:&amp;nbsp;ED pin does not trigger because it's not the last byte of the 256-byte SRAM&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Full SRAM write:&amp;nbsp;Works reliably - ED pin triggers and I2C master can read the data&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P class=""&gt;Workaround attempted:&amp;nbsp;Configured ED pin with&amp;nbsp;ED_CONFIG = 1100b (trigger on SYNCH_BLOCK write) and set the target data block as the SYNCH_DATA_BLOCK -&amp;nbsp;still no result.&lt;/P&gt;&lt;P class=""&gt;Is there a configuration method in NTAG5 Link that allows the ED pin to reliably trigger on a&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;single SRAM block write without requiring the entire SRAM to be written? If not, what is the recommended approach for efficient small-data transfers in pass-through mode?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Nov 2025 12:18:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG5-Link-Single-SRAM-Block-Write-Not-Triggering-I2C-Master/m-p/2247386#M13834</guid>
      <dc:creator>kavya_ap</dc:creator>
      <dc:date>2025-11-24T12:18:57Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG5 Link: Single SRAM Block Write Not Triggering I2C Master Read - Full SRAM Write Works</title>
      <link>https://community.nxp.com/t5/NFC/NTAG5-Link-Single-SRAM-Block-Write-Not-Triggering-I2C-Master/m-p/2247791#M13836</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/257240"&gt;@kavya_ap&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;There may not be a direct implementation to trigger ED pin on single SRAM block write. As you mention, pass-through mode expects SRAM write from 00h to 3Fh in order to trigger ED pin, as depicted in &lt;A href="https://www.nxp.com/docs/en/application-note/AN12364.pdf" target="_blank"&gt;NTAG 5 - Bidirectional data exchange&lt;/A&gt;, Figure 1.&lt;/P&gt;
&lt;P&gt;For proper pass-through implementation, please stick to the procedures and recommendations described in &lt;A href="https://www.nxp.com/docs/en/application-note/AN12364.pdf" target="_blank"&gt;NTAG 5 - Bidirectional data exchange&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Nov 2025 22:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG5-Link-Single-SRAM-Block-Write-Not-Triggering-I2C-Master/m-p/2247791#M13836</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-11-24T22:57:25Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG5 Link: Single SRAM Block Write Not Triggering I2C Master Read - Full SRAM Write Works</title>
      <link>https://community.nxp.com/t5/NFC/NTAG5-Link-Single-SRAM-Block-Write-Not-Triggering-I2C-Master/m-p/2253016#M13861</link>
      <description>Thank you so much.</description>
      <pubDate>Tue, 02 Dec 2025 09:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG5-Link-Single-SRAM-Block-Write-Not-Triggering-I2C-Master/m-p/2253016#M13861</guid>
      <dc:creator>kavya_ap</dc:creator>
      <dc:date>2025-12-02T09:04:59Z</dc:date>
    </item>
  </channel>
</rss>