<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN7462AU: USB CCID composite device for Windows</title>
    <link>https://community.nxp.com/t5/NFC/PN7462AU-USB-CCID-composite-device-for-Windows/m-p/2178040#M13662</link>
    <description>&lt;P&gt;Unfortunately, there is no examples&lt;/P&gt;</description>
    <pubDate>Tue, 30 Sep 2025 08:51:31 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2025-09-30T08:51:31Z</dc:date>
    <item>
      <title>PN7462AU: USB CCID composite device for Windows</title>
      <link>https://community.nxp.com/t5/NFC/PN7462AU-USB-CCID-composite-device-for-Windows/m-p/2174839#M13640</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Our company has developed a smartcard reader based on the NXP PN7462AU:&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;One contactless customer card and two contact SAM slots&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;USB CCID connection to a Windows host&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN&gt;Unfortunately the build in Windows CCID driver supports only one card slot 0 and there is no access to the other slots.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Does anyone have any ideas on how to overcome this limitation?&lt;/P&gt;&lt;P&gt;One idea I have is to build a USB composite device with two CCID devices one for the contactless customer card and the other for one SAM slot.&lt;/P&gt;&lt;P&gt;Is there any example for such an USB composite device with the PN7462AU?&lt;/P&gt;&lt;P&gt;I'm not the first to ask that question but I don't think the given &lt;SPAN&gt;ExamplesPN7462AU\phExNFCCcid solves my issue&lt;/SPAN&gt;:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/8-bit-Microcontrollers/pn7462-dual-ccid-example-soure-code/m-p/1668061" target="_blank"&gt;pn7462 dual ccid example soure code - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help and ideas,&lt;/P&gt;&lt;P&gt;Bernd&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 07:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462AU-USB-CCID-composite-device-for-Windows/m-p/2174839#M13640</guid>
      <dc:creator>Blk_Init</dc:creator>
      <dc:date>2025-09-24T07:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462AU: USB CCID composite device for Windows</title>
      <link>https://community.nxp.com/t5/NFC/PN7462AU-USB-CCID-composite-device-for-Windows/m-p/2178040#M13662</link>
      <description>&lt;P&gt;Unfortunately, there is no examples&lt;/P&gt;</description>
      <pubDate>Tue, 30 Sep 2025 08:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462AU-USB-CCID-composite-device-for-Windows/m-p/2178040#M13662</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-09-30T08:51:31Z</dc:date>
    </item>
  </channel>
</rss>