<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN7642 - Initial Calibration in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2174133#M13631</link>
    <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205266"&gt;@KaiLi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thanks for replying.&lt;/P&gt;&lt;P&gt;Yes, i have the SDK. So with flashing an example its calibrated?&lt;BR /&gt;I looked for the definitions of the Registers in some examples and also in the API Reference Manual.&amp;nbsp;&lt;BR /&gt;I don´t see them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe my question was a bit unclear.&lt;BR /&gt;I want to know, what i have to write into&amp;nbsp;REGISTER TX_NOV_CALIBRATE_AND_STORE_VAL_REG.&lt;BR /&gt;Cause there is no further explanation. Its 2 bit r/w register. What happens if i write 0x1, 0x2 or 0x3 into it?&lt;/P&gt;&lt;P&gt;NOV_CONFIG_CAL is clear. First write 0x01 for cold boot FW calibration and after succesfull calibration write 0x02 to reference to NOV_CAL_VAL1 and 2.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
    <pubDate>Tue, 23 Sep 2025 08:39:35 GMT</pubDate>
    <dc:creator>MPEngineering</dc:creator>
    <dc:date>2025-09-23T08:39:35Z</dc:date>
    <item>
      <title>PN7642 - Initial Calibration</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2173493#M13622</link>
      <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;i have a custom PCB with PN7642.&lt;/P&gt;&lt;P&gt;The Datasheet says, that before turning on the RF part, an initial calibration needs to be done.&lt;/P&gt;&lt;P&gt;Is there any further documentation about this than:&lt;/P&gt;&lt;P&gt;1. Write EEPROM configuration NOV_CFG_CAL.&lt;BR /&gt;2. Write REGISTER TX_NOV_CALIBRATE_AND_STORE_VAL_REG.&lt;BR /&gt;3. Write EEPROM configuration NOV_CFG_CAL.?&lt;/P&gt;&lt;P&gt;Which values should be set?&lt;/P&gt;&lt;P&gt;Thank for helping.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 10:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2173493#M13622</guid>
      <dc:creator>MPEngineering</dc:creator>
      <dc:date>2025-09-22T10:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 - Initial Calibration</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2173898#M13626</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248495"&gt;@MPEngineering&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It's recommended that you can run SDK the example&lt;/P&gt;
&lt;P&gt;log in:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/PN7642" target="_blank"&gt;Best-in-Class NFC Frontend with Integrated MCU | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and download:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KaiLi_0-1758595034002.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358056i796E39F3F857D9C8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KaiLi_0-1758595034002.png" alt="KaiLi_0-1758595034002.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;KaiLi_0-1758595034002.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 02:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2173898#M13626</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-09-23T02:38:52Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 - Initial Calibration</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2174133#M13631</link>
      <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205266"&gt;@KaiLi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thanks for replying.&lt;/P&gt;&lt;P&gt;Yes, i have the SDK. So with flashing an example its calibrated?&lt;BR /&gt;I looked for the definitions of the Registers in some examples and also in the API Reference Manual.&amp;nbsp;&lt;BR /&gt;I don´t see them.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe my question was a bit unclear.&lt;BR /&gt;I want to know, what i have to write into&amp;nbsp;REGISTER TX_NOV_CALIBRATE_AND_STORE_VAL_REG.&lt;BR /&gt;Cause there is no further explanation. Its 2 bit r/w register. What happens if i write 0x1, 0x2 or 0x3 into it?&lt;/P&gt;&lt;P&gt;NOV_CONFIG_CAL is clear. First write 0x01 for cold boot FW calibration and after succesfull calibration write 0x02 to reference to NOV_CAL_VAL1 and 2.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 08:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2174133#M13631</guid>
      <dc:creator>MPEngineering</dc:creator>
      <dc:date>2025-09-23T08:39:35Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 - Initial Calibration</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2174760#M13639</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248495"&gt;@MPEngineering&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This part should be encapsulated, and recommends to run the project:&lt;/P&gt;
&lt;P&gt;PN7642_MCUXpresso_SDK_02-15-003_PUB\boards\pnev7642fama\nfc_examples\pub\NFC_Config, and select "&lt;SPAN&gt;RFLD_NFCLD_CONFIG"&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KaiLi_0-1758693133679.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/358267i2EEC173A3CA4E357/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KaiLi_0-1758693133679.png" alt="KaiLi_0-1758693133679.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;KaiLi_0-1758693133679.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;After that, the device can be initialized and calibrated.&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 05:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Initial-Calibration/m-p/2174760#M13639</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-09-24T05:56:12Z</dc:date>
    </item>
  </channel>
</rss>