<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: AN12365 - High field strength mode</title>
    <link>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136802#M13433</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250984"&gt;@TheQuux&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;The High Field Strength optimization requires an industrial or specially designed VCD/Reader, while PN5190 is an NFC Reader with relatively low power output.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Fri, 18 Jul 2025 22:22:54 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2025-07-18T22:22:54Z</dc:date>
    <item>
      <title>AN12365 - High field strength mode</title>
      <link>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136669#M13432</link>
      <description>&lt;P&gt;In AN12365, Table 2, there is reference to &amp;gt; 20 mW energy harvesting being possible when in high field strength mode.&lt;/P&gt;&lt;P&gt;I've done this, and am not getting more than 20 mW, and I'm wondering if I need to do something to configure the modulation scheme?&lt;/P&gt;&lt;P&gt;I'm using a NXP5190 (PNEV5190BP eval board) with the reader library to talk to the NTAG5332 on a OM2NTP5332 eval board.&lt;/P&gt;&lt;P&gt;I'm not seeing any information on how the 5190 must be configured in order for this to work. Is there some information that shows how to do this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jul 2025 15:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136669#M13432</guid>
      <dc:creator>TheQuux</dc:creator>
      <dc:date>2025-07-18T15:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: AN12365 - High field strength mode</title>
      <link>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136802#M13433</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/250984"&gt;@TheQuux&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;The High Field Strength optimization requires an industrial or specially designed VCD/Reader, while PN5190 is an NFC Reader with relatively low power output.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jul 2025 22:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136802#M13433</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-07-18T22:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: AN12365 - High field strength mode</title>
      <link>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136804#M13434</link>
      <description>&lt;P&gt;Eduardo,&lt;/P&gt;&lt;P&gt;The app note says this:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Energy harvesting optimized for high field strength - if expected VCDs be able to output&lt;BR /&gt;more strong field (e.g. specially designed VCDs). The high field strength mode can&lt;BR /&gt;drive higher power and also supports a VCD with 10 % modulation index next to the&lt;BR /&gt;100 % ASK modulation scheme.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Is the 5190 at least not capable of being configured to this modulation scheme? If you must use a special VCD, is there an example of what that looks like? Perhaps a reference design or something? What sort of field strength must it present in order to enable the higher harvesting amount?&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jul 2025 22:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136804#M13434</guid>
      <dc:creator>TheQuux</dc:creator>
      <dc:date>2025-07-18T22:30:19Z</dc:date>
    </item>
    <item>
      <title>Re: AN12365 - High field strength mode</title>
      <link>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136820#M13436</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;This tag that can be powered by an NFC-enabled device at close range and by an ISO/IEC 15693-enabled industrial reader over a longer range.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;PN5190 is an NFC Forum compliant device, for this reason, it is designed to achieve a reading distance of up to ~10cm depending i.e. on antenna design. While&amp;nbsp;ISO/IEC 15693 should allow a longer operating distance, our NFC Readers cannot achieve this distance.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;As mentioned, an ISO/IEC 15693-enabled, powerful industrial reader would be required for High Field Strength configuration; however, we may not have any product that meet your needs in our portfolio.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 19 Jul 2025 01:37:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/AN12365-High-field-strength-mode/m-p/2136820#M13436</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-07-19T01:37:14Z</dc:date>
    </item>
  </channel>
</rss>