<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: CLRC663 layout on a multilayer stack</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-layout-on-a-multilayer-stack/m-p/2134896#M13410</link>
    <description>&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;Firstly thanks for your response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If below the matching circuit I place a GND plane for EMI control , is it necessary to remove the copper area in the rest of the layers?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my case I am using a 6 layers stack, if the matching is in the first layer and the GND in the second I think that I shouldn't remove the copper on the other four layers. The demo board is not made in that way and I cannot understand why.&lt;/P&gt;&lt;P&gt;Any idea about the best procedure?&lt;/P&gt;&lt;P&gt;Thanks to all&amp;nbsp;&lt;/P&gt;&lt;P&gt;david&lt;/P&gt;</description>
    <pubDate>Wed, 16 Jul 2025 09:56:36 GMT</pubDate>
    <dc:creator>dramos</dc:creator>
    <dc:date>2025-07-16T09:56:36Z</dc:date>
    <item>
      <title>CLRC663 layout on a multilayer stack</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-layout-on-a-multilayer-stack/m-p/2134664#M13406</link>
      <description>&lt;P&gt;Hi to all,&lt;/P&gt;&lt;P&gt;I am designing a 6 layer pcb with the #CLRC663. After reading the Application Note AN11019 (rev 1.5), in the chapter 3.2 Layout recommendation there is a mention about the GND plane under the&amp;nbsp;CLRC663 evaluation board. The GND plane is in middle layer of the board&lt;/P&gt;&lt;P&gt;On the SW4301 - CLEV6630B v2.0 PCB,there is not copper under the matching circuitry.&amp;nbsp;&lt;/P&gt;&lt;P&gt;As I mentioned before, I have a multilayer board and I would like to know if I can place a GND plane under the matching components (Matching components Layer1-GND Layer2). Can I have traces under the matching components in the other layers? For example layer 3 or Layer 6?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Or should I remove all the copper under the matching components in all layers of my stack?&lt;/P&gt;&lt;P&gt;Thanks for your comments.&lt;/P&gt;&lt;P&gt;david&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 05:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-layout-on-a-multilayer-stack/m-p/2134664#M13406</guid>
      <dc:creator>dramos</dc:creator>
      <dc:date>2025-07-16T05:47:40Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 layout on a multilayer stack</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-layout-on-a-multilayer-stack/m-p/2134672#M13407</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252738"&gt;@dramos&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We typically keep a first GND layer under matching as shown below. This is mainly due to EMI reasons.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="matching_GND.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/347776i50D5E4F87055BF63/image-size/medium?v=v2&amp;amp;px=400" role="button" title="matching_GND.jpg" alt="matching_GND.jpg" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 06:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-layout-on-a-multilayer-stack/m-p/2134672#M13407</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2025-07-16T06:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 layout on a multilayer stack</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-layout-on-a-multilayer-stack/m-p/2134896#M13410</link>
      <description>&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;Firstly thanks for your response.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If below the matching circuit I place a GND plane for EMI control , is it necessary to remove the copper area in the rest of the layers?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In my case I am using a 6 layers stack, if the matching is in the first layer and the GND in the second I think that I shouldn't remove the copper on the other four layers. The demo board is not made in that way and I cannot understand why.&lt;/P&gt;&lt;P&gt;Any idea about the best procedure?&lt;/P&gt;&lt;P&gt;Thanks to all&amp;nbsp;&lt;/P&gt;&lt;P&gt;david&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 09:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-layout-on-a-multilayer-stack/m-p/2134896#M13410</guid>
      <dc:creator>dramos</dc:creator>
      <dc:date>2025-07-16T09:56:36Z</dc:date>
    </item>
  </channel>
</rss>