<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN5190 DPC calibration</title>
    <link>https://community.nxp.com/t5/NFC/PN5190-DPC-calibration/m-p/2130329#M13380</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178677"&gt;@sinu52&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;The target power transfer of 5.3 V with TestPICC1 is only one example, typically it makes sense to use values around 5.5V. The limits are defined by EMVCo specification.&lt;/P&gt;
&lt;P&gt;I will recommend you taking a look at the &lt;A href="https://www.nxp.com/design/design-center/training/TIP-PN5190-DYNAMIC-POWER-CONTROL-DEMO" target="_blank"&gt;PN5190 Dynamic Power Control Quick Calibration and TxShaping Demo | NXP Semiconductors&lt;/A&gt;. This training series demonstrates a quick calibration of the PN5190 DPC by using NFC Cockpit and an EMVCo test setup to measure the power transfer to perform the compliance tests.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Tue, 08 Jul 2025 18:04:50 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2025-07-08T18:04:50Z</dc:date>
    <item>
      <title>PN5190 DPC calibration</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-DPC-calibration/m-p/2129824#M13379</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am in the process of calibrating the DPC of the PN5190B2.&lt;/P&gt;&lt;P&gt;I have purchased an Reference PICC 1,2,3 card.&lt;/P&gt;&lt;P&gt;When reading through AN12549 it states at page 66 that:&lt;/P&gt;&lt;P&gt;"The target for the DPC calibration shall be the power transfer: here the value of 5.3 V is chosen. The value of 5.3 V is somewhere in the center range between the allowed minimum and maximum power transfer."&lt;/P&gt;&lt;P&gt;How do i determine the center voltage value of allowed power transfer in my specific case and where do i find the allowed minimum and maximum power transfer for PICC 1,2,3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards Remco&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 06:12:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-DPC-calibration/m-p/2129824#M13379</guid>
      <dc:creator>sinu52</dc:creator>
      <dc:date>2025-07-08T06:12:30Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 DPC calibration</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-DPC-calibration/m-p/2130329#M13380</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/178677"&gt;@sinu52&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;The target power transfer of 5.3 V with TestPICC1 is only one example, typically it makes sense to use values around 5.5V. The limits are defined by EMVCo specification.&lt;/P&gt;
&lt;P&gt;I will recommend you taking a look at the &lt;A href="https://www.nxp.com/design/design-center/training/TIP-PN5190-DYNAMIC-POWER-CONTROL-DEMO" target="_blank"&gt;PN5190 Dynamic Power Control Quick Calibration and TxShaping Demo | NXP Semiconductors&lt;/A&gt;. This training series demonstrates a quick calibration of the PN5190 DPC by using NFC Cockpit and an EMVCo test setup to measure the power transfer to perform the compliance tests.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 18:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-DPC-calibration/m-p/2130329#M13380</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-07-08T18:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 DPC calibration</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-DPC-calibration/m-p/2157589#M13551</link>
      <description>&lt;P&gt;Currently I am trying to get the PN5190’s DPC calibrated. I purchased a set of PICC reference cards. &lt;A href="https://www.comprion.com/shop/iso-10373-6-test-picc-class-1-6.html" target="_blank"&gt;https://www.comprion.com/shop/iso-10373-6-test-picc-class-1-6.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I matched my antenna to ~16.5R (See the added smith chart).&lt;/P&gt;&lt;P&gt;The target current in unloaded condition is set to 246mA this is the maximum I am getting. (I would expect this to be much higher around 5.7V/16.5R ~345mA)&lt;/P&gt;&lt;P&gt;I now encounter the issue that when I am trying to read an NXP desfire EV1 card without the DPC calibrated I am getting 7.5 cm detection and 5.5cm read distance.&lt;/P&gt;&lt;P&gt;However with the DPC calibrated I only get 3.8cm detection and 2.3cm read distance. I would prefer it to have more read range. Is this to be expected or am I doing something wrong during calibration?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="matching result on A0.5.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353947i02519AF78769CB24/image-size/medium?v=v2&amp;amp;px=400" role="button" title="matching result on A0.5.PNG" alt="matching result on A0.5.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 13:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-DPC-calibration/m-p/2157589#M13551</guid>
      <dc:creator>sinu52</dc:creator>
      <dc:date>2025-08-25T13:40:44Z</dc:date>
    </item>
  </channel>
</rss>