<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックabout pn532 Card Emulation</title>
    <link>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2128851#M13367</link>
    <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;about pn532 Card Emulation&lt;/P&gt;&lt;P&gt;It is found that the frequency of Crystal oscillator will shift due to the temperature of the environment.&lt;/P&gt;&lt;P&gt;However, the offset is within the range specified in iso 14443, and the frequency of the card reader through the test is 13.565MHZ.&lt;/P&gt;&lt;P&gt;At this frequency offset, the card simulation mode is used.&lt;/P&gt;&lt;P&gt;I Would like to ask about the frequency of card simulation mode is using itself osc?&lt;/P&gt;&lt;P&gt;Or will the antenna get the frequency sent by the card reader?&lt;/P&gt;&lt;P&gt;Will card simulation mode have compatibility problems when using 13.565MHZ?&lt;/P&gt;</description>
    <pubDate>Sat, 05 Jul 2025 23:43:28 GMT</pubDate>
    <dc:creator>smartmx</dc:creator>
    <dc:date>2025-07-05T23:43:28Z</dc:date>
    <item>
      <title>about pn532 Card Emulation</title>
      <link>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2128851#M13367</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;about pn532 Card Emulation&lt;/P&gt;&lt;P&gt;It is found that the frequency of Crystal oscillator will shift due to the temperature of the environment.&lt;/P&gt;&lt;P&gt;However, the offset is within the range specified in iso 14443, and the frequency of the card reader through the test is 13.565MHZ.&lt;/P&gt;&lt;P&gt;At this frequency offset, the card simulation mode is used.&lt;/P&gt;&lt;P&gt;I Would like to ask about the frequency of card simulation mode is using itself osc?&lt;/P&gt;&lt;P&gt;Or will the antenna get the frequency sent by the card reader?&lt;/P&gt;&lt;P&gt;Will card simulation mode have compatibility problems when using 13.565MHZ?&lt;/P&gt;</description>
      <pubDate>Sat, 05 Jul 2025 23:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2128851#M13367</guid>
      <dc:creator>smartmx</dc:creator>
      <dc:date>2025-07-05T23:43:28Z</dc:date>
    </item>
    <item>
      <title>Re: about pn532 Card Emulation</title>
      <link>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2128877#M13370</link>
      <description>&lt;P&gt;PCD:&amp;nbsp; &amp;nbsp; 13.553Mhz&lt;/P&gt;&lt;P&gt;PICC:&amp;nbsp; &amp;nbsp;13.567Mhz&lt;/P&gt;&lt;P&gt;Can the card reader communicate with the card successfully?&lt;/P&gt;</description>
      <pubDate>Sun, 06 Jul 2025 23:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2128877#M13370</guid>
      <dc:creator>smartmx</dc:creator>
      <dc:date>2025-07-06T23:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: about pn532 Card Emulation</title>
      <link>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2129686#M13376</link>
      <description>&lt;P&gt;Would like to ask about the frequency of card simulation mode is using itself osc?&lt;/P&gt;
&lt;P&gt;-&amp;gt; Yes,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Or will the antenna get the frequency sent by the card reader?&lt;/P&gt;
&lt;P&gt;-&amp;gt; No.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Will card simulation mode have compatibility problems when using 13.565MHZ?&lt;/P&gt;
&lt;P&gt;-&amp;gt;&amp;nbsp;Minor frequency shifts&amp;nbsp;are&amp;nbsp;not typically a problem.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 02:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2129686#M13376</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-07-08T02:29:00Z</dc:date>
    </item>
    <item>
      <title>Re: about pn532 Card Emulation</title>
      <link>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2129691#M13377</link>
      <description>thanks for your help !</description>
      <pubDate>Tue, 08 Jul 2025 02:36:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2129691#M13377</guid>
      <dc:creator>smartmx</dc:creator>
      <dc:date>2025-07-08T02:36:23Z</dc:date>
    </item>
    <item>
      <title>Re: about pn532 Card Emulation</title>
      <link>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2139119#M13454</link>
      <description>&lt;P&gt;Hi, jimmychan:&lt;BR /&gt;After my testing of different phones during this time. The general information is summarized as follows:&lt;BR /&gt;1. The NFC chip of the NXP series can read PN532 working at 13.565Mhz normally.&lt;BR /&gt;2. The NFC chip of the ST series can read PN532 working at 13.565Mhz normally.&lt;BR /&gt;3. Samsung Electronics' NFC chips (like: S3NSN4V S3NRN4V) cannot read PN532 at 13.565Mhz normally, but it can obtain the card number and complete the anti-collision process.&lt;BR /&gt;Can you give some suggestions to solve the compatibility problem caused by this frequency offset?&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jul 2025 07:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/about-pn532-Card-Emulation/m-p/2139119#M13454</guid>
      <dc:creator>smartmx</dc:creator>
      <dc:date>2025-07-23T07:49:36Z</dc:date>
    </item>
  </channel>
</rss>