<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN7642 DPC in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2126639#M13343</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248495"&gt;@MPEngineering&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;If you already performed a symmetric antenna tuning, you can configure the DPC. DPC can operate in current limiting + current reduction mode. Current reduction is achieved by lowering the transmitter supply voltage, allowing the optimization of power transfer.&lt;/P&gt;
&lt;P&gt;Also, please take a look at &lt;A href="https://www.nxp.com/docs/en/application-note/AN13996.pdf" target="_blank"&gt;How to use the low-power features of the PN76 family NFC controller&lt;/A&gt;. This App Note explains how to use different low-power modes on PN76 family, including LPCD and ULPCD.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Jul 2025 21:09:16 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2025-07-01T21:09:16Z</dc:date>
    <item>
      <title>PN7642 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2126326#M13340</link>
      <description>&lt;P&gt;Hey there,&lt;/P&gt;&lt;P&gt;currently I´m designing a new PCB with the PN7642.&lt;/P&gt;&lt;P&gt;As far as i know, new values for DPC (LUT) control have to be written, when using your own antenna.&lt;/P&gt;&lt;P&gt;But in my case, i want to decrease power consumption. The only goal should be, to detect Mifare DESFire (EV1 - 3) safe, within a distance of 1 - 2 cm.&lt;/P&gt;&lt;P&gt;Should i disable DPC and change the impedance of the Antenna, or is it more useful to calibrate the Antenna with NFC Cockpit, enable DPC and set the Gear Level to a fixed value (Antenna design like suggested in AN´s)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for replying.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jul 2025 09:54:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2126326#M13340</guid>
      <dc:creator>MPEngineering</dc:creator>
      <dc:date>2025-07-01T09:54:12Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2126639#M13343</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248495"&gt;@MPEngineering&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;If you already performed a symmetric antenna tuning, you can configure the DPC. DPC can operate in current limiting + current reduction mode. Current reduction is achieved by lowering the transmitter supply voltage, allowing the optimization of power transfer.&lt;/P&gt;
&lt;P&gt;Also, please take a look at &lt;A href="https://www.nxp.com/docs/en/application-note/AN13996.pdf" target="_blank"&gt;How to use the low-power features of the PN76 family NFC controller&lt;/A&gt;. This App Note explains how to use different low-power modes on PN76 family, including LPCD and ULPCD.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jul 2025 21:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2126639#M13343</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-07-01T21:09:16Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2127244#M13344</link>
      <description>&lt;P&gt;Hey Eduardo,&lt;/P&gt;&lt;P&gt;thanks for replying.&lt;/P&gt;&lt;P&gt;In my case i dont want to use LPCD or ULPCD. The IC should always be sleeping or powered off, till a button is pressed.&lt;/P&gt;&lt;P&gt;Then poll for a card, interact and sleep again without card detection function.&lt;/P&gt;&lt;P&gt;But if there is a current limiting/reduction mode, it should be simple to reduce Transmitter Power to a level, where safe detection (1 - 2cm) is achieved, isnt´t it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 11:55:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2127244#M13344</guid>
      <dc:creator>MPEngineering</dc:creator>
      <dc:date>2025-07-02T11:55:04Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2127578#M13347</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248495"&gt;@MPEngineering&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;In addition to a wake-up due to an object detected in the proximity of the reader, ULPCD allows the usage of a GPIO (GPIO 3) to abort ULPCD from an external source. This is described in &lt;A href="https://www.nxp.com/docs/en/application-note/AN13996.pdf" target="_blank"&gt;How to use the low-power features of the PN76 family NFC controller&lt;/A&gt;, Section 2.3.2.1. Would you consider this approach?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 21:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-DPC/m-p/2127578#M13347</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-07-02T21:21:57Z</dc:date>
    </item>
  </channel>
</rss>