<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Implementing smart lock with PN7161 for Apple Wallet in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Implementing-smart-lock-with-PN7161-for-Apple-Wallet/m-p/2101714#M13209</link>
    <description>&lt;DIV&gt;&lt;DIV class=""&gt;&lt;P class=""&gt;Hello NXP Community,&lt;/P&gt;&lt;P class=""&gt;We're working with a lock manufacturer to develop a smart lock that can be unlocked via smartphone wallet applications (both iOS and Android). Our current plan centers around using the NXP PN7161 NFC controller, which has&amp;nbsp;"Enhanced Contactless Polling" (ECP) by Apple.&lt;/P&gt;&lt;P class=""&gt;We're in the early exploratory phase and trying to understand the full stack of technology requirements, certifications needed, and associated costs before making final design decisions.&lt;BR /&gt;&lt;BR /&gt;For the Apple integration, the workflow isn't so clear to us, and we have the following questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Does using the PN7161 still require MFi certification?&lt;/LI&gt;&lt;LI&gt;Do we need to join Apple's VAS program separately?&lt;/LI&gt;&lt;LI&gt;Are there other certificates/programs that we must join?&lt;/LI&gt;&lt;LI&gt;What are the associated costs? (type of costs, recurring, one time, ...)&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;Any guidance, documentation links, or suggestions would be greatly appreciated!&lt;/P&gt;&lt;P class=""&gt;Thank you,&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Wed, 21 May 2025 14:34:42 GMT</pubDate>
    <dc:creator>Geiger8759</dc:creator>
    <dc:date>2025-05-21T14:34:42Z</dc:date>
    <item>
      <title>Implementing smart lock with PN7161 for Apple Wallet</title>
      <link>https://community.nxp.com/t5/NFC/Implementing-smart-lock-with-PN7161-for-Apple-Wallet/m-p/2101714#M13209</link>
      <description>&lt;DIV&gt;&lt;DIV class=""&gt;&lt;P class=""&gt;Hello NXP Community,&lt;/P&gt;&lt;P class=""&gt;We're working with a lock manufacturer to develop a smart lock that can be unlocked via smartphone wallet applications (both iOS and Android). Our current plan centers around using the NXP PN7161 NFC controller, which has&amp;nbsp;"Enhanced Contactless Polling" (ECP) by Apple.&lt;/P&gt;&lt;P class=""&gt;We're in the early exploratory phase and trying to understand the full stack of technology requirements, certifications needed, and associated costs before making final design decisions.&lt;BR /&gt;&lt;BR /&gt;For the Apple integration, the workflow isn't so clear to us, and we have the following questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Does using the PN7161 still require MFi certification?&lt;/LI&gt;&lt;LI&gt;Do we need to join Apple's VAS program separately?&lt;/LI&gt;&lt;LI&gt;Are there other certificates/programs that we must join?&lt;/LI&gt;&lt;LI&gt;What are the associated costs? (type of costs, recurring, one time, ...)&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;Any guidance, documentation links, or suggestions would be greatly appreciated!&lt;/P&gt;&lt;P class=""&gt;Thank you,&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 21 May 2025 14:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Implementing-smart-lock-with-PN7161-for-Apple-Wallet/m-p/2101714#M13209</guid>
      <dc:creator>Geiger8759</dc:creator>
      <dc:date>2025-05-21T14:34:42Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing smart lock with PN7161 for Apple Wallet</title>
      <link>https://community.nxp.com/t5/NFC/Implementing-smart-lock-with-PN7161-for-Apple-Wallet/m-p/2101930#M13210</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223646"&gt;@Geiger8759&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;It is necessary to get approval from Apple for using PN7161 in the ECP application.ECP software, information and support can only be provided through a NXP FAE. You could also contact your local &lt;A href="https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS" target="_blank"&gt;Distributor&lt;/A&gt; for further support on this inquiry.&lt;/P&gt;
&lt;P&gt;For more information, please refer to &lt;A href="https://www.nxp.com/docs/en/application-note/AN13892.pdf" target="_blank"&gt;PN7160 frequently asked questions&lt;/A&gt;, Section 13.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 19:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Implementing-smart-lock-with-PN7161-for-Apple-Wallet/m-p/2101930#M13210</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-05-21T19:48:20Z</dc:date>
    </item>
  </channel>
</rss>