<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックHelp with device development.</title>
    <link>https://community.nxp.com/t5/NFC/Help-with-device-development/m-p/630797#M1300</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;Hello!&lt;/P&gt;&lt;P class=""&gt;Greetings for the day! I am working on a business start up which is about the eradication of sexual harassment against women through the use of technology. From past few months, I have been working on conceptualising a device which would operate on a RF application. It would be a sticker tag which a person could wear over the clothes or probably stick it on the back of their cell phones.&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;The work of an RFID STICKER TAG is to send&lt;STRONG&gt;&amp;nbsp;SIGNAL&lt;/STRONG&gt;&amp;nbsp;to the&lt;STRONG&gt;&amp;nbsp;Tied-Up Device&lt;/STRONG&gt;, which would be a&amp;nbsp;&lt;STRONG&gt;CELL PHONE(Android or I Phone)&lt;/STRONG&gt;. The maximum transceiving range of an RFID required is 80 centimetres to 1 meter.&amp;nbsp; We would have a&amp;nbsp;&lt;STRONG&gt;MOMENTARY SWITCH(BUTTON)&lt;/STRONG&gt;&amp;nbsp;on a device, only pressing which would lead to the initialisation of a transmission protocol by the RFID device. After pressing a momentary switch on a RFID device also has to have a vibration. So that, it can be realised that the protocol has been initiated.&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;It would only be a one time use tag device. Only that much power is to be provided to the device, that, it could transmit the signal once to the tied up cell phone. I also want the device to always stay connected to the cell phone. But, it should only utilise its power when the momentary switch is been pressed/ the transmission protocol is initialised.&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;I have able to conceptualise the form factor of the device but still stuck up on how to achieve the form factor. I would be more than grateful if someone who holds an expertise in this field could help me in designing the device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Mar 2017 08:07:35 GMT</pubDate>
    <dc:creator>mayankagrawal</dc:creator>
    <dc:date>2017-03-29T08:07:35Z</dc:date>
    <item>
      <title>Help with device development.</title>
      <link>https://community.nxp.com/t5/NFC/Help-with-device-development/m-p/630797#M1300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class=""&gt;Hello!&lt;/P&gt;&lt;P class=""&gt;Greetings for the day! I am working on a business start up which is about the eradication of sexual harassment against women through the use of technology. From past few months, I have been working on conceptualising a device which would operate on a RF application. It would be a sticker tag which a person could wear over the clothes or probably stick it on the back of their cell phones.&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;The work of an RFID STICKER TAG is to send&lt;STRONG&gt;&amp;nbsp;SIGNAL&lt;/STRONG&gt;&amp;nbsp;to the&lt;STRONG&gt;&amp;nbsp;Tied-Up Device&lt;/STRONG&gt;, which would be a&amp;nbsp;&lt;STRONG&gt;CELL PHONE(Android or I Phone)&lt;/STRONG&gt;. The maximum transceiving range of an RFID required is 80 centimetres to 1 meter.&amp;nbsp; We would have a&amp;nbsp;&lt;STRONG&gt;MOMENTARY SWITCH(BUTTON)&lt;/STRONG&gt;&amp;nbsp;on a device, only pressing which would lead to the initialisation of a transmission protocol by the RFID device. After pressing a momentary switch on a RFID device also has to have a vibration. So that, it can be realised that the protocol has been initiated.&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;It would only be a one time use tag device. Only that much power is to be provided to the device, that, it could transmit the signal once to the tied up cell phone. I also want the device to always stay connected to the cell phone. But, it should only utilise its power when the momentary switch is been pressed/ the transmission protocol is initialised.&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;I have able to conceptualise the form factor of the device but still stuck up on how to achieve the form factor. I would be more than grateful if someone who holds an expertise in this field could help me in designing the device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Mar 2017 08:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Help-with-device-development/m-p/630797#M1300</guid>
      <dc:creator>mayankagrawal</dc:creator>
      <dc:date>2017-03-29T08:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: Help with device development.</title>
      <link>https://community.nxp.com/t5/NFC/Help-with-device-development/m-p/630798#M1301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would go for an Arduino / BLE solution.&lt;/P&gt;&lt;P&gt;NFC is too specific not for this kind of things.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Mar 2017 11:59:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Help-with-device-development/m-p/630798#M1301</guid>
      <dc:creator>ericoudammervel</dc:creator>
      <dc:date>2017-03-31T11:59:46Z</dc:date>
    </item>
  </channel>
</rss>