<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN5180 Authentication MiFare Plus EV1 with 7 bite UID in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2049485#M12710</link>
    <description>&lt;P&gt;Thank you KellyLi&lt;/P&gt;&lt;P&gt;I'm&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;executing the MIFARE_AUTHENTICATE command on the Mifare Classic section in Mifare Plus Ev1 card with 7 byte UID.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I eventually found AN10927 (MIFARE Product and UID Processing) which explains that the lower 4 bytes of the 7-byte UID should be used.&lt;/P&gt;&lt;P&gt;Some of the card readers I'm working with use PN5180 and some use CRLC663. When I use the lower 4 bytes for authentication, the PN5180 works fine, but the CRLC663 gives me an error. What could be the issue?&lt;/P&gt;</description>
    <pubDate>Sun, 23 Feb 2025 22:58:23 GMT</pubDate>
    <dc:creator>ghshin</dc:creator>
    <dc:date>2025-02-23T22:58:23Z</dc:date>
    <item>
      <title>PN5180 Authentication MiFare Plus EV1 with 7 bite UID</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2047938#M12691</link>
      <description>&lt;P&gt;the card reader i'm developping use PN5180.&lt;BR /&gt;I want to read Mifare Plus ev1 Card with 7bytes UID&lt;BR /&gt;but PN5180 datasheet explain only 4byte UID card.&lt;BR /&gt;How can i make authentication mifare plus with 7 byte UID with PN5180&lt;/P&gt;&lt;P&gt;Please help me, how to do this.&lt;BR /&gt;Thank you so much.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 07:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2047938#M12691</guid>
      <dc:creator>ghshin</dc:creator>
      <dc:date>2025-02-20T07:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Authentication MiFare Plus EV1 with 7 bite UID</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2047962#M12692</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/114693"&gt;@ghshin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You need to activate Layer 4 of the protocol, and then reading the UID, please try.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 08:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2047962#M12692</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-02-20T08:19:07Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Authentication MiFare Plus EV1 with 7 bite UID</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2048591#M12701</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Thank you KellyLi&lt;/SPAN&gt;&lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;&lt;SPAN&gt;I am attempting the MIFARE_AUTHENTICATE(0x0C) command for the SL1 Mifare Classic section.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have activated the card and got a 7-byte UID.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is that the parameter UID of the MIFARE_AUTHENTICATE(0x0C) command requires only 4 bytes.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Feb 2025 22:52:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2048591#M12701</guid>
      <dc:creator>ghshin</dc:creator>
      <dc:date>2025-02-20T22:52:25Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Authentication MiFare Plus EV1 with 7 bite UID</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2048983#M12702</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/114693"&gt;@ghshin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So your question is to execute the MIFARE_AUTHENTICATE command on the Mifare Classic card, right?&lt;BR /&gt;If yes, perform AUTHENTICATE to the Mifare Classic card only at Layer 3 of the protocol.&lt;/P&gt;
&lt;P&gt;Also, it's recommanded that you can refer to the project &lt;STRONG&gt;NfcrdlibEx4_MIFAREClassic&lt;/STRONG&gt; to debug your Application.&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 09:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2048983#M12702</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-02-21T09:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Authentication MiFare Plus EV1 with 7 bite UID</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2049485#M12710</link>
      <description>&lt;P&gt;Thank you KellyLi&lt;/P&gt;&lt;P&gt;I'm&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;executing the MIFARE_AUTHENTICATE command on the Mifare Classic section in Mifare Plus Ev1 card with 7 byte UID.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I eventually found AN10927 (MIFARE Product and UID Processing) which explains that the lower 4 bytes of the 7-byte UID should be used.&lt;/P&gt;&lt;P&gt;Some of the card readers I'm working with use PN5180 and some use CRLC663. When I use the lower 4 bytes for authentication, the PN5180 works fine, but the CRLC663 gives me an error. What could be the issue?&lt;/P&gt;</description>
      <pubDate>Sun, 23 Feb 2025 22:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2049485#M12710</guid>
      <dc:creator>ghshin</dc:creator>
      <dc:date>2025-02-23T22:58:23Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Authentication MiFare Plus EV1 with 7 bite UID</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2049793#M12715</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/114693"&gt;@ghshin&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The CRLC663 and PN5180 are not fully compatible, so you need to properly transmit and parse RF signals against each other's data sheets.&amp;nbsp;For example, the polling command is the same, but the CRLC663 and PN5180 command codes are different.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 09:50:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Authentication-MiFare-Plus-EV1-with-7-bite-UID/m-p/2049793#M12715</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2025-02-24T09:50:02Z</dc:date>
    </item>
  </channel>
</rss>