<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NCx3321 communication problem in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NCx3321-communication-problem/m-p/2036049#M12584</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a S32K118 evaluation board and a NCx3321 S32K Addon board3.&lt;BR /&gt;I try to communicate through SPI but the NCx3321 does not answer.&lt;/P&gt;&lt;P&gt;Application note AN790311 shows some examples for the communiction. After sending a command frame there should be a interrupt to signal that date can be read.&lt;BR /&gt;But the IRQ line never changes to high level. And the chip never responses any data.&lt;/P&gt;&lt;P&gt;The IRQ line is connected with an input and configured to generate an interrupt on rising edge. This works when i manually change the level at this input.&lt;/P&gt;&lt;P&gt;How can I communicate with this chip?&lt;/P&gt;&lt;P&gt;Do I need further presets?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Christiane Eibeck&lt;/P&gt;</description>
    <pubDate>Thu, 30 Jan 2025 09:04:55 GMT</pubDate>
    <dc:creator>Christiane</dc:creator>
    <dc:date>2025-01-30T09:04:55Z</dc:date>
    <item>
      <title>NCx3321 communication problem</title>
      <link>https://community.nxp.com/t5/NFC/NCx3321-communication-problem/m-p/2036049#M12584</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a S32K118 evaluation board and a NCx3321 S32K Addon board3.&lt;BR /&gt;I try to communicate through SPI but the NCx3321 does not answer.&lt;/P&gt;&lt;P&gt;Application note AN790311 shows some examples for the communiction. After sending a command frame there should be a interrupt to signal that date can be read.&lt;BR /&gt;But the IRQ line never changes to high level. And the chip never responses any data.&lt;/P&gt;&lt;P&gt;The IRQ line is connected with an input and configured to generate an interrupt on rising edge. This works when i manually change the level at this input.&lt;/P&gt;&lt;P&gt;How can I communicate with this chip?&lt;/P&gt;&lt;P&gt;Do I need further presets?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Christiane Eibeck&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jan 2025 09:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NCx3321-communication-problem/m-p/2036049#M12584</guid>
      <dc:creator>Christiane</dc:creator>
      <dc:date>2025-01-30T09:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: NCx3321 communication problem</title>
      <link>https://community.nxp.com/t5/NFC/NCx3321-communication-problem/m-p/2036090#M12586</link>
      <description>&lt;P&gt;I use the NXP Eval-board and the NXP NFC Addon-board. The Addon-board is made to plug onto the S32K Eval-Board. So there should be no problems with wiring or level shifters. The SPI settings (CPOL/CPHA) ar set to the demanded values.&lt;/P&gt;&lt;P&gt;The SPI communication generally works with other devices. And of course I use a logic analyzer to check the communication.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Jan 2025 10:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NCx3321-communication-problem/m-p/2036090#M12586</guid>
      <dc:creator>Christiane</dc:creator>
      <dc:date>2025-01-30T10:48:31Z</dc:date>
    </item>
    <item>
      <title>Re: NCx3321 communication problem</title>
      <link>https://community.nxp.com/t5/NFC/NCx3321-communication-problem/m-p/2036688#M12597</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As you might know, there are some of the documents and libraries which are under NDA (Non-Disclosure Agreement)&lt;/P&gt;
&lt;P&gt;Could you please help us contact the person that helped you getting the device. The &lt;SPAN&gt;NCx3321&amp;nbsp;information is under NDA .&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 17:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NCx3321-communication-problem/m-p/2036688#M12597</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2025-01-31T17:38:08Z</dc:date>
    </item>
  </channel>
</rss>