<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Antenna Power Setting for PN7150 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Antenna-Power-Setting-for-PN7150/m-p/2030355#M12525</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using the &lt;STRONG&gt;PN7150&lt;/STRONG&gt; IC for detecting RFID cards and running it on a Linux kernel &lt;STRONG&gt;5.4&lt;/STRONG&gt;&amp;nbsp;&lt;STRONG&gt;(AM335x)&lt;/STRONG&gt; with the &lt;STRONG&gt;/drivers/misc/nxp-pn5xx&lt;/STRONG&gt; driver.&lt;/P&gt;&lt;P&gt;The datasheet specifies a maximum current of &lt;STRONG&gt;30mA&lt;/STRONG&gt;, but our measurements show approximately &lt;STRONG&gt;7mA&lt;/STRONG&gt; of current to the antenna.&lt;/P&gt;&lt;P&gt;We would like to know how we can retrieve and modify the antenna power settings from the firmware (driver) side.&lt;/P&gt;&lt;P&gt;Below is the antenna structure:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Type:&lt;/STRONG&gt; Loop – Copper trace&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Geometry (inches):&lt;/STRONG&gt; 1.57 × 1.57 (4 turns)&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Frequency Range:&lt;/STRONG&gt; 13.56 MHz&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Regards,&lt;BR /&gt;Ganesh.&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jan 2025 06:39:19 GMT</pubDate>
    <dc:creator>Ganesh_G</dc:creator>
    <dc:date>2025-01-20T06:39:19Z</dc:date>
    <item>
      <title>Antenna Power Setting for PN7150</title>
      <link>https://community.nxp.com/t5/NFC/Antenna-Power-Setting-for-PN7150/m-p/2030355#M12525</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using the &lt;STRONG&gt;PN7150&lt;/STRONG&gt; IC for detecting RFID cards and running it on a Linux kernel &lt;STRONG&gt;5.4&lt;/STRONG&gt;&amp;nbsp;&lt;STRONG&gt;(AM335x)&lt;/STRONG&gt; with the &lt;STRONG&gt;/drivers/misc/nxp-pn5xx&lt;/STRONG&gt; driver.&lt;/P&gt;&lt;P&gt;The datasheet specifies a maximum current of &lt;STRONG&gt;30mA&lt;/STRONG&gt;, but our measurements show approximately &lt;STRONG&gt;7mA&lt;/STRONG&gt; of current to the antenna.&lt;/P&gt;&lt;P&gt;We would like to know how we can retrieve and modify the antenna power settings from the firmware (driver) side.&lt;/P&gt;&lt;P&gt;Below is the antenna structure:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Type:&lt;/STRONG&gt; Loop – Copper trace&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Geometry (inches):&lt;/STRONG&gt; 1.57 × 1.57 (4 turns)&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Frequency Range:&lt;/STRONG&gt; 13.56 MHz&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Regards,&lt;BR /&gt;Ganesh.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jan 2025 06:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Antenna-Power-Setting-for-PN7150/m-p/2030355#M12525</guid>
      <dc:creator>Ganesh_G</dc:creator>
      <dc:date>2025-01-20T06:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: Antenna Power Setting for PN7150</title>
      <link>https://community.nxp.com/t5/NFC/Antenna-Power-Setting-for-PN7150/m-p/2030793#M12530</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227702"&gt;@Ganesh_G&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please, consider that our support for PN7150 is very limited as it is Not Recommended for New Designs; we recommend using &lt;A href="https://www.nxp.com/products/PN7160" target="_blank"&gt;PN7160&lt;/A&gt; instead.&lt;/P&gt;
&lt;P&gt;Tx power may depend on the antenna characteristics and a proper matching circuit. Please make sure you have followed the &lt;A href="https://www.nxp.com/docs/en/application-note/AN11756.pdf" target="_blank"&gt;PN7150 Hardware Design Guide&lt;/A&gt;; Chapter 7 describes the Antenna interface. Also, you can refer to the &lt;A href="https://www.nxp.com/design/training/nfc-antenna-design:TIP-NFC-ANTENNA-DESIGN" target="_blank"&gt;NFC Antenna Design&lt;/A&gt; training, an online training series that could help you with key aspects for the antenna, optimizing and debugging, and testing to get the best-matched antenna for your product; this in addition to the &lt;A href="https://community.nxp.com/t5/NFC/bd-p/nfc" target="_blank"&gt;NFC Antenna Tool&lt;/A&gt;. Additionally, I will recommend you checking the Chapter 6 Power interface of PN7150 Hardware Design Guide.&lt;/P&gt;
&lt;P&gt;More information on transmitter voltage configuration can be found in &lt;A href="https://www.nxp.com/docs/en/user-guide/UM10936.pdf" target="_blank"&gt;PN7150 User Manual&lt;/A&gt;, Section 5.7.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jan 2025 16:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Antenna-Power-Setting-for-PN7150/m-p/2030793#M12530</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2025-01-20T16:52:05Z</dc:date>
    </item>
  </channel>
</rss>