<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: Emulate Mifare Card on PN512 using TgInitAsTarget command</title>
    <link>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2024784#M12507</link>
    <description>&lt;P&gt;Thanks for your answer!&lt;/P&gt;&lt;P&gt;Unfortunately, there is no description of commands like TgInitAsTarget in this document.&lt;/P&gt;&lt;P&gt;When I send to the PN512 command TgInitAsTarget in the form&lt;BR /&gt;D4 8C 00 44 00 12 34 56 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 AA 99 88 77 66 55 44 33 22 11 00 00&lt;/P&gt;&lt;P&gt;then, on the PN512-based reader and on the MFRC531-based reader, I get the correct ATR for Mifare Ultralight card in the form&lt;BR /&gt;3B 8F 80 01 80 4F 0C A0 00 00 03 06 03 00 03 00 00 00 00 68&lt;BR /&gt;but the TgInitAsTarget command does not return anything and the client reader cannot receive any data from the emulated card.&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jan 2025 10:45:32 GMT</pubDate>
    <dc:creator>avgurt9</dc:creator>
    <dc:date>2025-01-09T10:45:32Z</dc:date>
    <item>
      <title>Emulate Mifare Card on PN512 using TgInitAsTarget command</title>
      <link>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2024174#M12504</link>
      <description>&lt;P&gt;Hello, everybody!&lt;/P&gt;&lt;P&gt;How can I emulate a Mifare Classic card or Mifare Ultralight card on a PN512 using the TgInitAsTarget command?&lt;/P&gt;&lt;P&gt;When I send to the PN512 command TgInitAsTarget in the form&lt;BR /&gt;D4 8C 00 08 00 12 34 56 40 01 FE A2 A3 A4 A5 A6 A7 C0 C1 C2 C3 C4 C5 C6 C7 FF FF AA 99 88 77 66 55 44 33 22 11 00 00&lt;/P&gt;&lt;P&gt;then on another PN512-based reader I get the ATR in the form&lt;BR /&gt;3B 8F 80 01 80 4F 0C A0 00 00 03 06 11 00 3B 00 00 00 00 42&lt;/P&gt;&lt;P&gt;and on an MFRC531-based reader, I get the ATR in the form&lt;BR /&gt;3B 8F 80 01 80 4F 0C A0 00 00 03 06 03 FF 40 00 00 00 00 D4&lt;/P&gt;&lt;P&gt;what doesn't match the Mifare card.&lt;/P&gt;&lt;P&gt;Is there a User Manual for NXP PN512 similar to UM0801-03 PN533 User Manual or UM0701-02 PN532 User Manual?&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jan 2025 16:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2024174#M12504</guid>
      <dc:creator>avgurt9</dc:creator>
      <dc:date>2025-01-08T16:31:21Z</dc:date>
    </item>
    <item>
      <title>Re: Emulate Mifare Card on PN512 using TgInitAsTarget command</title>
      <link>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2024624#M12505</link>
      <description>&lt;P&gt;Unfortunately, there is no UM for PN512. There are only datasheet.&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/PN512.pdf?pspll=1" target="_blank"&gt;PN512.fm&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 08:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2024624#M12505</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-01-09T08:17:40Z</dc:date>
    </item>
    <item>
      <title>Re: Emulate Mifare Card on PN512 using TgInitAsTarget command</title>
      <link>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2024784#M12507</link>
      <description>&lt;P&gt;Thanks for your answer!&lt;/P&gt;&lt;P&gt;Unfortunately, there is no description of commands like TgInitAsTarget in this document.&lt;/P&gt;&lt;P&gt;When I send to the PN512 command TgInitAsTarget in the form&lt;BR /&gt;D4 8C 00 44 00 12 34 56 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 AA 99 88 77 66 55 44 33 22 11 00 00&lt;/P&gt;&lt;P&gt;then, on the PN512-based reader and on the MFRC531-based reader, I get the correct ATR for Mifare Ultralight card in the form&lt;BR /&gt;3B 8F 80 01 80 4F 0C A0 00 00 03 06 03 00 03 00 00 00 00 68&lt;BR /&gt;but the TgInitAsTarget command does not return anything and the client reader cannot receive any data from the emulated card.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 10:45:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2024784#M12507</guid>
      <dc:creator>avgurt9</dc:creator>
      <dc:date>2025-01-09T10:45:32Z</dc:date>
    </item>
    <item>
      <title>Re: Emulate Mifare Card on PN512 using TgInitAsTarget command</title>
      <link>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2026494#M12517</link>
      <description>&lt;P&gt;Yes, it is a very old product. The information is not easy to find out. I cannot find out the example for your reference.&lt;/P&gt;
&lt;P&gt;I would suggest you to use PN7160 for the new project development.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/PN7160" target="_blank"&gt;PN7160 | NFC Controller with Integrated Firmware and NCI Interface | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 07:29:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Emulate-Mifare-Card-on-PN512-using-TgInitAsTarget-command/m-p/2026494#M12517</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2025-01-13T07:29:25Z</dc:date>
    </item>
  </channel>
</rss>