<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Power-harvesting using NFC to power up a light sensor and LED in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2006354#M12387</link>
    <description>&lt;P&gt;Hi, thank you for sharing the link to the product. I checked it and it seems that the NTAG5 link can control I2C devices. So it must be programmable. I was wondering if you have example codes that I can refer to?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Tue, 03 Dec 2024 20:24:01 GMT</pubDate>
    <dc:creator>samiha1234</dc:creator>
    <dc:date>2024-12-03T20:24:01Z</dc:date>
    <item>
      <title>Power-harvesting using NFC to power up a light sensor and LED</title>
      <link>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2000573#M12341</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I want to design a circuit that can read data from a sensor (this is a color sensor ,AS7341) and it will be connected to a LED.&amp;nbsp;I want to determine the light intensity of the LED using AS7341 (which requires 1.8V for operation, max 300µA consumption) and I'll use an led (HSMW-C230) which has a forward current of 5 mA with a typical forward voltage of 2.85 V.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want the circuit to be lightweight and don't want to use a battery. I want to wirelessly get the sensor reading from the device to the smartphone, it will just be a one time reading with NFC. I was wondering&amp;nbsp;if&amp;nbsp;this feasible with an NFC power harvesting IC like the NTAG I²C Plus by NXP? Will it be enough to power up the led and the color sensor? Is the&amp;nbsp;NTAG I²C Plus able to transfer the intensity data from AS7341 to smartphone via I2C or do I need a separate microcontroller for that task?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So as a summary:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I bring my smartphone closer to my device, the led should light up and the AS7341 should get a light intensity reading from the LED. Then it should transfer this intensity data over to the smartphone. Is this something feasible? What are my options? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 24 Nov 2024 22:47:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2000573#M12341</guid>
      <dc:creator>samiha1234</dc:creator>
      <dc:date>2024-11-24T22:47:53Z</dc:date>
    </item>
    <item>
      <title>Re: Power-harvesting using NFC to power up a light sensor and LED</title>
      <link>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2005092#M12367</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_5" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243747" target="_self" aria-label="View Profile of samiha1234"&gt;&lt;SPAN class=""&gt;samiha1234&lt;/SPAN&gt;&lt;/A&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please look at this product -&amp;gt;&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/connected-nfc-tags/ntag-5-link-nfc-forum-compliant-ic-bridge-for-iot-on-demand:NTAG5-LINK" target="_blank"&gt;https://www.nxp.com/products/rfid-nfc/nfc-hf/connected-nfc-tags/ntag-5-link-nfc-forum-compliant-ic-bridge-for-iot-on-demand:NTAG5-LINK&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 10:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2005092#M12367</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-12-02T10:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: Power-harvesting using NFC to power up a light sensor and LED</title>
      <link>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2006354#M12387</link>
      <description>&lt;P&gt;Hi, thank you for sharing the link to the product. I checked it and it seems that the NTAG5 link can control I2C devices. So it must be programmable. I was wondering if you have example codes that I can refer to?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 03 Dec 2024 20:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2006354#M12387</guid>
      <dc:creator>samiha1234</dc:creator>
      <dc:date>2024-12-03T20:24:01Z</dc:date>
    </item>
    <item>
      <title>Re: Power-harvesting using NFC to power up a light sensor and LED</title>
      <link>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2006376#M12388</link>
      <description>&lt;P&gt;I also found two development boards &lt;SPAN&gt;&amp;nbsp;OM2NTP5332 board for the NTAG 5 link/switch, and the OM2NTA5332 board for the NTAG 5 boost.&amp;nbsp;The one for the boost has a 10 by 10 mm antenna but the one for LINK has a larger antenna. I was wondering if the 10 by 10 mm antenna would work with the NTAG 5 LINK. I have little idea about antenna design so I am hoping to copy the design in the development board.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Dec 2024 21:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2006376#M12388</guid>
      <dc:creator>samiha1234</dc:creator>
      <dc:date>2024-12-03T21:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: Power-harvesting using NFC to power up a light sensor and LED</title>
      <link>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2009192#M12393</link>
      <description>&lt;P&gt;Hello&amp;nbsp;samiha1234&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For this product, we offer an evaluation board:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/connected-nfc-tags/ntag-5-development-kits:OM2NTX5332" target="_blank"&gt;https://www.nxp.com/products/rfid-nfc/nfc-hf/connected-nfc-tags/ntag-5-development-kits:OM2NTX5332&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;+ some FW examples&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_0-1733495096993.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314578i2ECC7AE876728B86/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_0-1733495096993.png" alt="Tomas_Parizek_0-1733495096993.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please look at them&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Dec 2024 14:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Power-harvesting-using-NFC-to-power-up-a-light-sensor-and-LED/m-p/2009192#M12393</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-12-06T14:25:15Z</dc:date>
    </item>
  </channel>
</rss>