<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Android 13 porting PN7220 issue</title>
    <link>https://community.nxp.com/t5/NFC/Android-13-porting-PN7220-issue/m-p/2004160#M12359</link>
    <description>&lt;P&gt;RK3568 Android 13 porting PN7220.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PN7220EV/C101&lt;/SPAN&gt; hardware uses single-host mode, and the kernel driver is ported by pulling down &lt;A href="https://github.com/nxp-nfc-infra/nfcandroid_platform_drivers.git" target="_blank"&gt;https://github.com/nxp-nfc-infra/nfcandroid_platform_drivers.git&lt;/A&gt; .&lt;BR /&gt;The current device is mounted on the corresponding i2c bus;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The HAL layer pulled down &lt;A href="https://github.com/NXPNFCLinux/PN7220_Android13" target="_blank"&gt;https://github.com/NXPNFCLinux/PN7220_Android13&lt;/A&gt; to the ANDROID_BUILD_TOP/vendor/nxp folder and successfully ran install_NFC.sh.&lt;BR /&gt;Some compilation issues were resolved by referring to &lt;A href="https://zhuanlan.zhihu.com/p/573489474" target="_blank"&gt;https://zhuanlan.zhihu.com/p/573489474&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;After the compiled image was burned to the device, "Control message: Could not find 'android.hardware.nfc@1.2::INfc/default' for ctl.interface_start from pid: 146 (/system/bin/hwservicemanager）"continued to print, but there was an explanation of "android.hardware.nfc" in the device's vendor/etc/vintf/manifest.xml. How can this problem be solved?Many thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the logcat log and the vendor/etc/Vintf/manifest.xml file&lt;/P&gt;</description>
    <pubDate>Fri, 29 Nov 2024 07:53:05 GMT</pubDate>
    <dc:creator>ChumingYang</dc:creator>
    <dc:date>2024-11-29T07:53:05Z</dc:date>
    <item>
      <title>Android 13 porting PN7220 issue</title>
      <link>https://community.nxp.com/t5/NFC/Android-13-porting-PN7220-issue/m-p/2004160#M12359</link>
      <description>&lt;P&gt;RK3568 Android 13 porting PN7220.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PN7220EV/C101&lt;/SPAN&gt; hardware uses single-host mode, and the kernel driver is ported by pulling down &lt;A href="https://github.com/nxp-nfc-infra/nfcandroid_platform_drivers.git" target="_blank"&gt;https://github.com/nxp-nfc-infra/nfcandroid_platform_drivers.git&lt;/A&gt; .&lt;BR /&gt;The current device is mounted on the corresponding i2c bus;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The HAL layer pulled down &lt;A href="https://github.com/NXPNFCLinux/PN7220_Android13" target="_blank"&gt;https://github.com/NXPNFCLinux/PN7220_Android13&lt;/A&gt; to the ANDROID_BUILD_TOP/vendor/nxp folder and successfully ran install_NFC.sh.&lt;BR /&gt;Some compilation issues were resolved by referring to &lt;A href="https://zhuanlan.zhihu.com/p/573489474" target="_blank"&gt;https://zhuanlan.zhihu.com/p/573489474&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;After the compiled image was burned to the device, "Control message: Could not find 'android.hardware.nfc@1.2::INfc/default' for ctl.interface_start from pid: 146 (/system/bin/hwservicemanager）"continued to print, but there was an explanation of "android.hardware.nfc" in the device's vendor/etc/vintf/manifest.xml. How can this problem be solved?Many thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is the logcat log and the vendor/etc/Vintf/manifest.xml file&lt;/P&gt;</description>
      <pubDate>Fri, 29 Nov 2024 07:53:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Android-13-porting-PN7220-issue/m-p/2004160#M12359</guid>
      <dc:creator>ChumingYang</dc:creator>
      <dc:date>2024-11-29T07:53:05Z</dc:date>
    </item>
    <item>
      <title>Re: Android 13 porting PN7220 issue</title>
      <link>https://community.nxp.com/t5/NFC/Android-13-porting-PN7220-issue/m-p/2004461#M12364</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228137"&gt;@ChumingYang&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please accept my apologies, porting our software to third-party devices is out of our support scope and it is up to the customer based on the available documentation.&lt;/P&gt;
&lt;P&gt;Could you please confirm that your customer followed the instructions from the &lt;A href="https://www.nxp.com/docs/en/application-note/AN13971.pdf" target="_blank"&gt;PN7220 &amp;amp; PN7160 - Android porting guide&lt;/A&gt;? After the images are installed, some MW cleanup must be performed. Please refer to Section 3.4 for PN7220 single host.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 29 Nov 2024 19:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Android-13-porting-PN7220-issue/m-p/2004461#M12364</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-11-29T19:43:33Z</dc:date>
    </item>
    <item>
      <title>回复： Android 13 porting PN7220 issue</title>
      <link>https://community.nxp.com/t5/NFC/Android-13-porting-PN7220-issue/m-p/2015223#M12416</link>
      <description>&lt;P&gt;Thanks, I have no compilation issues now&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 10:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Android-13-porting-PN7220-issue/m-p/2015223#M12416</guid>
      <dc:creator>ChumingYang</dc:creator>
      <dc:date>2024-12-17T10:55:40Z</dc:date>
    </item>
  </channel>
</rss>