<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NXP NFC Library v07.10.00 and Linux 6.6 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NXP-NFC-Library-v07-10-00-and-Linux-6-6/m-p/1979289#M12237</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any plans to upgrade the NFC library to support Linux 6.6.x ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Linux 6.6.x,&amp;nbsp; using GPIO through the &lt;STRONG&gt;/sys/class/gpio&lt;/STRONG&gt; filesystem is no longer supported, thus the NFC library cannot be used.&amp;nbsp; The NFC library is using that API to control PN5180 Frontend Reset, Busy, IRQ and DWL signals.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Oct 2024 13:56:06 GMT</pubDate>
    <dc:creator>eldar</dc:creator>
    <dc:date>2024-10-22T13:56:06Z</dc:date>
    <item>
      <title>NXP NFC Library v07.10.00 and Linux 6.6</title>
      <link>https://community.nxp.com/t5/NFC/NXP-NFC-Library-v07-10-00-and-Linux-6-6/m-p/1979289#M12237</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any plans to upgrade the NFC library to support Linux 6.6.x ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Linux 6.6.x,&amp;nbsp; using GPIO through the &lt;STRONG&gt;/sys/class/gpio&lt;/STRONG&gt; filesystem is no longer supported, thus the NFC library cannot be used.&amp;nbsp; The NFC library is using that API to control PN5180 Frontend Reset, Busy, IRQ and DWL signals.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 13:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NXP-NFC-Library-v07-10-00-and-Linux-6-6/m-p/1979289#M12237</guid>
      <dc:creator>eldar</dc:creator>
      <dc:date>2024-10-22T13:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: NXP NFC Library v07.10.00 and Linux 6.6</title>
      <link>https://community.nxp.com/t5/NFC/NXP-NFC-Library-v07-10-00-and-Linux-6-6/m-p/1979295#M12238</link>
      <description>&lt;P&gt;Maybe this guide helps:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/Porting-PN7160-NCI2-stack-to-Raspberry-Pi-5-OS-Bookworm/ta-p/1977521" target="_blank"&gt;https://community.nxp.com/t5/NFC-Knowledge-Base/Porting-PN7160-NCI2-stack-to-Raspberry-Pi-5-OS-Bookworm/ta-p/1977521&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It explains how to port the NFC library to support the newer kernel version.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 14:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NXP-NFC-Library-v07-10-00-and-Linux-6-6/m-p/1979295#M12238</guid>
      <dc:creator>kowalski_analysis</dc:creator>
      <dc:date>2024-10-22T14:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: NXP NFC Library v07.10.00 and Linux 6.6</title>
      <link>https://community.nxp.com/t5/NFC/NXP-NFC-Library-v07-10-00-and-Linux-6-6/m-p/1979883#M12244</link>
      <description>&lt;P&gt;Thanks, I will look into it!&lt;/P&gt;</description>
      <pubDate>Wed, 23 Oct 2024 06:39:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NXP-NFC-Library-v07-10-00-and-Linux-6-6/m-p/1979883#M12244</guid>
      <dc:creator>eldar</dc:creator>
      <dc:date>2024-10-23T06:39:28Z</dc:date>
    </item>
  </channel>
</rss>