<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Demo software for UCODE G2iM+ special features</title>
    <link>https://community.nxp.com/t5/NFC/Demo-software-for-UCODE-G2iM-special-features/m-p/627211#M1222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the Impinj Speedway Revolution R420 UHF reader to read custom tags based on the UCODE G2iM+ IC. Does there exist any free, high-level demo software to highlight the special features of the IC that are managed using the configuration word at address 200h in the EPC memory? In particular, I would like to automatically read out the status of the "Tag Tamper Alarm Indicator"&amp;nbsp;without having to write code in the Low-Level Reader Protocol (LLRP).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Mar 2017 14:56:07 GMT</pubDate>
    <dc:creator>philipponcedele</dc:creator>
    <dc:date>2017-03-28T14:56:07Z</dc:date>
    <item>
      <title>Demo software for UCODE G2iM+ special features</title>
      <link>https://community.nxp.com/t5/NFC/Demo-software-for-UCODE-G2iM-special-features/m-p/627211#M1222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the Impinj Speedway Revolution R420 UHF reader to read custom tags based on the UCODE G2iM+ IC. Does there exist any free, high-level demo software to highlight the special features of the IC that are managed using the configuration word at address 200h in the EPC memory? In particular, I would like to automatically read out the status of the "Tag Tamper Alarm Indicator"&amp;nbsp;without having to write code in the Low-Level Reader Protocol (LLRP).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 14:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Demo-software-for-UCODE-G2iM-special-features/m-p/627211#M1222</guid>
      <dc:creator>philipponcedele</dc:creator>
      <dc:date>2017-03-28T14:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: Demo software for UCODE G2iM+ special features</title>
      <link>https://community.nxp.com/t5/NFC/Demo-software-for-UCODE-G2iM-special-features/m-p/627212#M1223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Philip,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As we don't provide reader solution for UCODE G2iM+ ICs, we don't have such kind of demo as you queried. Please kindly check it with the reader vendor, please refer to &lt;A class="link-titled" href="http://www.impinj.com/products/readers/" title="http://www.impinj.com/products/readers/"&gt;Speedway UHF RFID Readers | Impinj&lt;/A&gt;&amp;nbsp; for details.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 04:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Demo-software-for-UCODE-G2iM-special-features/m-p/627212#M1223</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-04-12T04:18:34Z</dc:date>
    </item>
  </channel>
</rss>