<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Dynamic Lock Bytes for NT3H2111 is off by 4 bytes? in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Dynamic-Lock-Bytes-for-NT3H2111-is-off-by-4-bytes/m-p/1975500#M12205</link>
    <description>&lt;P&gt;The datasheet for The NT3H2111 shows the Dynamic lock bytes as starting at offset 4 on page 0x38.&amp;nbsp; However, in practice, setting bytes 4, 5, and 6 did not lock pages 16 and above.&amp;nbsp; Instead, writing to bytes 8, 9, and 10 did the trick.&amp;nbsp; I am wondering if this was a mistake in the datasheet or did we get a batch of chips that has the incorrect address for the dynamic lock bytes?&lt;/P&gt;</description>
    <pubDate>Wed, 16 Oct 2024 21:33:12 GMT</pubDate>
    <dc:creator>yanqil</dc:creator>
    <dc:date>2024-10-16T21:33:12Z</dc:date>
    <item>
      <title>Dynamic Lock Bytes for NT3H2111 is off by 4 bytes?</title>
      <link>https://community.nxp.com/t5/NFC/Dynamic-Lock-Bytes-for-NT3H2111-is-off-by-4-bytes/m-p/1975500#M12205</link>
      <description>&lt;P&gt;The datasheet for The NT3H2111 shows the Dynamic lock bytes as starting at offset 4 on page 0x38.&amp;nbsp; However, in practice, setting bytes 4, 5, and 6 did not lock pages 16 and above.&amp;nbsp; Instead, writing to bytes 8, 9, and 10 did the trick.&amp;nbsp; I am wondering if this was a mistake in the datasheet or did we get a batch of chips that has the incorrect address for the dynamic lock bytes?&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 21:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Dynamic-Lock-Bytes-for-NT3H2111-is-off-by-4-bytes/m-p/1975500#M12205</guid>
      <dc:creator>yanqil</dc:creator>
      <dc:date>2024-10-16T21:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: Dynamic Lock Bytes for NT3H2111 is off by 4 bytes?</title>
      <link>https://community.nxp.com/t5/NFC/Dynamic-Lock-Bytes-for-NT3H2111-is-off-by-4-bytes/m-p/1975628#M12206</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242084"&gt;@yanqil&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Dynamic Lock Bytes should be a bit difference between 1K version and 2K. What you used should be 2k version, so bytes8,9 and 10 are Dynamic Lock Bytes. But for 1K version, bytes4,5 and 6 are Dynamic Lock Bytes. Please check the below screenshot for the details.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="KellyLi_0-1729131443254.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/305153i0BB70A5B7D9AEA79/image-size/medium?v=v2&amp;amp;px=400" role="button" title="KellyLi_0-1729131443254.png" alt="KellyLi_0-1729131443254.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;KellyLi_0-1729131443254.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 02:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Dynamic-Lock-Bytes-for-NT3H2111-is-off-by-4-bytes/m-p/1975628#M12206</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2024-10-17T02:17:33Z</dc:date>
    </item>
  </channel>
</rss>