<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 NTAG 424 NDEF pattern</title>
    <link>https://community.nxp.com/t5/NFC/NTAG-424-NDEF-pattern/m-p/1974377#M12201</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i'm close to release my secure product but there is something still to fix: using different tools i can still read the ndef pattern. I mean i can see where starts the PICC, how is long, where start EncData ecc. ecc. I tried to hide it but the result is that the tag doesn't work anymore and i think is because the smartphone don't know how to build the ndef. Is there a way to completely hide tag info? The tag is closed, no one, even me, are able to write on it but i prefer to hide everything.&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Oct 2024 14:41:31 GMT</pubDate>
    <dc:creator>MPucci</dc:creator>
    <dc:date>2024-10-15T14:41:31Z</dc:date>
    <item>
      <title>NTAG 424 NDEF pattern</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-424-NDEF-pattern/m-p/1974377#M12201</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i'm close to release my secure product but there is something still to fix: using different tools i can still read the ndef pattern. I mean i can see where starts the PICC, how is long, where start EncData ecc. ecc. I tried to hide it but the result is that the tag doesn't work anymore and i think is because the smartphone don't know how to build the ndef. Is there a way to completely hide tag info? The tag is closed, no one, even me, are able to write on it but i prefer to hide everything.&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 14:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-424-NDEF-pattern/m-p/1974377#M12201</guid>
      <dc:creator>MPucci</dc:creator>
      <dc:date>2024-10-15T14:41:31Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG 424 NDEF pattern</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-424-NDEF-pattern/m-p/1974656#M12202</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220381"&gt;@MPucci&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;NTAG 424 allows the user to change the access rights configuration; file data can be accesses with 3 different access rights: Read, Write and ReadWrite. Write and ReadWrite access rights for the NDEF File (File No. 02h) should be changed after personalization in order to prevent unauthorized changes in the NDEF File.&lt;/P&gt;
&lt;P&gt;Please refer to &lt;A href="https://www.nxp.com/docs/en/data-sheet/NT4H2421Gx.pdf" target="_blank"&gt;NTAG 424 Data Sheet&lt;/A&gt;, Section 8.2.3 Files for more information on File access rights management; and &lt;A href="https://www.nxp.com/docs/en/application-note/AN12196.pdf" target="_blank"&gt;NTAG 424 DNA and NTAG 424 DNA TagTamper features and hints&lt;/A&gt;, Chapter 6 for an example of personalization.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 00:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-424-NDEF-pattern/m-p/1974656#M12202</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-10-16T00:23:54Z</dc:date>
    </item>
  </channel>
</rss>