<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NFC powering after using NFC program downloader. in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NFC-powering-after-using-NFC-program-downloader/m-p/1966351#M12177</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project with the NHS3100, where the device should not be constantly powered. The goal is for it to read the temperature from its sensor and expose it as a parameter in a URL, which will be published on the NFC tag.&lt;/P&gt;&lt;P&gt;I successfully uploaded the code using J-Link in MCUXpresso, and everything works perfectly. However, when I upload the code using the NHS31xx NFC Program Loader, the code uploads fine, but my phone no longer reads the tag unless the tag is externally powered.&lt;/P&gt;&lt;P&gt;What configuration do I need to enable the NFC tag to be powered through NFC after uploading the code via NFC Program Loader?&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated!&lt;/P&gt;</description>
    <pubDate>Thu, 03 Oct 2024 11:06:14 GMT</pubDate>
    <dc:creator>gpol2003</dc:creator>
    <dc:date>2024-10-03T11:06:14Z</dc:date>
    <item>
      <title>NFC powering after using NFC program downloader.</title>
      <link>https://community.nxp.com/t5/NFC/NFC-powering-after-using-NFC-program-downloader/m-p/1966351#M12177</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project with the NHS3100, where the device should not be constantly powered. The goal is for it to read the temperature from its sensor and expose it as a parameter in a URL, which will be published on the NFC tag.&lt;/P&gt;&lt;P&gt;I successfully uploaded the code using J-Link in MCUXpresso, and everything works perfectly. However, when I upload the code using the NHS31xx NFC Program Loader, the code uploads fine, but my phone no longer reads the tag unless the tag is externally powered.&lt;/P&gt;&lt;P&gt;What configuration do I need to enable the NFC tag to be powered through NFC after uploading the code via NFC Program Loader?&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated!&lt;/P&gt;</description>
      <pubDate>Thu, 03 Oct 2024 11:06:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-powering-after-using-NFC-program-downloader/m-p/1966351#M12177</guid>
      <dc:creator>gpol2003</dc:creator>
      <dc:date>2024-10-03T11:06:14Z</dc:date>
    </item>
  </channel>
</rss>