<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックInconsistent on iPhone</title>
    <link>https://community.nxp.com/t5/NFC/Inconsistent-on-iPhone/m-p/1957725#M12149</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a product which uses NTAG5 Link connected to an I2C sensor using energy harvesting. Android App performance is good, but with iPhone the performance is inconsistent. Some customers report 10% scan success rate, our testing shows more like 95%. There seems to be no logic that we can conclude in terms of which iPhone model or iOS version is worse, and hence struggle to investigate and solve the problem.&lt;/P&gt;&lt;P&gt;Is this something that others have experienced? Is there any good ideas to improve reliability of the iPhone App?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="NTAG5-LINK" id="NTAG5-LINK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 19 Sep 2024 13:11:59 GMT</pubDate>
    <dc:creator>chic014</dc:creator>
    <dc:date>2024-09-19T13:11:59Z</dc:date>
    <item>
      <title>Inconsistent on iPhone</title>
      <link>https://community.nxp.com/t5/NFC/Inconsistent-on-iPhone/m-p/1957725#M12149</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a product which uses NTAG5 Link connected to an I2C sensor using energy harvesting. Android App performance is good, but with iPhone the performance is inconsistent. Some customers report 10% scan success rate, our testing shows more like 95%. There seems to be no logic that we can conclude in terms of which iPhone model or iOS version is worse, and hence struggle to investigate and solve the problem.&lt;/P&gt;&lt;P&gt;Is this something that others have experienced? Is there any good ideas to improve reliability of the iPhone App?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="NTAG5-LINK" id="NTAG5-LINK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 13:11:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Inconsistent-on-iPhone/m-p/1957725#M12149</guid>
      <dc:creator>chic014</dc:creator>
      <dc:date>2024-09-19T13:11:59Z</dc:date>
    </item>
    <item>
      <title>Re: Inconsistent on iPhone</title>
      <link>https://community.nxp.com/t5/NFC/Inconsistent-on-iPhone/m-p/1958019#M12151</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206228"&gt;@chic014&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;By any chance, have you followed the App Note &lt;A href="https://www.nxp.com/docs/en/application-note/AN12365.pdf" target="_blank"&gt;NTAG 5 - How to use energy harvesting&lt;/A&gt;? There are many factors the influence on energy harvesting, such as the antenna size and field strength of the RF reader.&lt;/P&gt;
&lt;P&gt;You can find some measurements with Apple iPhone 11 in the same App Note; for NFC mobile phones, it is recommended to set energy harvesting mode optimized for low field strength (EH_MODE).&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Sep 2024 21:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Inconsistent-on-iPhone/m-p/1958019#M12151</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-09-19T21:06:45Z</dc:date>
    </item>
  </channel>
</rss>