<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: NFC tag</title>
    <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1955435#M12136</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;this is the info &amp;nbsp;I get if I use the NFC TagInfo app&lt;/P&gt;</description>
    <pubDate>Tue, 17 Sep 2024 06:09:00 GMT</pubDate>
    <dc:creator>Vilgot</dc:creator>
    <dc:date>2024-09-17T06:09:00Z</dc:date>
    <item>
      <title>NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1952033#M12115</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I have some nfc tags right now witch I am trying to get WiFi to but it’s not going to well and I need some advice on what do do?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I have the TagWriter app but don’t know what to put on authentication and encryption and if there could be something wrong with my WiFi cause I feel like I have tried all the options&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 11:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1952033#M12115</guid>
      <dc:creator>Vilgot</dc:creator>
      <dc:date>2024-09-11T11:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1952561#M12117</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240425"&gt;@Vilgot&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;The Authentication Type and Encryption Type will depend on the characteristics defined by your Wi-Fi Access Point and it is something you may need to check in its configuration.&lt;/P&gt;
&lt;P&gt;If your device is within the Wi-Fi range, TagWriter should list the network under "Available Wifi Networks", and those fields should be filled by default.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 20:24:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1952561#M12117</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-09-11T20:24:57Z</dc:date>
    </item>
    <item>
      <title>Re: NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1952645#M12118</link>
      <description>Hi Eduardo&lt;BR /&gt;Thanks for Your reply but I am still not getting it to work.&lt;BR /&gt;I feel like I’m getting the right info into the nfc but it’s never worked just putting my phone on the nfc tag for WiFi.&lt;BR /&gt;It’s has worked with other functions but not with WiFi.&lt;BR /&gt;Because if I haven’t gotten it wrong I understand that I shouldn’t need any applications to get the WiFi on the nfc.&lt;BR /&gt;Do you have any idea of what the problem is ?&lt;BR /&gt;And also it would be easier if I could send a video of it not working, is this possible? Maybe on another platform?&lt;BR /&gt;Thank you/ Vilgot</description>
      <pubDate>Wed, 11 Sep 2024 21:29:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1952645#M12118</guid>
      <dc:creator>Vilgot</dc:creator>
      <dc:date>2024-09-11T21:29:12Z</dc:date>
    </item>
    <item>
      <title>Re: NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1954437#M12129</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Could you please provide more details on your setup?&lt;/P&gt;
&lt;P&gt;What is the tag you are using for the test? What is the mobile device you are using to read de tag with the WiFi credentials?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If needed, you can attach the files to your post.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 13 Sep 2024 18:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1954437#M12129</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-09-13T18:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1954742#M12132</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;Im using an iPhone 13 and have tags from a small company called chipster and they are named NTAG213-tagg &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the picture I put in files shows the tags I have, well I have three of them but they are all called the same thing so I think they are the sam but just different amounts of storage and size&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 15 Sep 2024 11:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1954742#M12132</guid>
      <dc:creator>Vilgot</dc:creator>
      <dc:date>2024-09-15T11:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1955435#M12136</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;this is the info &amp;nbsp;I get if I use the NFC TagInfo app&lt;/P&gt;</description>
      <pubDate>Tue, 17 Sep 2024 06:09:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1955435#M12136</guid>
      <dc:creator>Vilgot</dc:creator>
      <dc:date>2024-09-17T06:09:00Z</dc:date>
    </item>
    <item>
      <title>Re: NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1956984#M12145</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Application launch after reading a tag may have some limitations or restrictions in iOS devices. I will recommend you redirecting your inquiry to the corresponding iOS support documentation and forums.&lt;/P&gt;
&lt;P&gt;I apologize for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Sep 2024 22:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-tag/m-p/1956984#M12145</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-09-18T22:09:41Z</dc:date>
    </item>
  </channel>
</rss>