<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN5190 DPC</title>
    <link>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1945423#M12085</link>
    <description>&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw "P&lt;FONT size="3"&gt;N5190 Dynamic Power Control Quick Calibration and TxShaping Demo", but If I don't have to use PN5190 for payaments, and I have to use it with small labels ISO15693 or different size of Mifare tags, I think that DPC is not the best solution, or what is the best way to setup the PN5190?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;Paolo&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Sep 2024 10:28:04 GMT</pubDate>
    <dc:creator>PDS</dc:creator>
    <dc:date>2024-09-02T10:28:04Z</dc:date>
    <item>
      <title>PN5190 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1945423#M12085</link>
      <description>&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw "P&lt;FONT size="3"&gt;N5190 Dynamic Power Control Quick Calibration and TxShaping Demo", but If I don't have to use PN5190 for payaments, and I have to use it with small labels ISO15693 or different size of Mifare tags, I think that DPC is not the best solution, or what is the best way to setup the PN5190?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;Paolo&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Sep 2024 10:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1945423#M12085</guid>
      <dc:creator>PDS</dc:creator>
      <dc:date>2024-09-02T10:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1946036#M12090</link>
      <description>&lt;P&gt;Hi PDS:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The Dynamic Power Control (DPC) is a feature that allows to control the transmitter current. Therefore the field strength depending on loading and detuning conditions. The DPC can be enabled and then dynamically adapts the output power.&lt;/P&gt;
&lt;P&gt;DPC is a nice feature,&amp;nbsp; it offers an improved RF performance.&amp;nbsp; but it is not directly related to EMVCo.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 08:08:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1946036#M12090</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2024-09-03T08:08:20Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1946060#M12091</link>
      <description>&lt;P&gt;Thank's Daniel for the answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The advantages of DPC are clear, but is not simple to configure. Which is the best procedure for setup the DPC if I don't have to "use EMVCO settings".&lt;/P&gt;&lt;P&gt;Paolo&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 08:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1946060#M12091</guid>
      <dc:creator>PDS</dc:creator>
      <dc:date>2024-09-03T08:33:38Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190 DPC</title>
      <link>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1946265#M12092</link>
      <description>&lt;P&gt;Hi:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can refer to AN 12549,&amp;nbsp; chapter 5:&amp;nbsp; &amp;nbsp;PN5190 and DPC&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN12549.pdf" target="_blank"&gt;PN5190 antenna design guide (nxp.com.cn)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 11:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5190-DPC/m-p/1946265#M12092</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2024-09-03T11:45:29Z</dc:date>
    </item>
  </channel>
</rss>