<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to use CLRC663 transmit data with Miller coded but not NRZ in ISO14443B? in NFC</title>
    <link>https://community.nxp.com/t5/NFC/How-to-use-CLRC663-transmit-data-with-Miller-coded-but-not-NRZ/m-p/1913759#M11947</link>
    <description>&lt;P&gt;hello, everybody:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have a question about CLRC663 how to transmit data with Miller coded but not NRZ in ISO14443B.&lt;/P&gt;&lt;P&gt;I saw that there are some description about data with miller coded.&lt;/P&gt;&lt;P&gt;It is in the 8.3.2 part ( ISO/IEC14443 type B functionality ) of datasheet (High performance multi-protocol NFC frontend CLRC663 and CLRC663 plus).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jaydon_0-1721612247540.png" style="width: 699px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289599i09D5529962C5A11B/image-size/large?v=v2&amp;amp;px=999" role="button" title="jaydon_0-1721612247540.png" alt="jaydon_0-1721612247540.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jaydon_0-1721612247540.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I've seen three registers for miller encoding, 9.16.3 TxDataMod, 9.16.12 TxSym10Mod Reg, and 9.16.13 TxSym32Mod.&lt;/P&gt;&lt;P&gt;I tried to configure them as follows but it seems not to work.By the way, I using the RC663 without library.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Rc663_WriteRegister(CLRC663_REG_TXDATAMOD, 0x50);&lt;BR /&gt;Rc663_WriteRegister(CLRC663_REG_TXSYM10MOD, 0x50);&lt;BR /&gt;Rc663_WriteRegister(CLRC663_REG_TXSYM32MOD, 0x50);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;So, I miss anything in the configuration or I configured it wrong.?&lt;/P&gt;&lt;P&gt;If it were possible to configure Miller coding in ISO14443B using CLRC663?&lt;/P&gt;</description>
    <pubDate>Mon, 22 Jul 2024 07:08:18 GMT</pubDate>
    <dc:creator>jaydon</dc:creator>
    <dc:date>2024-07-22T07:08:18Z</dc:date>
    <item>
      <title>How to use CLRC663 transmit data with Miller coded but not NRZ in ISO14443B?</title>
      <link>https://community.nxp.com/t5/NFC/How-to-use-CLRC663-transmit-data-with-Miller-coded-but-not-NRZ/m-p/1913759#M11947</link>
      <description>&lt;P&gt;hello, everybody:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have a question about CLRC663 how to transmit data with Miller coded but not NRZ in ISO14443B.&lt;/P&gt;&lt;P&gt;I saw that there are some description about data with miller coded.&lt;/P&gt;&lt;P&gt;It is in the 8.3.2 part ( ISO/IEC14443 type B functionality ) of datasheet (High performance multi-protocol NFC frontend CLRC663 and CLRC663 plus).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jaydon_0-1721612247540.png" style="width: 699px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289599i09D5529962C5A11B/image-size/large?v=v2&amp;amp;px=999" role="button" title="jaydon_0-1721612247540.png" alt="jaydon_0-1721612247540.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;jaydon_0-1721612247540.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I've seen three registers for miller encoding, 9.16.3 TxDataMod, 9.16.12 TxSym10Mod Reg, and 9.16.13 TxSym32Mod.&lt;/P&gt;&lt;P&gt;I tried to configure them as follows but it seems not to work.By the way, I using the RC663 without library.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Rc663_WriteRegister(CLRC663_REG_TXDATAMOD, 0x50);&lt;BR /&gt;Rc663_WriteRegister(CLRC663_REG_TXSYM10MOD, 0x50);&lt;BR /&gt;Rc663_WriteRegister(CLRC663_REG_TXSYM32MOD, 0x50);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;So, I miss anything in the configuration or I configured it wrong.?&lt;/P&gt;&lt;P&gt;If it were possible to configure Miller coding in ISO14443B using CLRC663?&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 07:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/How-to-use-CLRC663-transmit-data-with-Miller-coded-but-not-NRZ/m-p/1913759#M11947</guid>
      <dc:creator>jaydon</dc:creator>
      <dc:date>2024-07-22T07:08:18Z</dc:date>
    </item>
  </channel>
</rss>