<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic HITAG S not responding to UID Request in NFC</title>
    <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1907023#M11927</link>
    <description>&lt;P&gt;I am designing a custom hardware using stm32 and &lt;LI-PRODUCT title="HTRC11001T" id="HTRC11001T"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;I have got communications with the HTRC110&amp;nbsp;working but when I try and send any of the UID Request commands specified in the HITAG S&amp;nbsp;data sheet I no response that looks like any of the coding responses. I have set up my code to receive the anti-collision coding but it isn't picking up anything. I have attached to photos below of my command&lt;/P&gt;&lt;P&gt;yellow - antenna&lt;/P&gt;&lt;P&gt;blue Dout&lt;/P&gt;</description>
    <pubDate>Fri, 12 Jul 2024 10:16:19 GMT</pubDate>
    <dc:creator>Felix0209</dc:creator>
    <dc:date>2024-07-12T10:16:19Z</dc:date>
    <item>
      <title>HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1907023#M11927</link>
      <description>&lt;P&gt;I am designing a custom hardware using stm32 and &lt;LI-PRODUCT title="HTRC11001T" id="HTRC11001T"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;I have got communications with the HTRC110&amp;nbsp;working but when I try and send any of the UID Request commands specified in the HITAG S&amp;nbsp;data sheet I no response that looks like any of the coding responses. I have set up my code to receive the anti-collision coding but it isn't picking up anything. I have attached to photos below of my command&lt;/P&gt;&lt;P&gt;yellow - antenna&lt;/P&gt;&lt;P&gt;blue Dout&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 10:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1907023#M11927</guid>
      <dc:creator>Felix0209</dc:creator>
      <dc:date>2024-07-12T10:16:19Z</dc:date>
    </item>
    <item>
      <title>Re: HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1907029#M11928</link>
      <description>&lt;P&gt;I also know the ID from an off the shelf module so I can send the select (UID) command and it looks more promising with the SOC but still has no data&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 10:21:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1907029#M11928</guid>
      <dc:creator>Felix0209</dc:creator>
      <dc:date>2024-07-12T10:21:58Z</dc:date>
    </item>
    <item>
      <title>Re: HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1907417#M11930</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235594"&gt;@Felix0209&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please confirm that you have followed this App Note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN98080.pdf" target="_blank"&gt;Read/write devices based on the HITAG read/write IC HTRC110&lt;/A&gt; for the design of your reader?&lt;/P&gt;
&lt;P&gt;Is your development based on the &lt;A href="https://www.nxp.com/webapp/Download?colCode=RC110LB6" target="_blank"&gt;Control library HTRC110&lt;/A&gt; we provide? Unfortunately, there is no example for HITAG S, but you could use this library as a reference.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jul 2024 21:37:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1907417#M11930</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-07-12T21:37:37Z</dc:date>
    </item>
    <item>
      <title>Re: HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1909618#M11933</link>
      <description>&lt;P&gt;Yes I followed that app note and yes i used the library as a reference&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 09:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1909618#M11933</guid>
      <dc:creator>Felix0209</dc:creator>
      <dc:date>2024-07-16T09:20:23Z</dc:date>
    </item>
    <item>
      <title>Re: HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1910723#M11935</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;By any chance, did you manufacture your device based on our &lt;A href="https://www.nxp.com/products/rfid-nfc/hitag-lf/hitag-s-transponder-ic:HTSX" target="_blank"&gt;HITAG S&lt;/A&gt; IC or is it a product from a third-party?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 17:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1910723#M11935</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-07-17T17:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1911362#M11938</link>
      <description>&lt;P&gt;Its this tag&lt;/P&gt;&lt;P&gt;&lt;A href="https://xpressrfid.com/product/hid-logi-tag-120-lf-hitag-s-2048-no-logo" target="_blank"&gt;https://xpressrfid.com/product/hid-logi-tag-120-lf-hitag-s-2048-no-logo&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jul 2024 12:06:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1911362#M11938</guid>
      <dc:creator>Felix0209</dc:creator>
      <dc:date>2024-07-18T12:06:30Z</dc:date>
    </item>
    <item>
      <title>Re: HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1911577#M11940</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Since this is an end product from a third-party, I would recommend you contacting the product manufacturer for further support on this part.&lt;/P&gt;
&lt;P&gt;I apologize for the inconvenience this might cause you.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jul 2024 18:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1911577#M11940</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-07-18T18:45:39Z</dc:date>
    </item>
    <item>
      <title>Re: HITAG S not responding to UID Request</title>
      <link>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1912419#M11943</link>
      <description>&lt;P&gt;I finally solved the problem by tweaking the electrical side of things - making sure coil - end is at about 140V. also I changed the timings slightly of the command - using cursors and checking data sheet&lt;/P&gt;&lt;P&gt;Hope this helps anyone with the same problem&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jul 2024 16:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/HITAG-S-not-responding-to-UID-Request/m-p/1912419#M11943</guid>
      <dc:creator>Felix0209</dc:creator>
      <dc:date>2024-07-19T16:21:30Z</dc:date>
    </item>
  </channel>
</rss>