<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Mifare Classic EV1 4K Compatibility in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Mifare-Classic-EV1-4K-Compatibility/m-p/1868529#M11702</link>
    <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;Currently troubleshooting an issue with a device, it has no issue reading older issue Mifare Classic 1K cards, however is having delayed or intermittent reads with a newer batch of Classic EV1 4K cards.&lt;BR /&gt;&lt;BR /&gt;These devices were produced in 2013 and have no available firmware updates, I noticed the EV1 cards were released 2018.&lt;BR /&gt;&lt;BR /&gt;Is there anything known that would cause compatibility issues with these newer revision EV1 cards?&lt;BR /&gt;&lt;BR /&gt;The other potential avenue being investigated is the device having an issue with the additional sectors and block size with the 4K cards.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;There are other devices on site that have no issue with either card, however they have had firmware updates or newer manufacture dates.&lt;/P&gt;&lt;P&gt;Trying to narrow it down at this stage.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Classic 4K:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Type:&lt;/P&gt;&lt;P&gt;MIFARE Classic EV1 (MF1S70)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Information:&lt;/P&gt;&lt;P&gt;Full product name: MF1S703xX/V1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Classic 1K:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Type:&lt;/P&gt;&lt;P&gt;MIFARE Classic (MF1S50)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Information:&lt;/P&gt;&lt;P&gt;Full product name: MF1S5037&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Mon, 20 May 2024 03:39:16 GMT</pubDate>
    <dc:creator>dmaher</dc:creator>
    <dc:date>2024-05-20T03:39:16Z</dc:date>
    <item>
      <title>Mifare Classic EV1 4K Compatibility</title>
      <link>https://community.nxp.com/t5/NFC/Mifare-Classic-EV1-4K-Compatibility/m-p/1868529#M11702</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;&lt;BR /&gt;Currently troubleshooting an issue with a device, it has no issue reading older issue Mifare Classic 1K cards, however is having delayed or intermittent reads with a newer batch of Classic EV1 4K cards.&lt;BR /&gt;&lt;BR /&gt;These devices were produced in 2013 and have no available firmware updates, I noticed the EV1 cards were released 2018.&lt;BR /&gt;&lt;BR /&gt;Is there anything known that would cause compatibility issues with these newer revision EV1 cards?&lt;BR /&gt;&lt;BR /&gt;The other potential avenue being investigated is the device having an issue with the additional sectors and block size with the 4K cards.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;There are other devices on site that have no issue with either card, however they have had firmware updates or newer manufacture dates.&lt;/P&gt;&lt;P&gt;Trying to narrow it down at this stage.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Classic 4K:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Type:&lt;/P&gt;&lt;P&gt;MIFARE Classic EV1 (MF1S70)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Information:&lt;/P&gt;&lt;P&gt;Full product name: MF1S703xX/V1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Classic 1K:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Type:&lt;/P&gt;&lt;P&gt;MIFARE Classic (MF1S50)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;# IC Information:&lt;/P&gt;&lt;P&gt;Full product name: MF1S5037&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 20 May 2024 03:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Mifare-Classic-EV1-4K-Compatibility/m-p/1868529#M11702</guid>
      <dc:creator>dmaher</dc:creator>
      <dc:date>2024-05-20T03:39:16Z</dc:date>
    </item>
    <item>
      <title>Re: Mifare Classic EV1 4K Compatibility</title>
      <link>https://community.nxp.com/t5/NFC/Mifare-Classic-EV1-4K-Compatibility/m-p/1870056#M11711</link>
      <description>&lt;P lang="es-MX"&gt;This is Fabian, I've been assigned to support your case.&lt;/P&gt;
&lt;P lang="es-MX"&gt;I appreciate your interest in our products.&lt;/P&gt;
&lt;P lang="es-MX"&gt;There should not be any variations when reading any MIFARE cards. Even if they are Classic of DESFire, the application Reads and Writes in a Classic card should do the same regardless of the year it was released. This is because all MIFARE cards comply with ISO 14443 specifications.&lt;/P&gt;
&lt;P lang="es-MX"&gt;Could you please provide a little more information? What reader are you using, if you using a host, an MCU, or an Operative System?&lt;/P&gt;</description>
      <pubDate>Tue, 21 May 2024 22:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Mifare-Classic-EV1-4K-Compatibility/m-p/1870056#M11711</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2024-05-21T22:33:11Z</dc:date>
    </item>
  </channel>
</rss>