<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックManipulate Keystore File from Card Test Framework</title>
    <link>https://community.nxp.com/t5/NFC/Manipulate-Keystore-File-from-Card-Test-Framework/m-p/1860550#M11661</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;using the &lt;EM&gt;Card Test Framework&lt;/EM&gt; it is possible to export/import .key files. Hereby it is easy for me to test a DESFire Card "Layout" where I can export keys from the &lt;EM&gt;Card Test Framework&lt;/EM&gt; and import it to &lt;EM&gt;RFIDDiscover&lt;/EM&gt; and vice-versa.&lt;/P&gt;&lt;P&gt;Unfortunately I can only open and read/write this Keystore file using the two programs.However, I would really want to get keys from a third source, write it to a .key file and then open it using the &lt;EM&gt;NXP Card Test Framework&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;It seems that the .key file is some binary data stream export from some .NET classes. Is there a wrapper from NXP or an class definition?&lt;/P&gt;&lt;P&gt;Tanks for any help!&lt;/P&gt;</description>
    <pubDate>Tue, 07 May 2024 13:01:32 GMT</pubDate>
    <dc:creator>johannesdev</dc:creator>
    <dc:date>2024-05-07T13:01:32Z</dc:date>
    <item>
      <title>Manipulate Keystore File from Card Test Framework</title>
      <link>https://community.nxp.com/t5/NFC/Manipulate-Keystore-File-from-Card-Test-Framework/m-p/1860550#M11661</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;using the &lt;EM&gt;Card Test Framework&lt;/EM&gt; it is possible to export/import .key files. Hereby it is easy for me to test a DESFire Card "Layout" where I can export keys from the &lt;EM&gt;Card Test Framework&lt;/EM&gt; and import it to &lt;EM&gt;RFIDDiscover&lt;/EM&gt; and vice-versa.&lt;/P&gt;&lt;P&gt;Unfortunately I can only open and read/write this Keystore file using the two programs.However, I would really want to get keys from a third source, write it to a .key file and then open it using the &lt;EM&gt;NXP Card Test Framework&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;It seems that the .key file is some binary data stream export from some .NET classes. Is there a wrapper from NXP or an class definition?&lt;/P&gt;&lt;P&gt;Tanks for any help!&lt;/P&gt;</description>
      <pubDate>Tue, 07 May 2024 13:01:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Manipulate-Keystore-File-from-Card-Test-Framework/m-p/1860550#M11661</guid>
      <dc:creator>johannesdev</dc:creator>
      <dc:date>2024-05-07T13:01:32Z</dc:date>
    </item>
    <item>
      <title>Re: Manipulate Keystore File from Card Test Framework</title>
      <link>https://community.nxp.com/t5/NFC/Manipulate-Keystore-File-from-Card-Test-Framework/m-p/1861948#M11669</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/146905"&gt;@johannesdev&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;My apologies, there is no information available about modifying or creating compatible .key files to work with these tools, as this may be a security topic and we do not have access to this information.&lt;/P&gt;
&lt;P&gt;I truly apologize for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 08 May 2024 22:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Manipulate-Keystore-File-from-Card-Test-Framework/m-p/1861948#M11669</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-05-08T22:20:35Z</dc:date>
    </item>
  </channel>
</rss>