<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN7642 SPI host interface not working with NxPNfcRdlib in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7642-SPI-host-interface-not-working-with-NxPNfcRdlib/m-p/1857821#M11632</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180883"&gt;@asknxp&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;I just sent you a private Community message.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Tue, 30 Apr 2024 21:17:30 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2024-04-30T21:17:30Z</dc:date>
    <item>
      <title>PN7642 SPI host interface not working with NxPNfcRdlib</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-SPI-host-interface-not-working-with-NxPNfcRdlib/m-p/1857507#M11631</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;
&lt;P&gt;I am using SDK_2.x_board_PNEV7642FAMA SDK(2.12.5) and tested the following examples.&lt;/P&gt;
&lt;P&gt;-&amp;nbsp;pnev7642fama_NfcrdlibEx2_ECP_Freertos_Ecp&lt;/P&gt;
&lt;P&gt;-&amp;nbsp;pnev7642fama_pn76_hostif_spi&lt;/P&gt;
&lt;P&gt;I can test both examples without any issue.&lt;/P&gt;
&lt;P&gt;I tried to combine both examples so that the credential information can be sent to the host(LPC55S16 board) by the SPI bus.&lt;/P&gt;
&lt;P&gt;Here is what I did.&lt;/P&gt;
&lt;P&gt;- modified exiting&amp;nbsp;pnev7642fama_NfcrdlibEx2_ECP_Freertos_Ecp example and add a new freeRTOS thread to run the hostif_spi function(from example pnev7642fama_pn76_hostif_spi). Something like this&lt;/P&gt;
&lt;P&gt;[CODE]&lt;/P&gt;
&lt;P&gt;If I comment out ECP_thread, then&amp;nbsp;LPC55S16 board can send loopback command and receive the response from PN7642 board. As long as I enable&amp;nbsp;ECP_thread, then LPC55S16 board was unable to receive the response from PN7642 but PN7642 was still able to execute ECP functionality properly.&lt;/P&gt;
&lt;P&gt;Any insight?!&lt;/P&gt;
&lt;P&gt;Thank you very much.&lt;/P&gt;
&lt;P&gt;--Kenny&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Apr 2024 21:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-SPI-host-interface-not-working-with-NxPNfcRdlib/m-p/1857507#M11631</guid>
      <dc:creator>asknxp</dc:creator>
      <dc:date>2024-04-30T21:14:40Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 SPI host interface not working with NxPNfcRdlib</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-SPI-host-interface-not-working-with-NxPNfcRdlib/m-p/1857821#M11632</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180883"&gt;@asknxp&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;I just sent you a private Community message.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 30 Apr 2024 21:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-SPI-host-interface-not-working-with-NxPNfcRdlib/m-p/1857821#M11632</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-04-30T21:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 SPI host interface not working with NxPNfcRdlib</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-SPI-host-interface-not-working-with-NxPNfcRdlib/m-p/1857909#M11633</link>
      <description>&lt;P&gt;OK. Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 01 May 2024 06:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-SPI-host-interface-not-working-with-NxPNfcRdlib/m-p/1857909#M11633</guid>
      <dc:creator>asknxp</dc:creator>
      <dc:date>2024-05-01T06:24:12Z</dc:date>
    </item>
  </channel>
</rss>