<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN7160 EMI Problems</title>
    <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1857474#M11629</link>
    <description>&lt;P&gt;Hi&amp;nbsp;michael_d_1983,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We created a case about your issue. Can you confirm that you have access there, please?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 30 Apr 2024 10:29:41 GMT</pubDate>
    <dc:creator>Tomas_Parizek</dc:creator>
    <dc:date>2024-04-30T10:29:41Z</dc:date>
    <item>
      <title>PN7160 EMI Problems</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1853549#M11596</link>
      <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;We are using the PN7160 for the first time in 2 new designs.&lt;/P&gt;&lt;P&gt;Functionality is very good, unfortunately the EMI measurements in both (different) designs show limit violations at 40.68MHz&amp;nbsp;(3rd harmonics) by approx. 3-6dB, occasionally also 67.8MHz and 94.92MHz (5th, 7th harmonics). A (Desfire) card was placed during these tests so the app was in “presence check” mode.&lt;/P&gt;&lt;P&gt;What did we try?&lt;BR /&gt;* Reducing the power by reducing TXLDO to 2.7V (a quarter power)-&amp;gt;&lt;BR /&gt;This only brought a small improvement, if any.&lt;/P&gt;&lt;P&gt;* EMI filter L0/C0 to 14.4MHz instead of 22MHz (without adjusting the rest, or values calculated with the tool) -&amp;gt;&lt;BR /&gt;This only brought a small improvement, if any, or in the higher frequency range.&lt;BR /&gt;TXLDO was set to 2V7, the DPC was not active/configured, current about 190mA.&lt;/P&gt;&lt;P&gt;* Place a series resistor (33R) between PN7160-TX1/TX2 and the inductors.&lt;BR /&gt;Brings improvements in the EMI, very bad functionality, is just nonsense.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;What else could we try or check?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Is it possible to set the slope of TX1 and TX2 via the CLIF_ANA_TX_AMPLITUDE_REG as described in the RF settings guide?&lt;BR /&gt;Can you give me some values that I could try?&lt;/P&gt;&lt;P&gt;Can we reduce the power further by increasing the Z or is there something else to look for?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Are there any other software options for reducing the radiated power?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Our antenna (Rectangular):&lt;BR /&gt;64x38, 3 turns, Flex-PCB (with 40mm feed line, but that should work since we have already gotten other designs through EMI testing with this antenna).&lt;/P&gt;&lt;P&gt;Our matching:&lt;BR /&gt;Asymmetrical matching, DPC not activated, Z = 24R&lt;BR /&gt;LQW18CNR16J0H 160nH / C0 = 330pF&lt;BR /&gt;C1 = 78p, C2 = 122p, Rq = 2R2&lt;/P&gt;&lt;P&gt;Our Config (see attachment):&lt;BR /&gt;# CFG2: VBAT2 to 3V9&lt;BR /&gt;NXP_EXT_TVDD_CFG_2={20, 02, 0F, 01, A0, 0E, 0B, 11, 01, 02, B2, 00, B2, 1E, 9F, 00, D0, 0C}&lt;/P&gt;&lt;P&gt;Measure Current Factoryapp: 5V: Idle: 155mA, with card: 83mA&lt;BR /&gt;Measure Current Factoryapp: 3V9 : Idle: 128mA, with card: 146mA (??)&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="00 Antenne eingebaut vermessen mit VNA.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275581i763DB54DFF65D349/image-size/medium?v=v2&amp;amp;px=400" role="button" title="00 Antenne eingebaut vermessen mit VNA.png" alt="00 Antenne eingebaut vermessen mit VNA.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20 Matching 78p 122p 2R2 xx.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275582iA9340392AA1E11EA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="20 Matching 78p 122p 2R2 xx.PNG" alt="20 Matching 78p 122p 2R2 xx.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="michael_d_1983_0-1713970392277.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/275583i8FED23A92BB9FE10/image-size/medium?v=v2&amp;amp;px=400" role="button" title="michael_d_1983_0-1713970392277.png" alt="michael_d_1983_0-1713970392277.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Mon, 29 Apr 2024 14:55:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1853549#M11596</guid>
      <dc:creator>michael_d_1983</dc:creator>
      <dc:date>2024-04-29T14:55:57Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 EMI Problems</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1856468#M11611</link>
      <description>&lt;P&gt;Hello Michael,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have you already seen these two documents?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;--&amp;gt;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13892.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/application-note/AN13892.pdf&lt;/A&gt;&amp;nbsp;--&amp;gt;&amp;nbsp;&lt;STRONG&gt;7 How to support/pass ETSI and FCC tests&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;--&amp;gt;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12988.pdf" target="_blank" rel="noopener"&gt;https://www.nxp.com/docs/en/application-note/AN12988.pdf&lt;/A&gt;&amp;nbsp;--&amp;gt;&amp;nbsp;&lt;STRONG&gt;11 Radiated Spurious Emissions&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;These two chapters could help.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;However, I don´t think that we will fully solve the issue by reducing the output power by register settings.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Imagine that the drop of 3dB is 50% of the power.&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;We need to check layout, especially the NFC part. Can you share the full design files, please? (Layout + schematic).&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;Slightly increase the C0 capacitors to have more symmetrical tuning&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;Do you have some EMI measurements without a DESfire card? Just RF ON or Polling ? It would be interesting to see the EMI radiation for nominal tuning.&amp;nbsp;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;About the layout. What is the loop I marked with green?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_0-1714370274530.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276389i19C1999D9E47FAB7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_0-1714370274530.png" alt="Tomas_Parizek_0-1714370274530.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Apr 2024 17:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1856468#M11611</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-04-29T17:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 EMI Problems</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1856801#M11620</link>
      <description>&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;I tested the whole thing without a card in the RF field via NfcFactoryApp PRBS / Type A / 106 kBit (or is there another way to switch to card polling with 100% duty cycle?).&lt;/P&gt;&lt;P&gt;The result is better here.&lt;BR /&gt;According to our findings, the whole thing depends not only on whether a card or token is in the field, but also on how it is positioned (orientation).&lt;/P&gt;&lt;P&gt;EMI filter L0/C0 to 14.4MHz instead of 22MHz (without adjusting the rest, or values calculated with the tool) -&amp;gt; This only brought a small improvement, if any, or in the higher frequency range.&lt;/P&gt;&lt;P&gt;Our idea was to be able to adjust the slope of TX1 and TX2 via a register. For example via the TX_GSN_CW_RM or TX_GSN_MOD_RM settings. If that makes any sense.&lt;/P&gt;&lt;P&gt;The marked loop is GND which was drawn manually because the layout flood engine does not fill everything here.&lt;/P&gt;&lt;P&gt;I will attach the layout data in our case.&lt;BR /&gt;The circuit diagram can also already be found there. (Please note that the “VNA-optimized” capacitor values are not yet entered in the circuit diagram)&lt;BR /&gt;If you need anything else let me know!&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;P&gt;Measure NfcFactoryApp PRBS / Type A / 106 kBit / 2V7 / No Card&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="michael_d_1983_0-1714401104536.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/276473i59A9BC0E7A055D63/image-size/medium?v=v2&amp;amp;px=400" role="button" title="michael_d_1983_0-1714401104536.png" alt="michael_d_1983_0-1714401104536.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Apr 2024 14:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1856801#M11620</guid>
      <dc:creator>michael_d_1983</dc:creator>
      <dc:date>2024-04-29T14:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 EMI Problems</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1857474#M11629</link>
      <description>&lt;P&gt;Hi&amp;nbsp;michael_d_1983,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We created a case about your issue. Can you confirm that you have access there, please?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Apr 2024 10:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1857474#M11629</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-04-30T10:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 EMI Problems</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1857483#M11630</link>
      <description>&lt;P&gt;Hello Tomas,&lt;/P&gt;&lt;P&gt;yes, I can confirm.&lt;BR /&gt;I have uploaded the circuit diagram and layout there.&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
      <pubDate>Tue, 30 Apr 2024 10:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/1857483#M11630</guid>
      <dc:creator>michael_d_1983</dc:creator>
      <dc:date>2024-04-30T10:47:22Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 EMI Problems</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/2164665#M13581</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I’m having a similar problem. Could you please share the solution if you’ve found one? Thanks.&lt;/P&gt;</description>
      <pubDate>Sat, 06 Sep 2025 13:47:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/2164665#M13581</guid>
      <dc:creator>utqq</dc:creator>
      <dc:date>2025-09-06T13:47:56Z</dc:date>
    </item>
    <item>
      <title>Re: PN7160 EMI Problems</title>
      <link>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/2164887#M13585</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254508"&gt;@utqq&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;The previous case was related to the combination of high TX power and very good coupling between the NFC Reader Antenna and the NFC Card.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;The solution was&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;-&amp;gt; Reduce TX power by reducing the TXLDO and RF Settings (TVDD Amplitude)&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;-&amp;gt; If needed, further reduce by GSN settings:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/PN7160-How-to-reduce-output-power-using-DPC-Reader-Mode/ta-p/1884989" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/NFC-Knowledge-Base/PN7160-How-to-reduce-output-power-using-DPC-Reader-Mode/ta-p/1884989&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;-&amp;gt; Consider a smaller TX antenna or increase the distance between TX and NFC Coard cantenna.&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;UPDATE:&lt;/STRONG&gt; Seeing your actual issue (&lt;A href="https://community.nxp.com/t5/NFC/PN5190-EMI-Problem-Harmonic/m-p/2164669#M13582" target="_blank"&gt;https://community.nxp.com/t5/NFC/PN5190-EMI-Problem-Harmonic/m-p/2164669#M13582&lt;/A&gt;)&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The problem seems to be at higher frequencies. That is typically related to NFC Reader mathcing and layout.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check the following document -&amp;gt;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12988.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12988.pdf&lt;/A&gt;&amp;nbsp;, chapter&amp;nbsp;9 Radiated Spurious Emissions.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The measures are valid for PN5190 as well.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Sep 2025 05:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7160-EMI-Problems/m-p/2164887#M13585</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2025-09-08T05:57:50Z</dc:date>
    </item>
  </channel>
</rss>