<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: OM27160 raspberry i2c NfcService Init Failed</title>
    <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1856746#M11619</link>
    <description>guys, I had no time to perform the full install and try to use the driver which I believe can change something.&lt;BR /&gt;At the same time what is marked as solution, does not solve anything. If you read my description, I have no problem talking to different devices using I2C. So the marked solution solves only the problem it created itself by disabling I2C.</description>
    <pubDate>Mon, 29 Apr 2024 12:53:07 GMT</pubDate>
    <dc:creator>paweljasinski</dc:creator>
    <dc:date>2024-04-29T12:53:07Z</dc:date>
    <item>
      <title>OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825250#M11431</link>
      <description>&lt;P&gt;I have a OM27160A1HN connected to raspberry pi.&lt;/P&gt;&lt;P&gt;I have followed the instructions for i2c from &lt;A href="https://www.nxp.com/docs/en/application-note/AN12991.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12991.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;When I run "nfcDemoApp poll", I get the "NfcService Init Failed".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What I tried so far:&lt;/P&gt;&lt;P&gt;I have double checked the board and it is i2c and not spi.&lt;/P&gt;&lt;P&gt;Scanning of the i2c with "i2cdetect -y 1" does not show anything.&lt;/P&gt;&lt;P&gt;I have tried with 2 different raspberries, which are knows to work with other i2c devices.&lt;/P&gt;&lt;P&gt;I have enabled debug, log is attached.&lt;/P&gt;&lt;P&gt;Any idea what should I check now?&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 14:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825250#M11431</guid>
      <dc:creator>paweljasinski</dc:creator>
      <dc:date>2024-03-11T14:26:39Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825598#M11434</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230768"&gt;@paweljasinski&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please refer to the &lt;A href="https://www.nxp.com/docs/en/application-note/AN13287.pdf" target="_blank"&gt;PN7160 Linux porting guide&lt;/A&gt;? This document describes in detail how to add support for a PN7160 controller to a generic GNU/Linux system.&lt;/P&gt;
&lt;P&gt;Regards.&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 01:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825598#M11434</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-03-12T01:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825888#M11437</link>
      <description>&lt;P&gt;Hello Pawel,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you check the &lt;STRONG&gt;libnfc-nxp.conf&lt;/STRONG&gt;, please?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;You need to set the I2C alternative driver also here:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_0-1710230229143.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267737iAE91108295114407/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_0-1710230229143.png" alt="Tomas_Parizek_0-1710230229143.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So for I2C -&amp;gt; NXP_TRANSPORT=&lt;STRONG&gt;0x02&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 07:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825888#M11437</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-03-12T07:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825975#M11438</link>
      <description>The setting are correct. I will attach strace log which shows opening /dev/i2c-1</description>
      <pubDate>Tue, 12 Mar 2024 09:05:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825975#M11438</guid>
      <dc:creator>paweljasinski</dc:creator>
      <dc:date>2024-03-12T09:05:57Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825992#M11439</link>
      <description>&lt;P&gt;here is the relevant snipped from the config. The config was changed before building.&lt;/P&gt;&lt;P&gt;NXP_TRANSPORT=0x02&lt;/P&gt;&lt;P&gt;###############################################################################&lt;BR /&gt;# Nfc Device Node name&lt;BR /&gt;NXP_NFC_DEV_NODE="/dev/i2c-1"&lt;/P&gt;&lt;P&gt;The strace file shows that the correct file is open. I have selected only the log from interesting thread.&lt;/P&gt;&lt;P&gt;The command was: "strace -ff -o strace.log nfcDemoApp poll"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 09:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825992#M11439</guid>
      <dc:creator>paweljasinski</dc:creator>
      <dc:date>2024-03-12T09:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825994#M11440</link>
      <description>&lt;P&gt;Is it possible that the 7160 is missing firmware or has a wrong firmware?&lt;/P&gt;&lt;P&gt;Would trying with SPI help?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 09:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1825994#M11440</guid>
      <dc:creator>paweljasinski</dc:creator>
      <dc:date>2024-03-12T09:18:32Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1828401#M11455</link>
      <description>&lt;P&gt;Hello Pawel,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Ok, I see. Let me grab one Raspberry Pi and check with PN7160 on my side.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BTW. Are you using a raspberry Pi "shield" or are you using a cable connection?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Mar 2024 11:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1828401#M11455</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-03-14T11:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1831298#M11473</link>
      <description>&lt;P&gt;Hello Pawel,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I just tested with the Raspberry Pi on my side&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I exactly followed the instructions listed in the App. Note you have mentioned.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Here is the result:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_0-1710863994273.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/269273iE41EC9C207406EF7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_0-1710863994273.png" alt="Tomas_Parizek_0-1710863994273.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can see that for the first time, I also got the "&lt;STRONG&gt;NfcService Init Failed&lt;/STRONG&gt;" error message as you.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So I removed the PN7160 from the socket and put it back + I checked if the I2C was enabled.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Then the NFC application started to work as you can see in the picture.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Here is the information about HW that I am using:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_1-1710864521904.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/269275iC19035E86B0A98D5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_1-1710864521904.png" alt="Tomas_Parizek_1-1710864521904.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also, one more thing I did at the beginning. I enabled the I2C in preferences:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_2-1710864679129.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/269277iB504DB1711F138C7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_2-1710864679129.png" alt="Tomas_Parizek_2-1710864679129.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Mar 2024 16:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1831298#M11473</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-03-19T16:12:02Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1856746#M11619</link>
      <description>guys, I had no time to perform the full install and try to use the driver which I believe can change something.&lt;BR /&gt;At the same time what is marked as solution, does not solve anything. If you read my description, I have no problem talking to different devices using I2C. So the marked solution solves only the problem it created itself by disabling I2C.</description>
      <pubDate>Mon, 29 Apr 2024 12:53:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1856746#M11619</guid>
      <dc:creator>paweljasinski</dc:creator>
      <dc:date>2024-04-29T12:53:07Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1894218#M11853</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201669"&gt;@Tomas_Parizek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the same issue. I've checked the I2C, unplugged and rebooted multiple times but I always get the "NfcService Init Failed". Do you have any more suggestions I could try to get my setup running?&lt;/P&gt;&lt;P&gt;The error message is the same whether the OM27160 is plugged in or not. Is there a easy way to verify whether the PN7160 is responding? Maybe my hardware has some defect?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Stephan&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 08:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1894218#M11853</guid>
      <dc:creator>Stephan_B</dc:creator>
      <dc:date>2024-06-26T08:20:11Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1895137#M11861</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;A id="link_6" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235524" target="_self" aria-label="View Profile of Stephan_B"&gt;&lt;SPAN class=""&gt;Stephan_B&lt;/SPAN&gt;&lt;/A&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you share more details about your setup.... what Raspberry and OS are you using, please?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It seems that the latest Raspberry has an issue with our PN7160, our SW team is already checking that.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Jun 2024 11:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1895137#M11861</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-06-27T11:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1901877#M11904</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201669"&gt;@Tomas_Parizek&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;I used a tried with a Raspberry Pi 5 as well as with a Raspberry Pi 3 B+. I tested both 32 and 64bit versions. Though when compiling for the 64bit version I needed to correct some of the code as I later found in the 64bit patch file.&lt;BR /&gt;I then assumed, that it is a HW problem, as I can see the I2C signals being sent with the oscilloscope. So I bought another EvalBoard, but it still not working.&lt;BR /&gt;"NfcService Init Failed"&lt;BR /&gt;"Leaving ..."&lt;BR /&gt;is all i get. As for the OS, I am working with Rasbian. I use the Raspberry Shield, that came with the Developmentkit and setup/installed everything via the Terminal (SSH/Putty)&lt;BR /&gt;&lt;BR /&gt;Regards Stephan&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jul 2024 11:50:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1901877#M11904</guid>
      <dc:creator>Stephan_B</dc:creator>
      <dc:date>2024-07-08T11:50:27Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1903832#M11920</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201669"&gt;@Tomas_Parizek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Today, I got my setup working. I had to install an old Rasbian version (bullseye) and then it compiled without error and it works.&lt;/P&gt;&lt;P&gt;Would have been nice to have some pointers in the "get started guide" concerning which OS / HW versions this has been tested with.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Stephan&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jul 2024 08:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1903832#M11920</guid>
      <dc:creator>Stephan_B</dc:creator>
      <dc:date>2024-07-09T08:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1920576#M11980</link>
      <description>&lt;P&gt;***UPDATE***&lt;/P&gt;
&lt;P&gt;--&amp;gt; See the fix&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/Porting-PN7160-NCI2-stack-to-Raspberry-Pi-5-OS-Bookworm/ta-p/1977521" target="_blank"&gt;https://community.nxp.com/t5/NFC-Knowledge-Base/Porting-PN7160-NCI2-stack-to-Raspberry-Pi-5-OS-Bookworm/ta-p/1977521&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;We see that the PN7160 returns "NfcService Init Failed" for latest Raspian Linux version 12 (Bookworm).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For Linux version 11 (bullseye), the issue should not occur.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomas_Parizek_0-1722347889218.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/290996i7E7E9D0D7EF85E63/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomas_Parizek_0-1722347889218.png" alt="Tomas_Parizek_0-1722347889218.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;NXP is working to fix it as as soon as possible.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Feb 2025 12:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1920576#M11980</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2025-02-11T12:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1988106#M12297</link>
      <description>&lt;P&gt;Has this been resolved to work on the latest Pi releases?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--Ken&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 16:24:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/1988106#M12297</guid>
      <dc:creator>KennyG</dc:creator>
      <dc:date>2024-11-05T16:24:12Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2005117#M12369</link>
      <description>&lt;P&gt;Hello &lt;A id="link_70" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241955" target="_self" aria-label="View Profile of KennyG"&gt;&lt;SPAN class=""&gt;KennyG&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;and&amp;nbsp;&lt;A id="link_94" class="lia-link-navigation lia-page-link lia-user-name-link" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235524" target="_self" aria-label="View Profile of Stephan_B"&gt;&lt;SPAN class=""&gt;Stephan_B&lt;/SPAN&gt;&lt;/A&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The solution is already in place. My colleague will share it via NXP NFC Knowladge base.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I will also update the link here soon.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 11:21:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2005117#M12369</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2024-12-02T11:21:18Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2156978#M13546</link>
      <description>Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201669"&gt;@Tomas_Parizek&lt;/a&gt;&lt;BR /&gt;&lt;BR /&gt;I am in a similar position as the above. I found the patch file and still running into issues when I run nfcDemoApp poll. When I run sudo i2cdetect -y 1 it shows none of the pins are detected. I determined the raspberry pi is not fried because I am using with other setups and it worked. So what other things can I try to patch to get the pi to detect the NFC controller?</description>
      <pubDate>Sat, 23 Aug 2025 02:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2156978#M13546</guid>
      <dc:creator>mikytron98</dc:creator>
      <dc:date>2025-08-23T02:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2156987#M13547</link>
      <description>&lt;P&gt;For context, I am getting the same:&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NfcService Init Failed&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;and have been following the Elechouse Quick start guide.&lt;/P&gt;&lt;P&gt;I am access the Pi via SSH from my mac that has M2 chip. Some additional context that can help pinpoint what is going on here.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mikytron98_0-1755915990215.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353734iE080554F12979E24/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mikytron98_0-1755915990215.png" alt="mikytron98_0-1755915990215.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mikytron98_1-1755916050409.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/353735i956BC66976148C25/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mikytron98_1-1755916050409.png" alt="mikytron98_1-1755916050409.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 23 Aug 2025 02:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2156987#M13547</guid>
      <dc:creator>mikytron98</dc:creator>
      <dc:date>2025-08-23T02:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2158797#M13555</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254041"&gt;@mikytron98&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you share more details about your setup? Which Raspberry Pi and Linux version are you using?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 06:05:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2158797#M13555</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2025-08-27T06:05:04Z</dc:date>
    </item>
    <item>
      <title>Re: OM27160 raspberry i2c NfcService Init Failed</title>
      <link>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2166017#M13589</link>
      <description>&lt;P class=""&gt;&lt;STRONG&gt;Setup Details:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Raspberry Pi 5 running Debian (kernel 6.12.25+rpt-rpi-2712, aarch64)&lt;/LI&gt;&lt;LI&gt;Using linux_libnfc-nci library for NXP NFC chips&lt;/LI&gt;&lt;LI&gt;I2C enabled with buses at /dev/i2c-1, /dev/i2c-13, /dev/i2c-14&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;&lt;STRONG&gt;Current Issue:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;sudo i2cdetect -y 1 shows no devices (all "--")&lt;/LI&gt;&lt;LI&gt;nfcDemoApp compiles but fails with "NfcService Init Failed"&lt;/LI&gt;&lt;LI&gt;Also getting C++ std::out_of_range exception in strings.cpp&lt;/LI&gt;&lt;/UL&gt;&lt;P class=""&gt;The I2C scan suggests no NFC hardware is detected on bus 1. Either the module isn't connected properly or I2C isn't configured correctly for the NFC chip.&lt;/P&gt;&lt;P class=""&gt;I made progress when I used a forked branch of the source code but it seems you guys have a version of the source code that works saved privately somewhere based on another conversation I saw&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/369"&gt;@danielchen&lt;/a&gt;&amp;nbsp;reply in&lt;/P&gt;</description>
      <pubDate>Tue, 09 Sep 2025 15:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/OM27160-raspberry-i2c-NfcService-Init-Failed/m-p/2166017#M13589</guid>
      <dc:creator>mikytron98</dc:creator>
      <dc:date>2025-09-09T15:25:54Z</dc:date>
    </item>
  </channel>
</rss>