<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?</title>
    <link>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1818078#M11375</link>
    <description>&lt;P&gt;Hello sir,&lt;BR /&gt;My recommendation when using DPC is to please follow AN11742 steps, you can start with a 3kΩ and adjust, If the AGC value is too high, increase the Rx resistor value.&lt;/P&gt;</description>
    <pubDate>Wed, 28 Feb 2024 23:25:46 GMT</pubDate>
    <dc:creator>Fabian_R</dc:creator>
    <dc:date>2024-02-28T23:25:46Z</dc:date>
    <item>
      <title>PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1816521#M11362</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I am immersed in the process of optimizing the receiver&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt; but I´m a little confused about it.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;AN11740 - 4.5.1 External RX components says&lt;/EM&gt; to increase R1A and R1B if AGC_VALUE is low (&amp;lt;250)&lt;/P&gt;&lt;P&gt;but AN11742 says:&lt;/P&gt;&lt;P&gt;-&lt;EM&gt;1.2.4.1 Step 1: Unloaded.&lt;/EM&gt; The Rx resistor was chosen to be R = 3.0 kΩ. The measurement shows the AGC value of 369 in gear 0, driving ITVDD = 139mA (unloaded). The recommended AGC value is 300, so in this case the Rx resistor could be slightly increased.&lt;/P&gt;&lt;P&gt;-&lt;EM&gt;7 Annex, Table 13&lt;/EM&gt; "The Rx resistor = 5.1kΩ, so the nominal AGC value unloaded is too low."&lt;/P&gt;&lt;P&gt;-7&lt;EM&gt; Annex&lt;/EM&gt;&amp;nbsp; ...However, here the AGC values are lower, since a higher Rx coupling resistor has been used."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;So, should I increase or decrease the coupling resistors if AGC_VALUE is low (=139)?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Currently, the chosen resistor are 4.7kOhm, as recomended as starting point.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 11:42:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1816521#M11362</guid>
      <dc:creator>oferrer</dc:creator>
      <dc:date>2024-02-27T11:42:37Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1816878#M11367</link>
      <description>&lt;P&gt;Hello sir,&lt;/P&gt;
&lt;P&gt;Please keep in mind that these are recommendations that may vary on your design and requirements.&amp;nbsp; These component values should be selected according to the antenna characteristics and your measurements.&lt;/P&gt;
&lt;P&gt;Please take a look at our &lt;A href="https://community.nxp.com/t5/NFC/bd-p/nfc" target="_blank"&gt;NFC Antenna Tool&lt;/A&gt; for a quick recommendation of the components of your antenna.&lt;/P&gt;
&lt;P&gt;I also want to recommend to please take a look at our &lt;A href="https://www.nxp.com/design/training/nfc-antenna-design:TIP-NFC-ANTENNA-DESIGN" target="_blank"&gt;Antenna design video series&lt;/A&gt; which shows the iterative process for successfully designing your matching circuit along with the proper calibration and, fine-tuning using &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-cockpit-configuration-tool-for-nfc-ics:NFC-COCKPIT" target="_blank"&gt;NFC Cockpit&lt;/A&gt;.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 22:23:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1816878#M11367</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2024-02-27T22:23:47Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1816886#M11368</link>
      <description>&lt;P&gt;Thanks &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158520"&gt;@Fabian_R&lt;/a&gt;&amp;nbsp; for your answer.&lt;/P&gt;&lt;P&gt;My circuit board (prototype) is already printed with pn5180 and a customized antenna on it. NFC Antenna Tool was used for maths (no RX resistor calculated). Now, it's running well.&amp;nbsp;&lt;/P&gt;&lt;P&gt;As i said, i'm optimizing receiver before production. I need to change RX external resistors (1kohm-10kohm) to get optimal AGC_VALUE 600 (ANT1/ANT2 were not connected, pure read mode).&lt;/P&gt;&lt;P&gt;I need to increase AGC_VALUE. That's why my question.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Should I increase or decrease external coupling resistors in order to increase AGC_VALUE?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Is there any contradiction between AN11740 4.5.1 AND (AN11742 Table 5 Example OR AN11742&amp;nbsp; Table 13 Example)?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Osmany&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 01:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1816886#M11368</guid>
      <dc:creator>oferrer</dc:creator>
      <dc:date>2024-02-28T01:35:09Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1818078#M11375</link>
      <description>&lt;P&gt;Hello sir,&lt;BR /&gt;My recommendation when using DPC is to please follow AN11742 steps, you can start with a 3kΩ and adjust, If the AGC value is too high, increase the Rx resistor value.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 23:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1818078#M11375</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2024-02-28T23:25:46Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Should I increase or decrease the coupling resistors to increase AGC_VALUE?</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1819127#M11378</link>
      <description>&lt;P&gt;Thanks &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/158520"&gt;@Fabian_R&lt;/a&gt; for your answer,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I had to use an even lower value (2,2kΩ) to get the minimum AGC_VALUE required.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Maybe this low value has to do with the selected high target impedance (battery powered handheld device).&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;STRONG&gt;So, i had to decrease coupling resistor in order to increase AGC_VALUE&lt;/STRONG&gt;. DPC calibration is now done.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thanks again.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Osmany&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 02:13:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Should-I-increase-or-decrease-the-coupling-resistors-to/m-p/1819127#M11378</guid>
      <dc:creator>oferrer</dc:creator>
      <dc:date>2024-03-01T02:13:14Z</dc:date>
    </item>
  </channel>
</rss>