<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: Can NFC Reader Library support for MFRC522</title>
    <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1801764#M11245</link>
    <description>&lt;P&gt;HI!&lt;BR /&gt;Could I get the sample code as well?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Mon, 05 Feb 2024 09:02:27 GMT</pubDate>
    <dc:creator>AP1</dc:creator>
    <dc:date>2024-02-05T09:02:27Z</dc:date>
    <item>
      <title>Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1340424#M8850</link>
      <description>&lt;P&gt;Dear Support,&lt;/P&gt;&lt;P&gt;We have a project that needs to use MFRC522 as reader IC. We already have the experience with using NFC Reader Library&amp;nbsp;v06.10.00, working with CLRC663 to host NXP/ST32L 32-bit ARM MCU and runs very well.&lt;/P&gt;&lt;P&gt;My question is:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Does the NFC Reader Library support the MFRC522 reader IC?&lt;/LI&gt;&lt;LI&gt;If NFC Reader Library doesn't support MFRC522, is there any library or sample code that you can provide us to implement the MFRC522 functions?&lt;/LI&gt;&lt;LI&gt;If there are samples or libraries for MFRCF522, can these codes run on 8-bit MCU? or only supports on 32-bit MCU platform?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I search relative topics below but not found the answer:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/Make-the-NFC-reader-library-easier-to-read-by-removing-folders/ta-p/1129953" target="_blank"&gt;Make the NFC reader library easier to read, by rem... - NXP Community&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/NFC/NFC-Library-for-MFRC522/m-p/466257" target="_blank"&gt;NFC Library for MFRC522 - NXP Community&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/RC522-RFID-Library-in-C-for-MCUXpresso-LPC845/m-p/1159305#M2786" target="_blank"&gt;Solved: RC522 RFID Library in C for MCUXpresso? - LPC845 - NXP Community&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;David Huang&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 08:27:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1340424#M8850</guid>
      <dc:creator>david13</dc:creator>
      <dc:date>2021-09-15T08:27:53Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341018#M8857</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes,&amp;nbsp; NFC Reader Library can't support for MFRC522.&amp;nbsp;&lt;SPAN&gt;but I have some sample code for it, I will send it via email to you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;PS:MFRC522 is not recommended for new designs. For new designs, please use recommended product&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/clrc663-iplus-i-family-high-performance-nfc-frontends:CLRC66303HN" target="_blank"&gt;CLRC663&amp;nbsp;&lt;I&gt;plus&lt;/I&gt;&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a nice day.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 02:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341018#M8857</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-09-16T02:14:02Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341162#M8859</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your prompt reply. I got the sample code you sent via Email.&lt;/P&gt;&lt;P&gt;I reviewed the sample code and knows it supports MIFARE Classic card. If possible, can you also provide the sample code for manipulating the MIFARE DESFire and MIFARE Ultralight card?&amp;nbsp;&lt;/P&gt;&lt;P&gt;The reason why we use MFRC522 instead of CLRC663 is that the lead time of ARM MCU required by CLRC663 NFC Reader Library are 52 weeks or longer in Taiwan. Not like CLRC663, the MFRC522 can be implemented by 8-bit MCU, which has not the lead time issue.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;David Huang&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 05:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341162#M8859</guid>
      <dc:creator>david13</dc:creator>
      <dc:date>2021-09-16T05:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341291#M8860</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your prompt reply. I got the sample code you sent via Email.&lt;/P&gt;&lt;P&gt;I reviewed the sample code and knows it supports MIFARE Classic card. If possible, can you also provide the sample code for manipulating the MIFARE DESFire and MIFARE Ultralight card?&amp;nbsp;&lt;/P&gt;&lt;P&gt;The reason why we use MFRC522 instead of CLRC663 is that the lead time of ARM MCU required by CLRC663 NFC Reader Library are 52 weeks or longer in Taiwan. Not like CLRC663, the MFRC522 can be implemented by 8-bit MCU, which has not the lead time issue.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;David Huang&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 06:56:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341291#M8860</guid>
      <dc:creator>david13</dc:creator>
      <dc:date>2021-09-16T06:56:48Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341377#M8861</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-family: inherit;"&gt;Unfortunately, There's nothing else except the example code I sent you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-family: inherit;"&gt;Have a nice day.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 08:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1341377#M8861</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-09-16T08:13:08Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1400518#M9118</link>
      <description>&lt;P&gt;Could you please share the sample code for the MFRC522?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jan 2022 23:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1400518#M9118</guid>
      <dc:creator>pablollanos</dc:creator>
      <dc:date>2022-01-17T23:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1457783#M9434</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;fangfang,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you send me the example code to me, please?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Hugh Lin&lt;/P&gt;</description>
      <pubDate>Fri, 13 May 2022 08:29:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1457783#M9434</guid>
      <dc:creator>TecomHugh</dc:creator>
      <dc:date>2022-05-13T08:29:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1764855#M11021</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;fangfang,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you send me the example code to me, please?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alex&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 10:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1764855#M11021</guid>
      <dc:creator>A_C</dc:creator>
      <dc:date>2023-11-28T10:46:43Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1801366#M11243</link>
      <description>&lt;P&gt;Could you please send me the example code on my email ?&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 04 Feb 2024 08:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1801366#M11243</guid>
      <dc:creator>Mr7</dc:creator>
      <dc:date>2024-02-04T08:03:41Z</dc:date>
    </item>
    <item>
      <title>Re: Can NFC Reader Library support for MFRC522</title>
      <link>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1801764#M11245</link>
      <description>&lt;P&gt;HI!&lt;BR /&gt;Could I get the sample code as well?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 05 Feb 2024 09:02:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Can-NFC-Reader-Library-support-for-MFRC522/m-p/1801764#M11245</guid>
      <dc:creator>AP1</dc:creator>
      <dc:date>2024-02-05T09:02:27Z</dc:date>
    </item>
  </channel>
</rss>