<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RC522, ATQA and valid bits. Pls explain. in NFC</title>
    <link>https://community.nxp.com/t5/NFC/RC522-ATQA-and-valid-bits-Pls-explain/m-p/1788729#M11170</link>
    <description>&lt;P&gt;I am using from beginning an arduino example converted to C. The MCU has a RC522 connected to it and using SPI as communication method.&amp;nbsp;No collision handling or authentication is needed.&amp;nbsp;The device only checks that the PICC can send its UID (it's a production test)&lt;/P&gt;&lt;P&gt;The call chain is:&amp;nbsp;&lt;STRONG&gt;PICC_IsNewCardPresent&lt;/STRONG&gt; -&amp;gt;&amp;nbsp;&lt;STRONG&gt;PICC_RequestA&lt;/STRONG&gt; -&amp;gt;&amp;nbsp;&lt;STRONG&gt;PICC_REQA_or_WUPA&lt;/STRONG&gt;(PICC_REQIDL 0x26) -&amp;gt;&amp;nbsp;&lt;STRONG&gt;PCD_TransceiveData-&amp;gt;PCD_CommunicateWithPICC&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;When I present a PICC near the RC522 i get a response. The FIFO reg reports that 2 bytes is in buffer (ATQA). I fetch the two bytes and the data is 0x0002. However, just after that I read register (CONTROLREG &amp;amp; 0x07) and that returns and set valid bits to 7. This function returns OK back to&amp;nbsp;&lt;STRONG&gt;PICC_REQA_or_WUPA&lt;/STRONG&gt; but that functions reports &lt;STRONG&gt;error&lt;/STRONG&gt; because valid bits != 0.&lt;BR /&gt;&lt;U&gt;Can anyone explain this valid bits issue? Do I need it?&lt;/U&gt;&lt;BR /&gt;&lt;BR /&gt;FYI: I have three different PICC.&amp;nbsp; The reponse is 0x002, 0x0004 and 0x0044 respective. I was thinking of using this ATQA to get the UID somehow - if that is possible. As I said, it will not be a collision with other PICC:s.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jan 2024 10:40:41 GMT</pubDate>
    <dc:creator>Haddock</dc:creator>
    <dc:date>2024-01-15T10:40:41Z</dc:date>
    <item>
      <title>RC522, ATQA and valid bits. Pls explain.</title>
      <link>https://community.nxp.com/t5/NFC/RC522-ATQA-and-valid-bits-Pls-explain/m-p/1788729#M11170</link>
      <description>&lt;P&gt;I am using from beginning an arduino example converted to C. The MCU has a RC522 connected to it and using SPI as communication method.&amp;nbsp;No collision handling or authentication is needed.&amp;nbsp;The device only checks that the PICC can send its UID (it's a production test)&lt;/P&gt;&lt;P&gt;The call chain is:&amp;nbsp;&lt;STRONG&gt;PICC_IsNewCardPresent&lt;/STRONG&gt; -&amp;gt;&amp;nbsp;&lt;STRONG&gt;PICC_RequestA&lt;/STRONG&gt; -&amp;gt;&amp;nbsp;&lt;STRONG&gt;PICC_REQA_or_WUPA&lt;/STRONG&gt;(PICC_REQIDL 0x26) -&amp;gt;&amp;nbsp;&lt;STRONG&gt;PCD_TransceiveData-&amp;gt;PCD_CommunicateWithPICC&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;When I present a PICC near the RC522 i get a response. The FIFO reg reports that 2 bytes is in buffer (ATQA). I fetch the two bytes and the data is 0x0002. However, just after that I read register (CONTROLREG &amp;amp; 0x07) and that returns and set valid bits to 7. This function returns OK back to&amp;nbsp;&lt;STRONG&gt;PICC_REQA_or_WUPA&lt;/STRONG&gt; but that functions reports &lt;STRONG&gt;error&lt;/STRONG&gt; because valid bits != 0.&lt;BR /&gt;&lt;U&gt;Can anyone explain this valid bits issue? Do I need it?&lt;/U&gt;&lt;BR /&gt;&lt;BR /&gt;FYI: I have three different PICC.&amp;nbsp; The reponse is 0x002, 0x0004 and 0x0044 respective. I was thinking of using this ATQA to get the UID somehow - if that is possible. As I said, it will not be a collision with other PICC:s.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 10:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-ATQA-and-valid-bits-Pls-explain/m-p/1788729#M11170</guid>
      <dc:creator>Haddock</dc:creator>
      <dc:date>2024-01-15T10:40:41Z</dc:date>
    </item>
    <item>
      <title>Re: RC522, ATQA and valid bits. Pls explain.</title>
      <link>https://community.nxp.com/t5/NFC/RC522-ATQA-and-valid-bits-Pls-explain/m-p/1788922#M11172</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you using any Arduino library?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I apologize but &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/standard-performance-mifare-and-ntag-frontend:MFRC52202HN1" target="_blank"&gt;MFRC522&lt;/A&gt; is not recommended for new designs. For new designs, please use recommended product&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/clrc663-iplus-i-family-high-performance-nfc-frontends:CLRC66303HN" target="_blank"&gt;CLRC663&amp;nbsp;plus&lt;/A&gt;, so the support is limited.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 18:08:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-ATQA-and-valid-bits-Pls-explain/m-p/1788922#M11172</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-01-15T18:08:49Z</dc:date>
    </item>
  </channel>
</rss>