<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7642 Mass Storage Device Activation</title>
    <link>https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1786251#M11153</link>
    <description>&lt;P&gt;I am attempting to flash the firmware required for the Cockpit application on to a PNEV7642A development board. I am unable to get the USB port to enumerate as a mass storage device on my PC.&lt;/P&gt;&lt;P&gt;I think that I have the host interface correctly configured for USB using switches 5, 6, and 7. I have held down and released various combinations of the the VEN and DWL_REQ buttons without success.&lt;/P&gt;&lt;P&gt;The unit is powered from a 7.5V supply on J9.&lt;/P&gt;&lt;P&gt;I've read through through the various applications guides and these are main things that appear to be required.&lt;/P&gt;&lt;P&gt;What am I doing wrong? Thanks.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 10 Jan 2024 18:09:53 GMT</pubDate>
    <dc:creator>MLang</dc:creator>
    <dc:date>2024-01-10T18:09:53Z</dc:date>
    <item>
      <title>PN7642 Mass Storage Device Activation</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1786251#M11153</link>
      <description>&lt;P&gt;I am attempting to flash the firmware required for the Cockpit application on to a PNEV7642A development board. I am unable to get the USB port to enumerate as a mass storage device on my PC.&lt;/P&gt;&lt;P&gt;I think that I have the host interface correctly configured for USB using switches 5, 6, and 7. I have held down and released various combinations of the the VEN and DWL_REQ buttons without success.&lt;/P&gt;&lt;P&gt;The unit is powered from a 7.5V supply on J9.&lt;/P&gt;&lt;P&gt;I've read through through the various applications guides and these are main things that appear to be required.&lt;/P&gt;&lt;P&gt;What am I doing wrong? Thanks.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 18:09:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1786251#M11153</guid>
      <dc:creator>MLang</dc:creator>
      <dc:date>2024-01-10T18:09:53Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 Mass Storage Device Activation</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1786636#M11157</link>
      <description>&lt;P&gt;Hello sir,&lt;BR /&gt;My name is Fabian, I'm happy to help you with your case.&lt;BR /&gt;Thank you for your interest in our products. Would you mind sending us a photo of your setup just to scratch any possible issues?&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 01:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1786636#M11157</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2024-01-11T01:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: PN7642 Mass Storage Device Activation</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1790516#M11178</link>
      <description>&lt;P&gt;I resolved this myself.&lt;/P&gt;&lt;P&gt;If the PNEV7642A is not connected to the LPC55S16 dev board, the AD_NFC_HOSTSEL2 line is unterminated and allowed to float. This can prevent the USB interface from being enabled. Terminating this line to +3.3V properly enabled the USB interface allowing proper mass storage device operation.&lt;/P&gt;&lt;P&gt;This should probably be included as a note in the quick start guide.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 18:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Mass-Storage-Device-Activation/m-p/1790516#M11178</guid>
      <dc:creator>MLang</dc:creator>
      <dc:date>2024-01-17T18:40:08Z</dc:date>
    </item>
  </channel>
</rss>