<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7642 Host SPI Driver Example fails to run</title>
    <link>https://community.nxp.com/t5/NFC/PN7642-Host-SPI-Driver-Example-fails-to-run/m-p/1785593#M11142</link>
    <description>&lt;P&gt;The host interface SPI driver example runs successfully when using SDK V021201.&lt;/P&gt;&lt;P&gt;I upgraded to SDK V021205 and the SPI driver example fails to boot. It appears to reset immediately when executing the following line of code in main():&lt;/P&gt;&lt;P&gt;HOSTIF_Init(HOSTIF, &amp;amp;hifSpiConfig);&lt;/P&gt;&lt;P&gt;Tracing further in to the failure, I find that the reset happens when the call to the library function PN76_Get_NSRam_Addr_Len() is made from within HOSTIF_Init().&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a patch or other type of solution for this problem? I require the Host SPI interface for our target application and would prefer to be using the latest released SDK.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Wed, 10 Jan 2024 01:14:58 GMT</pubDate>
    <dc:creator>MLang</dc:creator>
    <dc:date>2024-01-10T01:14:58Z</dc:date>
    <item>
      <title>PN7642 Host SPI Driver Example fails to run</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Host-SPI-Driver-Example-fails-to-run/m-p/1785593#M11142</link>
      <description>&lt;P&gt;The host interface SPI driver example runs successfully when using SDK V021201.&lt;/P&gt;&lt;P&gt;I upgraded to SDK V021205 and the SPI driver example fails to boot. It appears to reset immediately when executing the following line of code in main():&lt;/P&gt;&lt;P&gt;HOSTIF_Init(HOSTIF, &amp;amp;hifSpiConfig);&lt;/P&gt;&lt;P&gt;Tracing further in to the failure, I find that the reset happens when the call to the library function PN76_Get_NSRam_Addr_Len() is made from within HOSTIF_Init().&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a patch or other type of solution for this problem? I require the Host SPI interface for our target application and would prefer to be using the latest released SDK.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 01:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Host-SPI-Driver-Example-fails-to-run/m-p/1785593#M11142</guid>
      <dc:creator>MLang</dc:creator>
      <dc:date>2024-01-10T01:14:58Z</dc:date>
    </item>
    <item>
      <title>回复： PN7642 Host SPI Driver Example fails to run</title>
      <link>https://community.nxp.com/t5/NFC/PN7642-Host-SPI-Driver-Example-fails-to-run/m-p/1787014#M11158</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227953"&gt;@MLang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;If you update the SDK you also have to update the Firmware of the PN7642. Every SDK is based on a particular firmware. Unfortunately not every SDK, or application, is backwards compatible as new functions have been introduced and addresses of APIs have changed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is explained in the Quick Start Guide&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13134.pdf" target="_self"&gt;https://www.nxp.com/docs/en/application-note/AN13134.pdf&lt;/A&gt;&amp;nbsp;in Chapter [1.2 Firmware Overview].&lt;/P&gt;&lt;P&gt;I hope this helps &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;Greetings, alex&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 08:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7642-Host-SPI-Driver-Example-fails-to-run/m-p/1787014#M11158</guid>
      <dc:creator>AlexanderB</dc:creator>
      <dc:date>2024-01-11T08:27:16Z</dc:date>
    </item>
  </channel>
</rss>