<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MFRC522 and RC522 Consultation in NFC</title>
    <link>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783431#M11122</link>
    <description>&lt;P&gt;Hi Kelly,&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;&lt;SPAN class=""&gt;Are there any restrictions on MCU manufacturers/models?&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;Thank you.&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Fri, 05 Jan 2024 07:01:34 GMT</pubDate>
    <dc:creator>Karyliu</dc:creator>
    <dc:date>2024-01-05T07:01:34Z</dc:date>
    <item>
      <title>MFRC522 and RC522 Consultation</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1781014#M11099</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;What's the main difference between MFRC522 and RC522?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Do these two chips support use on the operating system (Windows \ Android \ Linux)?&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;Is there a corresponding driver code?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Are there any restrictions on the main control chips that these two ICs can be paired with?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;What support does NXP provide for these two chips?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Dec 2023 02:40:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1781014#M11099</guid>
      <dc:creator>Karyliu</dc:creator>
      <dc:date>2023-12-29T02:40:11Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 and RC522 Consultation</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1781895#M11107</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198313"&gt;@Karyliu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What's the main difference between MFRC522 and RC522?&lt;BR /&gt;Ans: Actually, the two are the same product.&lt;/P&gt;
&lt;P&gt;Do these two chips support use on the operating system (Windows \ Android \ Linux)? Is there a corresponding driver code?&lt;BR /&gt;Ans: Just running on Windows, and there are not any examples for reference.&lt;/P&gt;
&lt;P&gt;Are there any restrictions on the main control chips that these two ICs can be paired with?&lt;BR /&gt;Ans: No restrictions, just SPI interface communication should be available.&lt;/P&gt;
&lt;P&gt;What support does NXP provide for these two chips?&lt;BR /&gt;Ans: As the MFRC522 is not recommended for new designs we do not have more information but the one in the public we page. We have some examples for some LPC's and other Kinetis files for the recommended products CLRC663 plus.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kelly&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 02:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1781895#M11107</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2024-01-03T02:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 and RC522 Consultation</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783319#M11120</link>
      <description>&lt;P&gt;Hi Kelly,&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thank you for your reply!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Does CLRC663 support freeRTOS?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Is there any restriction on MCU.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 02:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783319#M11120</guid>
      <dc:creator>Karyliu</dc:creator>
      <dc:date>2024-01-05T02:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 and RC522 Consultation</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783419#M11121</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198313"&gt;@Karyliu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, CLRC663+MCU can run with FreeRTOS, and NXP provides the examples all based on FreeRTOS.&lt;/P&gt;
&lt;P&gt;For MCU, which is no limitation, just has SPI or I2C interface should be ok.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kelly&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 06:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783419#M11121</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2024-01-05T06:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 and RC522 Consultation</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783431#M11122</link>
      <description>&lt;P&gt;Hi Kelly,&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;&lt;SPAN class=""&gt;Are there any restrictions on MCU manufacturers/models?&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;Thank you.&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 05 Jan 2024 07:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783431#M11122</guid>
      <dc:creator>Karyliu</dc:creator>
      <dc:date>2024-01-05T07:01:34Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 and RC522 Consultation</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783510#M11123</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/198313"&gt;@Karyliu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It's best to choose NXP MCUS because NXP offers routines that are based NXP's MCUS, such as LPC1769 and FRDM-K82F for your reference.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;kelly&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 08:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-and-RC522-Consultation/m-p/1783510#M11123</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2024-01-05T08:32:17Z</dc:date>
    </item>
  </channel>
</rss>