<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN7150 Reading Tag unreliable in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1777161#M11087</link>
    <description>Hello Janine, &lt;BR /&gt;Ok, please let us know if this helped. &lt;BR /&gt;&lt;BR /&gt;BR&lt;BR /&gt;Tomas</description>
    <pubDate>Tue, 19 Dec 2023 11:36:31 GMT</pubDate>
    <dc:creator>Tomas_Parizek</dc:creator>
    <dc:date>2023-12-19T11:36:31Z</dc:date>
    <item>
      <title>PN7150 Reading Tag unreliable</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1762448#M11005</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I have problems reading tags reliably.&lt;/P&gt;&lt;P&gt;Hardware:&amp;nbsp;Custom Board with&amp;nbsp;&lt;SPAN&gt;PN7150&lt;BR /&gt;&lt;/SPAN&gt;Tag: LXMS33HCNG-134&lt;BR /&gt;DH: Embedded Linux, using Library linux_nfc_api.h&lt;BR /&gt;Antenna and tag are at a fixed position towards one another.&lt;/P&gt;&lt;P&gt;Reading multiple blocks of the tags is done using the function &lt;STRONG&gt;nfcTag_transceive()&lt;BR /&gt;&lt;/STRONG&gt;with the following ReadCmd:&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;{0x02U, 0x23, /*block*/ 0x00, /* num Blocks 0x1C */ 28};&lt;/PRE&gt;&lt;P&gt;Analyzing the I2C communication between PN7150 and the DH I have the following different outcomes:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Tag recognizes immediately and read correctly&lt;/LI&gt;&lt;LI&gt;Tag recognized,&amp;nbsp;the function is able to read multiple blocks after several read attempts.&lt;BR /&gt;Unsuccessful attempts return "STATUS_RF_FRAME_CORRUPTED"&lt;/LI&gt;&lt;LI&gt;Tag recognized, but I2C communication stops mid Data Packets after the Notification Message is sent.&lt;/LI&gt;&lt;LI&gt;Tag nor recognized at all, returning&amp;nbsp;CORE_GENERIC_ERROR_NTF,&amp;nbsp;DISCOVERY_TARGET_ACTIVATION_FAILED&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;What could be the reason for this behavior? And how can I solve it?&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 07:43:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1762448#M11005</guid>
      <dc:creator>Janine</dc:creator>
      <dc:date>2023-11-23T07:43:02Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Reading Tag unreliable</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1764362#M11020</link>
      <description>&lt;P&gt;Hi Janine:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What is the distance between the reader and Tag?&amp;nbsp; maybe that is the maximum reader range for your project.&amp;nbsp; It is a critical distance.&amp;nbsp; Sometimes it can work, but not stable.&amp;nbsp; &amp;nbsp;This is normal.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;If you lower the distance, it should be stable.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Danie&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 00:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1764362#M11020</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2023-11-28T00:37:47Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Reading Tag unreliable</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1772411#M11072</link>
      <description>&lt;P&gt;Hi Daniel&lt;/P&gt;&lt;P&gt;Thanks a lot for your response. Sorry for not getting back sooner, I am still working on this and haven't found a reliable solution.&lt;/P&gt;&lt;P&gt;The distance between the reader and the tag is approx. 2.5mm.&lt;/P&gt;&lt;P&gt;The thing that still puzzles me is the following:&lt;BR /&gt;I had a setup in my lab, which was running flawlessly.&lt;BR /&gt;I then moved it into the field, same setup, no change of distance between tag and reader.&lt;BR /&gt;At the new location I have a lot of reading errors.&lt;/P&gt;&lt;P&gt;I cannot think of anything else besides temperature or humidity that is different.&lt;BR /&gt;Is the reader sensitive to those factors?&lt;/P&gt;&lt;P&gt;Thanks a lot for your help.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Janine&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 15:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1772411#M11072</guid>
      <dc:creator>Janine</dc:creator>
      <dc:date>2023-12-11T15:54:15Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Reading Tag unreliable</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1773167#M11074</link>
      <description>&lt;P&gt;Hello Janine,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please check this document -&amp;gt;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13892.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13892.pdf&lt;/A&gt;. (the principle is the same for PN7150 and PN7160)&lt;/P&gt;
&lt;P&gt;Especially pages 20 and 21. I think the issue could be due to the high RX gain.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Tomas&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Dec 2023 14:06:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1773167#M11074</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2023-12-12T14:06:23Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Reading Tag unreliable</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1775474#M11081</link>
      <description>&lt;P&gt;Hello Tomas&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;By default, the RX_GAIN (configured in libnfc-nxp-pn548.conf) was set to the maximum (57dB).&lt;/P&gt;&lt;P&gt;The first experiments look promising (for 40dB or 50dB, 33dB are not enough).&lt;BR /&gt;I will keep you posted.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Janine&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 09:03:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1775474#M11081</guid>
      <dc:creator>Janine</dc:creator>
      <dc:date>2023-12-15T09:03:35Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Reading Tag unreliable</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1777161#M11087</link>
      <description>Hello Janine, &lt;BR /&gt;Ok, please let us know if this helped. &lt;BR /&gt;&lt;BR /&gt;BR&lt;BR /&gt;Tomas</description>
      <pubDate>Tue, 19 Dec 2023 11:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Reading-Tag-unreliable/m-p/1777161#M11087</guid>
      <dc:creator>Tomas_Parizek</dc:creator>
      <dc:date>2023-12-19T11:36:31Z</dc:date>
    </item>
  </channel>
</rss>